Skip to main content
Visitor II
September 2, 2024
Question

MCSDK 6.3.1 release?

Hello there,

I am trying to generate 6 Step motor control firmware for some custom hardware based on the B-G431B-ESC1.

I would like to use the ESC PWM input feature, however the auto-generated code throws errors. This feature works fine in FOC mode, and I have tried to fix the errors by copying across the code generated in the FOC project and changing the TIMER configurations, but to no avail.

The problem is described in this post:

Error when generating code with MC Workbench 6.3.0 - STMicroelectronics Community

The responses there suggested this would be fixed in the 6.3.1 release. Is there any news on when this version will become available, or would it be possible to gain access to the beta?

Many thanks

    This topic has been closed for replies.

    1 reply

    GMA
    ST Technical Moderator
    October 10, 2024

    Hello @SquirrelySquirrel99,

    MCSDK 6.3.1 is out.

    If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA