Skip to main content
steve feng
Associate II
March 11, 2026
Solved

Using Custom HID and BNO055

Hi Forum!

----------------------------------------------------------------------------------------------------------------------------------------------------------

----------------------------------------------------------------------------------------------------------------------------------------------------------

  1. I using BNO055 to get the quaternion value via I2C
  2. The quaternion value will send to host(PC or SBC) using USB cable
  3. I using STM32 EV-Board (NUCLEO-F412ZG)
  4. Using the BNO055 library from:
    https://github.com/ivyknob/bno055_stm32

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

  • The setting is shown as below
  • CubeMX *.ioc Configuration
    • Select the board NUCLEO-F412ZG
    • System Core
      • RCC ->High Speed Clock: Crystal/Ceramic 
      • SYS ->Debug: Serial Wire
    • Connectivity
      • I2C1->i2c, change to i2c speed mode from standard mode to fast mode
      • USB_OTG_FS-> mode: Device_Only
    • Middleware and software
      • Class for FS IP: select Custom Human Interface Device and change the PID to 22352
        upload3.png
    • Clock configuration
      • HCLK:72MHz
      • USB CLK: 48MHz
    • Others:
      • Add necessary library files as reference and in the toolchain project configuration file
      • Generate peripheral initialization as pair of '.c/.h' file per peripheral
      • PB0(On EV-board LED, LD1) set as GPIO output push pull, default pull down for debugging
  • Keil C Configuration
    • After generate code, compile and flash the hex file to the board, open the Device Administrator, and I could see the human device interface is found but driver error detect
    • Modify the Report descriptor, found the usbd_custom_hid_if.c file and in function CUSTOM_HID_ReprotDesc_FS add the code as below
/** Usb HID report descriptor. */
__ALIGN_BEGIN static uint8_t CUSTOM_HID_ReportDesc_FS[USBD_CUSTOM_HID_REPORT_DESC_SIZE] __ALIGN_END =
{
 /* USER CODE BEGIN 0 */
 	0x06,0xFF,0x00, // USAGE_PAGE (Vendor Page: 0xFF00)
	0x09,0x01,			// USAGE (Vendor Usage 1)
	0xA1,0x01,			// COLLECTION (Application)
	0x15,0x00,			// LOGICAL_MINIMUM (0)
	0x26,0xFF,0x00,		// LOGICAL_MAXIMUM (255)
	0x75,0x08,			// REPORT_SIZE (8)
	0x95,0x40,			// REPORT_COUNT (64)
	0x09,0x02,			// USAGE (Vendor Usage 2)
	0x81,0x02,			// INPUT (Data,Var,Abs)
	0x09,0x03,			// USAGE (Vendor Usage 3)
	0x91,0x02,			// OUTPUT (Data,Var,Abs) 
	0x0A,0x00,0xFF,	 // UsageS(0xFF00)
	0x0B1,0x02,
 /* USER CODE END 0 */
 0xC0 /* END_COLLECTION	 */
};
  • The number of CUSTOM_HID_ReportDesc_FS array is "30", so modify the "USBD_CUSTOM_HID_REPORT_DESC_SIZE", open the usbd_conf.h, modify these two define as shown below
#define USBD_CUSTOMHID_OUTREPORT_BUF_SIZE 64
/*---------- -----------*/
#define USBD_CUSTOM_HID_REPORT_DESC_SIZE 30
  • Modify the node "output" and "input" define from usbd_customhid.h, 0x40hex =64dec 
#define CUSTOM_HID_EPIN_ADDR 0x81U
#endif /* CUSTOM_HID_EPIN_ADDR */

#ifndef CUSTOM_HID_EPIN_SIZE
#define CUSTOM_HID_EPIN_SIZE 0x40//0x02U
#endif /* CUSTOM_HID_EPIN_SIZE */

#ifndef CUSTOM_HID_EPOUT_ADDR
#define CUSTOM_HID_EPOUT_ADDR 0x02U//0x01U
#endif /* CUSTOM_HID_EPOUT_ADDR */

#ifndef CUSTOM_HID_EPOUT_SIZE
#define CUSTOM_HID_EPOUT_SIZE 0x40//0x02U
  • STM32 need to receive the data from host, add the code in CUSTOM_HID_OutEvent_FS, the function is from usbd_custom_hid_if.c file
//add variable

/* USER CODE BEGIN INCLUDE */
extern uint8_t report_buffer[64]; 
extern uint8_t volatile flag_rx;
/* USER CODE END INCLUDE */

//modify the custom hid outevnet fs
static int8_t CUSTOM_HID_OutEvent_FS(uint8_t event_idx, uint8_t state)
{
 /* USER CODE BEGIN 6 */
 USBD_CUSTOM_HID_HandleTypeDef *hhid = (USBD_CUSTOM_HID_HandleTypeDef *)hUsbDeviceFS.pClassData;
 memcpy(report_buffer, hhid->Report_buf, 64);
 flag_rx = 1;
 return (USBD_OK);
 /* USER CODE END 6 */
}
​
  • In the main function, including the BNO055 library and confirm the input string 
/* USER CODE BEGIN Includes */
#include "usbd_customhid.h"
#include "string.h"
#include "bno055_stm32.h"
/* USER CODE END Includes */

/* USER CODE BEGIN PM */
uint8_t tx_buffer[64];
uint8_t report_buffer[64];
uint8_t volatile flag_rx = 0;
extern USBD_HandleTypeDef hUsbDeviceFS;
int32_t data_to_send[4];
/* USER CODE END PM */

 /* USER CODE BEGIN 2 */
	HAL_Delay(2000);
	bno055_assignI2C(&hi2c1);
	bno055_setup();
	bno055_setOperationModeNDOF();
 /* USER CODE END 2 */

 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
		if(flag_rx==1)
		{
			report_buffer[63] = '\0'; 
			flag_rx=0;
			char cmd[10];
			int duty=0;
			
			if(sscanf((char*)report_buffer,"%s %d",cmd,&duty)==2)
			{
				HAL_Delay(2);
				if(strcmp(cmd,"LM3435")==0)
				{
					sprintf((char*)tx_buffer, "OK! Duty set to %d", duty);
					USBD_CUSTOM_HID_SendReport(&hUsbDeviceFS, tx_buffer, 64);
				}
			}
			memset(report_buffer,0,64);
		}

		
		USBD_CUSTOM_HID_HandleTypeDef *hhid = (USBD_CUSTOM_HID_HandleTypeDef*)hUsbDeviceFS.pClassData;

		if (hhid->state == CUSTOM_HID_IDLE) 
		{
			bno055_vector_t v = bno055_getVectorQuaternion();
			data_to_send[0] = (int32_t)(v.w * 1000000);
			data_to_send[1] = (int32_t)(v.x * 1000000);
			data_to_send[2] = (int32_t)(v.y * 1000000);
			data_to_send[3] = (int32_t)(v.z * 1000000);
			memset(tx_buffer, 0, 64);				
			memcpy(tx_buffer, data_to_send, sizeof(data_to_send));				
			USBD_CUSTOM_HID_SendReport(&hUsbDeviceFS, tx_buffer, 64);
		}
		HAL_Delay(10); // BNO055 100Hz,		
				
			}
 /* USER CODE END 3 */



​
  • Reserved typing space

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Result:

  1. BNO055 pin connection: SCL-> PB8, SDA->PB9, 3V0->VCC, GND->GND, ADR->GND
  2. Option for Target "myHIDBNO055", in the device->code generation, select "Use MicroLIB"
  3. Connect the USB power from CN1(micro A) first, and connect the User USB from CN13
  4. The HID device could found from host
    upload2.png
  5. Could read the BNO055 via I2C
  6. Could send the data from STM32 to host in100Hz
  7. Could receive the data from host to STM32 first time
    upload1.png
  8. Fail: Could not receive the data from host to STM32 second time
    1. modify the BNO055 speed by HAL_Delay(10 ~ 1000), the tool still crash

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Reference:
1. micro lib to solve the LDR R0, =SystemInit
https://community.st.com/t5/stm32-mcus-products/stm32f4-random-hard-faults-solved/td-p/516713
2. how to use Custom hid 1
https://blog.csdn.net/qq_36347513/article/details/127694257 
3. how to use Custom hid 2
https://lungtenghsu.blogspot.com/2024/11/stm32usb-custom-hid.html 

4. HID Learning
https://www.youtube.com/watch?v=umkD1piCNvc 
5.BNO055 Library
https://github.com/ivyknob/bno055_stm32 

6. MATA OCULUS Tracking 

https://msl.cs.illinois.edu/~lavalle/papers/LavYerKatAnt14.pdf 

 

 

steve feng
steve fengBest answer
Associate II
April 22, 2026

Hi

 

After some testing,

The problem is from function "USBD_CUSTOM_HID_DataOut()"

static uint8_t USBD_CUSTOM_HID_DataOut(...)
{
 // ... callback after
 return (uint8_t)USBD_OK;
 
 // did not called, USBD_CUSTOM_HID_ReceivePacket()!
 // OUT endpoint will not preprare to receive the new data
 // the second data send from host, stm will lock in NAK
 // SimpleHIDWrite timeout ->software crash
}

 

I found the problem that I forget to add this 

static uint8_t USBD_CUSTOM_HID_DataOut(USBD_HandleTypeDef *pdev, uint8_t epnum)
{
 UNUSED(epnum);
 USBD_CUSTOM_HID_HandleTypeDef *hhid;
 if (pdev->pClassDataCmsit[pdev->classId] == NULL)
 {
 return (uint8_t)USBD_FAIL;
 }
 hhid = (USBD_CUSTOM_HID_HandleTypeDef *)pdev->pClassDataCmsit[pdev->classId];

#ifdef USBD_CUSTOMHID_REPORT_BUFFER_EVENT_ENABLED
 ((USBD_CUSTOM_HID_ItfTypeDef *)pdev->pUserData[pdev->classId])->OutEvent(hhid->Report_buf);
#else
 ((USBD_CUSTOM_HID_ItfTypeDef *)pdev->pUserData[pdev->classId])->OutEvent(hhid->Report_buf[0],
 hhid->Report_buf[1]);
#endif

 /* add this line */
 (void)USBD_CUSTOM_HID_ReceivePacket(pdev);

 return (uint8_t)USBD_OK;
}

 

1.This file is not in user code part (this is STM32 HAL middleware), if CUBEMX re-generate, these  code will be          overwritten.

2.After this step, I can receive and transmit the data from BNO055 to STM32 and get these data via USB HID.

-------------------------------------------------------------

the main part

 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 if (flag_rx == 1)
 {
 flag_rx = 0;

 char cmd[16] = {0};
 int duty = 0;

 if (sscanf((char*)report_buffer, "%15s %d", cmd, &duty) == 2)
 {
 if (strcmp(cmd, "LM3435") == 0)
 {
 memset(tx_buffer, 0, 64);
 snprintf((char*)tx_buffer, 64, "OK! Duty set to %d", duty);
 HID_SafeSend(tx_buffer, 64); 
 }
 }
 memset(report_buffer, 0, 64);
 }

 bno055_vector_t v = bno055_getVectorQuaternion();
 int32_t data_to_send[4];
 data_to_send[0] = (int32_t)(v.w * 1000000);
 data_to_send[1] = (int32_t)(v.x * 1000000);
 data_to_send[2] = (int32_t)(v.y * 1000000);
 data_to_send[3] = (int32_t)(v.z * 1000000);

 memset(tx_buffer, 0, 64);
 memcpy(tx_buffer, data_to_send, 16);
 HID_SafeSend(tx_buffer, 64); 
		HAL_GPIO_TogglePin(GPIOB,GPIO_PIN_0);//testing that if loop is still on-work or broken
 HAL_Delay(10);
				
	}
 /* USER CODE END 3 */

/********************************/
/* USER CODE BEGIN 4 */
uint8_t HID_SafeSend(uint8_t *buf, uint16_t len)
{
 USBD_CUSTOM_HID_HandleTypeDef *hhid = 
 (USBD_CUSTOM_HID_HandleTypeDef*)hUsbDeviceFS.pClassData;
 
 uint32_t tick = HAL_GetTick();
 while (hhid->state != CUSTOM_HID_IDLE)
 {
 if ((HAL_GetTick() - tick) > 10) 
 {
 return USBD_FAIL; // 
 }
 }
 return USBD_CUSTOM_HID_SendReport(&hUsbDeviceFS, buf, len);
}
/* USER CODE END 4 */

 

Thank you

Best Regard Steve

 

4 replies

ST Technical Moderator
March 11, 2026

Hi @steve feng 

I assume the descriptor you posted in CUSTOM_HID_ReportDesc_FS has an issue with 

	0x0B1,0x02,

 0x0B1 is not a valid hex byte; and if you meant 0xB1, it’s still not valid in this context and will corrupt the descriptor parse in the host HID stack. Then instead of hard coded size to 30, set 

#define USBD_CUSTOM_HID_REPORT_DESC_SIZE (sizeof(CUSTOM_HID_ReportDesc_FS))

The issue seems endpoint / report descriptor mismatch.

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
steve feng
Associate II
March 17, 2026

Hi FBL

 

Thank you for advice, I try to correct my code.

  • modify the  "__ALIGN_BEGIN static uint8_t CUSTOM_HID_ReportDesc_FS[USBD_CUSTOM_HID_REPORT_DESC_SIZE] __ALIGN_END =" content, 
	0xB1,0x02, //orginal 0x0B1,0x02,​

 the result is as as previous experiments, when the second time, host sending the data to EVK, the             SimpleHIDWrite exe will be crash.

  • Modify the  "[USBD_CUSTOM_HID_REPORT_DESC_SIZE] "
    1. set the value above 30
      1. result: compile success, but the host could not identified this HID device (Device settings for XXXXX could not be migrated from the previous operating system due to incomplete or unclear device pairing.)
    2. set the value below 30
      1. result: compile fail, the terminal said that: error:#146: too many initializer values
Pavel A.
March 11, 2026

@steve feng While NotebookLM and other AI tricks are cool, a real human may be still a better locomotive to success.

You can find helping hands for your project here; and use AI to formulate the tasks.

 

steve feng
steve fengAuthorBest answer
Associate II
April 22, 2026

Hi

 

After some testing,

The problem is from function "USBD_CUSTOM_HID_DataOut()"

static uint8_t USBD_CUSTOM_HID_DataOut(...)
{
 // ... callback after
 return (uint8_t)USBD_OK;
 
 // did not called, USBD_CUSTOM_HID_ReceivePacket()!
 // OUT endpoint will not preprare to receive the new data
 // the second data send from host, stm will lock in NAK
 // SimpleHIDWrite timeout ->software crash
}

 

I found the problem that I forget to add this 

static uint8_t USBD_CUSTOM_HID_DataOut(USBD_HandleTypeDef *pdev, uint8_t epnum)
{
 UNUSED(epnum);
 USBD_CUSTOM_HID_HandleTypeDef *hhid;
 if (pdev->pClassDataCmsit[pdev->classId] == NULL)
 {
 return (uint8_t)USBD_FAIL;
 }
 hhid = (USBD_CUSTOM_HID_HandleTypeDef *)pdev->pClassDataCmsit[pdev->classId];

#ifdef USBD_CUSTOMHID_REPORT_BUFFER_EVENT_ENABLED
 ((USBD_CUSTOM_HID_ItfTypeDef *)pdev->pUserData[pdev->classId])->OutEvent(hhid->Report_buf);
#else
 ((USBD_CUSTOM_HID_ItfTypeDef *)pdev->pUserData[pdev->classId])->OutEvent(hhid->Report_buf[0],
 hhid->Report_buf[1]);
#endif

 /* add this line */
 (void)USBD_CUSTOM_HID_ReceivePacket(pdev);

 return (uint8_t)USBD_OK;
}

 

1.This file is not in user code part (this is STM32 HAL middleware), if CUBEMX re-generate, these  code will be          overwritten.

2.After this step, I can receive and transmit the data from BNO055 to STM32 and get these data via USB HID.

-------------------------------------------------------------

the main part

 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 if (flag_rx == 1)
 {
 flag_rx = 0;

 char cmd[16] = {0};
 int duty = 0;

 if (sscanf((char*)report_buffer, "%15s %d", cmd, &duty) == 2)
 {
 if (strcmp(cmd, "LM3435") == 0)
 {
 memset(tx_buffer, 0, 64);
 snprintf((char*)tx_buffer, 64, "OK! Duty set to %d", duty);
 HID_SafeSend(tx_buffer, 64); 
 }
 }
 memset(report_buffer, 0, 64);
 }

 bno055_vector_t v = bno055_getVectorQuaternion();
 int32_t data_to_send[4];
 data_to_send[0] = (int32_t)(v.w * 1000000);
 data_to_send[1] = (int32_t)(v.x * 1000000);
 data_to_send[2] = (int32_t)(v.y * 1000000);
 data_to_send[3] = (int32_t)(v.z * 1000000);

 memset(tx_buffer, 0, 64);
 memcpy(tx_buffer, data_to_send, 16);
 HID_SafeSend(tx_buffer, 64); 
		HAL_GPIO_TogglePin(GPIOB,GPIO_PIN_0);//testing that if loop is still on-work or broken
 HAL_Delay(10);
				
	}
 /* USER CODE END 3 */

/********************************/
/* USER CODE BEGIN 4 */
uint8_t HID_SafeSend(uint8_t *buf, uint16_t len)
{
 USBD_CUSTOM_HID_HandleTypeDef *hhid = 
 (USBD_CUSTOM_HID_HandleTypeDef*)hUsbDeviceFS.pClassData;
 
 uint32_t tick = HAL_GetTick();
 while (hhid->state != CUSTOM_HID_IDLE)
 {
 if ((HAL_GetTick() - tick) > 10) 
 {
 return USBD_FAIL; // 
 }
 }
 return USBD_CUSTOM_HID_SendReport(&hUsbDeviceFS, buf, len);
}
/* USER CODE END 4 */

 

Thank you

Best Regard Steve