Join discussions in the Product Forums. Ask questions, learn from your peers, and share insights on ST solutions to accelerate your design journey.
Most recent activity
Hi ST Engineers: Is the audio amplifier demo board STEVAL-CCA044V1 still active for ordering, or is the board STEVAL-CCA044V1 obsolete? Best Regards Simon Peng
Hello everyone, I'm having some trouble implementing I3C communication and would like to ask for some help. I am using the NUCLEO-H503RB board as my main controller. For the target devices, I have the NUCLEO-IKS01A3 expansion board and the TSC1641 (Click Board) connected. I'm currently facing some issues with the I3C communication setup between these components. I have successfully managed to read the WHO_AM_I ID from the LSM6DSO (on the NUCLEO-IKS01A3). However, when I attempt to read the ID from the TSC1641, the SCL line continues to output a clock signal (or stays toggling) without a proper response. I am seeking assistance in analyzing the root cause of this issue.
hello,now I am using stm32f030cct6 to design a simple program. i used all the 6 uarts of this chip. it works fine, but the interrupt code generated by STM32CubeMX has a simple bug. the code as below.for the uart6, there is a useless (&huart6); i think it is no effect to the function, but when building, there is a warning.stm32f0xx_it.c:172:33: warning: statement with no effect [-Wunused-value][build] 172 | HAL_UART_IRQHandler(&huart6);(&huart6);[build] | ~^~~~~~~~ I dont like the warning. so i think you can simplly fix this bug. thanks.
Hello ST Community,I am working on an OTA firmware update implementation on STM32L496, and I am facing an issue related to dual-bank internal flash usage when the firmware size exceeds 512 KB.I would like to explain my setup and the problem in a simple and clear way. MCU and Flash DetailsMCU: STM32L496Internal Flash: 1 MBFlash configured in dual-bank modeBank1: 512 KBBank2: 512 KB What We Are DoingNormal ApplicationThe main application is stored in internal flashFirmware is built using STM32CubeIDENo OTA activity during normal operationOTA (Current / Tested)OTA is performed using NB-IoT and NFCFirmware is received in chunksChunks are written to flashCRC is verifiedAfter successful verification, firmware is switchedThis OTA flow works only when firmware size is less than 512 KB. Main Issue (Occurs Even Without OTA)When the firmware size increases beyond 512 KB (for example ~600 KB), the system starts misbehaving even if OTA is not started at all.Observed BehaviorUART logs
I want to make a pedometer app that would count steps and display the number of steps on an LCD screen. I have tested my functions for the screen (ILI9341 SPI), and they work successfully. I tested the LCD code by initializing a timer that incremented the value to display every second and sets the flag update_lcd_flag.But when I add the pedometer code, which uses SPI1, the value on the screen never gets updated past zero. Is it because I launch a DMA interrupt from the timer interrupt, or do I need to look for problems somehwere else, e.g. in my pedometer logic or SPI1 configuration? The pedometer relies on the accelometer, which is built into STM32F4O7G-DISC1, which is my board, by defaultP.S. The LCD functions don't use interrupts or DMA, they only use polling.The timer callbackvoid HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef* htim) { if (htim->Instance == TIM2) { if (draw_ready == 1) { HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_RESET); HAL_SPI_T
I am working with the NUCLEO-WB55RG, trying to get the filter accept list ("white list") feature working. Here is what I'm doing: - The NUCLEO is a peripheral implementing a custom BLE template, generated with STM32CubeMX 6.16.1. The "full" wireless stack V1.24.0 is installed on the M0+ core. - Start advertising with NO_WHITE_LIST_USE, connect, pair, and bond with a Central. This all works. Disconnect, call "aci_gap_add_devices_to_list()" (mode 0x03, also tried 0x05) with my bonded device list (retrieved with "aci_gap_get_bonded_devices()"). I have _also_ tried just called the "aci_gap_configure_whitelist()" command, the result is the same. - Then, if the # of bonded devices is > 0, when advertising restarts I use WHITE_LIST_FOR_ALL as the filter policy. In either case, I can connect and bond with two iOS devices. It seems that the white list isn't actually doing anything, and I can't figure out what to do. I followed the advice here, with no resul
I'm currently using Touchgfx after updating from version 4.25 to 4.26.When I build and run the code generated by Touchgfx 4.26, Display color doesn't match the design in Touchgfx 4.26.But When I do the same thing through Touchgfx 4.25, Display color matched very well.
I am migrating from STM32L431 to STM32L471. After migration, the function relating to internal flash writing does not work any more. The problem is when I programmed internal flash with HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, address, data), following errors occurred, including FLASH_SR_PROGERR, FLASH_FLAG_PGAERR, and FLASH_FLAG_PGSERR.I searched on the web, and found problem may relate to timer initialization and watchdog usage. I added HAL_TIM_Base_DeInit before HAL_TIM_Base_Init, and watchdog is disabled completely in the system including wathdog initialization and update.. But the problem is still there.By the way, the development environment is MDK5.36, ARM::CMSIS IS 5.8.0 (5.6.0 is also tested), ARM::CMSIS-Driver is 2.6.1, Keil::STM32L4xx_DFP is 2.6.1.So, what the problem it might be, and how can I solve this problem?Thanks
Hello ST, We are trying to enable USART6 as a serial console, in the stm32mp257f-dk board, we have builded the SDK using Openstlinux "Distribution package", I had done the below changes in the stm32mp257f-dk.dts device tree present in the kernel-source and u-boot directory : aliases { serial1 = &usart6; }; chosen { stdout-path = "serial1:115200n8"; #address-cells = <2>; #size-cells = <2>; ranges; }; &usart2 { pinctrl-names = "default", "idle", "sleep"; pinctrl-0 = <&usart2_pins_a>; pinctrl-1 = <&usart2_idle_pins_a>; pinctrl-2 = <&usart2_sleep_pins_a>; /delete-property/dmas; /delete-property/dma-names; status = "okay"; }; &usart6 { pinctrl-names = "default", "idle", "sleep"; pinctrl-0 = <&usart6_pins_a>; pinctrl-1 = <&usart6_idle_pins_a>; pinctrl-2 = <&usart6_sleep_pins_a>; uart-has-rtscts; status = "okay"; }; And also modified the stm32mp257f-dk-
I have a STM32MP257 custom board and I'm listening on UART6.When I boot, I get nothing. No messages or other text. I have not yet implemented any Linux onto my SD-card.The issue is that I have my USART6 boot pins on PF13 and PF14, instead of PF4 and PF5. Are there any way to change this in ROM?Or do I need to load TF-A from my SD-card so TF-A can change USART6 pins?
Hello, I am planning out a project that uses new BLE 5.4 feature periodic advertising with response and I wanted to use STM32WBA as a broadcaster and STM32WB0s as observers. There seems to be a great software support for this on WB0 but when it comes to WBA I can't find much documentation or any examples even on periodic advertising. Do you plan to add this in the future? Or is STM3WBA more focused on audio and will not get these features? Thank you
Hello ST team,I am facing a reproducible issue with USART6 on the STM32MP257F-DK board when working with the OpenSTLinux 6.6.78-stm32mp-r2 distribution.1. Summary of the ProblemWhen I enable USART6 in the Linux Device Tree and deploy the DTB on the target:SSH access breaks completely after reboot(ssh root@192.168.7.1 no longer works)When running a simple A35 UART6 echo application via minicom,the entire board resets.The reset is triggered by RIFSC / SERC firewall exceptions.The very same DTS configuration works perfectly on OpenSTLinux 6.6.48 —no SSH issue, no kernel panic, and UART6 user application runs fine.This strongly suggests a firewall / RIF / OP-TEE integration regression between OSTL 6.0.0 and 6.6.78.2. DTS Snippet That Triggers the Problem &usart6 { pinctrl-names = "default", "idle", "sleep"; pinctrl-0 = <&usart6_pins_a>; pinctrl-1 = <&usart6_idle_pins_a>; pinctrl-2 = <&usart6_sleep_pins_a>; status = "okay"; /* e
I installed the latest STM32CubeProgrammer in WSL on windows 11: the GUI has issue to load so I'm using the STM32_Programmer_CLI.However the flashing would fail most of the time:---- log output begin -----....Sector[0] downloaded successfully...File download completeTime elapsed during download operation: 00:00:01.624RUNNING Program ...PartID: :0x01DFU status = 0 : OKDFU state = 5 : dfuDNLOAD-IDLEbwPollTimeout = 1sending a dfu end of download requestDFU status = 0 : OKDFU state = 7 : dfuMANIFESTbwPollTimeout = 1DFU status = 0 : OKDFU state = 2 : dfuIDLEsending a set alternate setting request with index: 4receiving packetDFU status = 0 : OKDFU state = 2 : dfuIDLEUpLoading dataDFU status = 0 : OKDFU state = 2 : dfuIDLEdata: 00ffffffff000000000....Request detach value = 1sending a set alternate setting request with index: 0DFU status = 0 : OKDFU state = 2 : dfuIDLEReconnecting the device ...Reconnecting...Error: Unable to reconnect the target device: time out expiredError: Start
Hello,I am using an ST7701S LCD over 3-wire SPI (CS, SCK, SDA) with my STM32.When I send the initialization commands from my ESP, I noticed the following:The first command of the sequence is not sent.The program seems to stop at the second stage, around the 100th command.SPI is configured in master mode, polling (no DMA, no interrupts).Example of the write function:void ST7701_Write(uint8_t dc, uint8_t data) { uint16_t value = ((dc & 0x01) << 8) | data; HAL_GPIO_WritePin(LCD_CS_GPIO_Port, LCD_CS_Pin, GPIO_PIN_RESET); HAL_SPI_Transmit(&hspi2, (uint8_t *)&value, 1, HAL_MAX_DELAY); HAL_GPIO_WritePin(LCD_CS_GPIO_Port, LCD_CS_Pin, GPIO_PIN_SET); }Questions:Could the first command being skipped be due to HAL/SPI initialization or state?What is the recommended method to ensure all commands are reliably sent over 3-wire SPI to ST7701S?Thank you for your help.
Hello Everyone,I hope this message finds you well. I am currently developing a USB Host application using the STM32H573I-DK and have encountered a persistent Hard Fault issue that I would like to seek your expertise on.[Environment Information]Target: STM32H573I-DKExample: USBPD_SRC_UX_Host_MSC Stack: Azure RTOS (ThreadX, USBX)[Detailed Symptom]A hard fault occurs during initialization or while driving the process thread (msc_process_thread_entry) when connecting a USB MSC device. Debugging revealed abnormal memory access occurring during execution of the _ux_utility_memory_copy function.[Inquiry]When implementing USBX Host in this example and the STM32H5 environment, we seek broad advice on potential causes that could trigger memory copy and access errors.Example Stability: Are there any known issues or patch histories related to USBX memory management or stack configuration in the currently deployed USBPD_SRC_UX_Host_MSC example?H5 Architecture Characteristics: Are there scenari
I'm using stm32u535 and would like to have zero crossing detection of supply voltage. I've requirement of 6ADC channels and all are configured in differential mode and adc clock is 25Mhz and resolution is 14 bit and dma circular mode is enabled. On channel 6 i e enabled analog watchdog and written logic in isr to toggle GPIO. I proved gpio and I see deviation. Can someone help here. Here is my code snippet:ADC and AWDG initialization: hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1; hadc1.Init.Resolution = ADC_RESOLUTION_14B; hadc1.Init.GainCompensation = 0; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV; hadc1.Init.LowPowerAutoWait = DISABLE; hadc1.Init.ContinuousConvMode = ENABLE; hadc1.Init.NbrOfConversion = 8; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_N
Hi STM Devs!I would like to introduce a thread scheduling library - SuperTinyKernel (STK).Its GitHub repo: https://github.com/dmitrykos/stkYou can check capabilities in detail on GitHub but briefly STK can:Soft and hard real-time support: STK supports cooperative scheduling for “soft real-time” tasks, you can also enable hard real-time mode (KERNEL_HRT) for periodic tasks with guaranteed deadlines.Static and dynamic tasks: Define all tasks at startup (KERNEL_STATIC) or allow tasks to be created and destroyed at runtime (KERNEL_DYNAMIC).Low-power friendliness: STK puts MCU into a low-power mode when there are no runnable tasks (task calls Sleep).Tiny footprint: Minimal C++ abstractions (no STL, no heavy namespaces) keep the kernel small and simple.Portability: Supports ARM Cortex-M and RISC-V RV32 MCUs.Multi-core support: Fully implemented for Cortex-M and RISC-V.x86 development mode: Compile & debug your code on a PC before flashing to the MCU, which helps with early
the best I achieve so far using DWT as well as PMU is 'few cycles' accuracy. My question is, how I measure execution time such that I get 1 cycle difference when I insert a nop in the measured code ? (assuming interrupts and caches are disabled).Both functions below return 1!.global test_pmu0 .type test_pmu0, %function .align 2 test_pmu0: isb sy dsb sy ldr r3, .test_pmu0.pmu_base ldr r0, [r3, #0x7C] //read PMU->CCNTR ldr r1, [r3, #0x7C] //read PMU->CCNTR sub r0,r1,r0 bx lr .align 2 .test_pmu0.pmu_base: .word 0xE0003000 //PMU base address .global test_pmu1 .type test_pmu1, %function .align 2 test_pmu1: isb sy dsb sy ldr r3, .test_pmu1.pmu_base ldr r0, [r3, #0x7C] //read PMU->CCNTR nop ldr r1, [r3, #0x7C] //read PMU->CCNTR sub r0,r1,r0 bx lr .align 2 .test_pmu1.pmu_base: .word 0xE0003000 //PMU base address
I try to enable the PCROP Feature on a STM32H753I am using the STM32CubeProgrammer and connect via ST-Link V2After connecting, I go to the "OB" page and set the PROT_AREA_END1 value to 0xFFF and activate the DMEP1Then I press the "Apply" button and this happens in the log:Option byte command : -ob PROT_AREA_END1=0xFFF PROGRAMMING OPTION BYTES AREA ... Bank : 0x00 Address : 0x5200201c Size : 308 Bytes UPLOADING OPTION BYTES DATA ... Bank : 0x00 Address : 0x5200201c Size : 308 Bytes OPTION BYTE PROGRAMMING VERIFICATION: Error: Expected value for Option Byte "PROT_AREA_END1": 0xFFF, found: 0x0 Error: Option Byte Programming failedAnd then, I always get the error Message "Option Byte Programming failed"The RDP has level 0, but the same error occures, if I try to set RDP to level 1 at the same time.In the documentation I found no hint, that there is any other prerequisite must be met to set the PCROP.Has anyone an idea what the problem could be?(In generally the chip works, I can eras
Hi everyone,I am encountering an issue with the "Access to MCU Selector" feature.The Problem: After installing X-CUBE-AI packages version 10.2 (or any version later than 10.0), the MCU Selector fails to open. It gets stuck in an infinite loading loop. Additionally, the "Output" view remains empty, showing no error logs.Troubleshooting: I found that if I uninstall the versions newer than 10.0 and revert to X-CUBE-AI version 9.0.0, the MCU Selector works perfectly fine.Has anyone faced this issue? Is there a known workaround or solution to use the 10.2 version without breaking the MCU Selector?Thanks in advance.
I have a custom PCB with an STM32H563VGT6 microcontroller and an external Winbond W25Q16JVUXIQ NOR flash memory connected to the octoSPI's (XSPI) upper four pins. The problem is I can only write data to the flash memory after an erase, if I reset my board between the two operation. Everything the erasing, writing, indirect reading, memory mapped reading work on their own, but not after erase without reset. I read out all 3 status registers, they are the same before and after the chip erase. (Of course I set the write enable bit before trying to write into the memory) Any idea what could be the problem?
I want to design a baord with stm32h7b0zbt6 with extranal sdram chip W9825G6KH-6. I get PG15 with FMC_SDNCAS alt func in datasheet as below:But when I looked the PG15 alt func config I get as below info, I could not found an alternate function number for FMC_SDNCAS here ?? why they are not consistent ?
Hi there, i hope youre doing great! Im exploring FUOTA over LoRa/LoRaWAN using STM32CubeWL and the Nucleo-WL55JC1For this purpose im exploring the application (included in STM32CubeWL) "LoRaWAN_FUOTA_DualCore"I read the 'readme' file to accomplish build and flashing of the board with this application but the build.bat file throws an errorSo i decided to compile every project of the full application inside STM32CubeIDE, but in the project 'LoRaWAN_End_Node_DualCore_CM0PLUS' i found a linker error:... LoRaWAN_End_Node_DualCore_CM0PLUS.elf section `.data' will not fit in region `APPLI_ROM'...region `APPLI_ROM' overflowed by 272 bytesIm using STM32CubeIDE v2.0.0 and STM32CubeWL v1.4.0, running on windows 11Am i doing something wrong? Any suggestions?
Hello,Description: I am attempting to generate two simultaneous pulses of different lengths using a single timer (TIM4) and multiple channels.Current Implementation: I am currently using One-Pulse Mode (OPM). In my existing setup, the pulse starts at CCR and ends at ARR. However, since ARR is a global register for the timer, all channels are constrained to the same end time, making it impossible to achieve independent pulse widths if they all trigger at the same ARR event.Objective: To achieve independent pulse widths, I want the pulse to start at CNT = 0 and end at CNT = CCRx for each channel. This would allow CCR1 and CCR2 to define the lengths independently while sharing the same timer base.The Problem: I am struggling to maintain the correct output state outside of the pulse window (specifically for t<0 and t>ARR). I have attempted to use LL_TIM_OCMODE_FORCED_INACTIVE to keep the pin low before the trigger and then switch to LL_TIM_OCMODE_PWM1 just before enabling the counter
NUCLEO-F411REI have ADC1 to DMA in a circular buffer 4 samples long (ADC_VAL). I then use a TIM1 interrupt to send the contents via UART to a PC. int16_t ADC_VAL[4]; ... HAL_ADC_STart_DMA(&hadc1, (uint32_t *)ADC_VAL, 4); /* TIM1 callback */ void HAL_TIM_periodElapsedCallback(TIM_HandleTypeDef *htim) { HAL_UART_Transmit(&huart2, (uint8_t *)ADC_VAL, 16, 10); } Should I have declared ADC_VAL as a uint32_t ?
ST Community highlights – April to June 2026
Already have an account? Login
No account yet? Create an account
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.