Skip to main content
Visitor II
Feb 20, 2026 2:32 PM UTC
Question

EMIF06-HMC02F2 - Pinout configuration

Hi,

 

In our schematic, the IC’s SD card pin is connected to the controller pin of the STM32H753VIH6, and the IC’s controller pin is connected to the SD card. Could this connection cause any issues during SD card read and write operations? I have attached the schematic for your reference.

 

https://drive.google.com/drive/folders/1fHC0aW8OWq_DrnzWL8WemED_ALq8BC_0?usp=sharing

2 replies

TDK
Feb 20, 2026 2:46 PM UTC

It looks to be symmetric to me. All of those data lines are bi-directional. Should work fine.

Screenshot 2026-02-20 094548.png

"If you feel a post has answered your question, please click ""Accept as Solution""."
FGUIT
ST Employee
Feb 23, 2026 8:39 AM UTC

Hi,

Normal connections of EMIF06-HMC02F2 is:

  • MMCxx pins connected to  STM32H753ViH6 (bumps A4, B4, C3, C4, D3, D4)
  • Others pins connected to MMC card (bumps A1, A2, A3, B1, B2, C1, D1

If I well understood your schematic, it is connected like that, so it's good.

One question: are pull-up resistors inside STM32H753ViH6 disabled (as they are on EMIF06-HMC02F2)? 

Best regards.

Fabrice.