Skip to main content
Associate II
Apr 2, 2025 11:45 AM UTC
Solved

OTA firmware update using W5500

Hii, I want to update the firmware of my STM32H723ZGT6 microcontroller. Here, I want to send firmware file from server to W5500 Wiznet IC then I want that this firmware should load in to the microcontroller flash and it should update the program so can anyone help me with this??

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 2, 2025 12:00 PM UTC

Hello @Aries16 and welcome to the community,

W5500 seems to be a SPI/Ethernet bridge.

If you intend to use the SPI bootloader, you have to take care about the bootloader protocol over the SPI:

mALLEm_0-1743595139164.png

Refer to this application note.

You need to handle the Boot pin and the reset pin of the STM32H7.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

Andrew Neil
Super User
Apr 2, 2025 11:55 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 2, 2025 12:00 PM UTC

Hello @Aries16 and welcome to the community,

W5500 seems to be a SPI/Ethernet bridge.

If you intend to use the SPI bootloader, you have to take care about the bootloader protocol over the SPI:

mALLEm_0-1743595139164.png

Refer to this application note.

You need to handle the Boot pin and the reset pin of the STM32H7.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.