Skip to main content
ÍStef.1
Associate III
August 29, 2024
Question

doubt eeprom

  1. How long do EEPROM memories used in HDDs retain all data at a temperature of 36°C?
  2. EEPROM, like flash, does the number of erases/writes have to do with the data retention time?
  3. 2.5" and 3.5" HDDs use EEPROM or flash to store BIOS/firmware. What type of flash memory do they use? Is it the same type of flash for all HDDs that use this technology?
This topic has been closed for replies.

3 replies

TDK
August 29, 2024

This is about your 8th post on this exact or very similar topic. You're addressing the same people with each post.

doubts chips memory

doubt information of temperature flash Nor in datasheet

doubt memory chip hdd bios

ST M29W640FT 70N6H doubt

Doubt HDDs flash chip for store firmware

media for archival data doubt

Doubt flash memory Nor retention

What recommendation do I follow to avoid losing data retention in NOR flash memory M29W640FT?

 

Manufacturers aren't going to guarantee anything outside of the datasheet, especially on decades old products. Asking repeatedly won't change that, as you've already been told.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ÍStef.1
ÍStef.1Author
Associate III
August 29, 2024

The other topics are about flash and not eeprom, you are very concerned with the topics created and not with the answers

BarryWhit
Lead
August 29, 2024

@ÍStef.1 , TDK is one of the most active users on this forum and has helped many hundreds thousands of people with their issues, for many years, for free. When he tells you that you are violating the norms around here, you should listen.

"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."