WATCH ON-DEMAND | STM32 Summit 2026
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
Most recent activity
Posted on August 31, 2014 at 12:45In our device, we use BLUENRGGCSP module (marking on the chip: BLUENRG AZ 001 P6 TW 4 18) in WLCSP34 package. We also have BlueNRG Eval Kit. In our device and in the Evaluation board, we use the same firmware (bluenrg_6_3_Mode_2-16MHz.img) of the BlueNRG module.Description of the problem: When we try to send any command to the
Posted on June 15, 2016 at 13:15Hi to all, I've created simple dynamic webpages using CGI and SSI provided by the wi-fi module. The pages are stored in the external flash of the SPWF01SA module and it works well. Now I would like to add authentication to the pages by entering a username and password on the first page. There is HTTP with SSL protocol implemented for secure identification of the web server? If not, please give me some guide how can I implement this kind (or any other type) of authentication. Thanks a lot.
Posted on March 23, 2015 at 13:57Hi All, I'm evaluating the SPWF01, so I want to send an Android GCM HTTP post (json or plain text) - but I've no success. I tried it with: AT+S.HTTPPOST=android.googleapis.com,/gcm/send,Content-Type:application/x-www-form-urlencoded;charset=UTF-8&Authorization:key=APIKEY,80 and also with: AT+S.HTTPPOST=android.googleapis.com,/gcm/send,Content-Type:application/json&Authorization:key=APIKEY,80 I got following answer: HTTP/1.0 401 Unauthorized Has anybody an idea or can give me an example how to send the http header via the SPWF AT command? Best regards, Flo #http-post #spwf #gcm
Posted on June 27, 2016 at 13:52Hello!Is there a way to connect to an existing AP without hardcoding the SSID, login credentials etc? For example, using WPS. In the AT command spec there is a Table defining some errors where number 21 has the message ''Cannot use GPIO7. Reserved for WPS feature'' but the meaning is set to ''!!!!Ignore!!!!''. Is this an upcoming feature? Or is there any other way to be able to connect to an arbitrary local AP?Regards,Pontus
Posted on June 28, 2016 at 16:25I am trying to connect my SPWF01S to an AP but am not able to do so. This is the WINDS i get:+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:19:WiFi Join:74:EA:3A:D3:C4:D4+WIND:25:WiFi Association with 'InOutDemo' successful+WIND:40:WiFi Deauthentication:2+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:74:Rejected found Network+WIND:74:Rejected found Network+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:74:Rejected found NetworkAnd this is the config:# Dumping All Configuration Keys:# nv_manuf = ST# nv_model = SPWF01S# nv_serial = value# nv_wifi_macaddr = 00:80:E1:B8:33:20# etf_mode = 0# blink_led = 0# wind_off_low = 0x00000000# wind_off_medium = 0x00000000# wind_off_high = 0x00000000# user_desc = anonymous# escape_seq = at+s.# localecho1 = 0# console1_speed = 115200# console1_hwfc = 0# console1_enabled = 1# console1_de
Posted on July 03, 2016 at 01:55Hello,Kindly advise with the exact discrete balun values in the following document, page7:http://www.st.com/content/ccc/resource/technical/document/application_note/b7/1b/cd/46/3b/a8/46/81/DM00150501.pdf/files/DM00150501.pdf/jcr:content/translations/en.DM00150501.pdfC9, C10, C11, C14, C15, C16,C21, L2, L3, L4Please advise with manufacturing part numbers.Thanks in advance. #bluenrg
Posted on July 01, 2016 at 00:54Hi,I am rather new, although advancing in big steps with through the blueNRG chips, which i find the be really great!I am runing latest FW version, and i noticed something rather strange:If my central device has a random (not public) address, it can only connect to peripheral devices having also random addresses. if i try to create a connection with a public address peripheral, i never get any response from the blueNRG chip after issuing the create connection command.Is this a known issue, or is it normal? Thank you very much,
Posted on June 01, 2016 at 16:45Hello, I tried to delete the characteristics and the service that I created but I didn't succeed. I used the commands aci_gatt_del_char and aci_gatt_del_service but it didn't work. If I understand, I have to give the handlers of the service and/or characteristics as parameters, so I tried to delete them directly after creating them when aci_gatt_add_serv and aci_gatt_add_char give me the handlers. It always answer me 0xFF (timeout). I tried to reset the component before, I tried to delete them at the beginning of the initialization (before creating the service/characteristics) but it's always the same result. Apart of this, I managed to communicate with the BlueNRG. Any help or suggestions would be appreciated. Regards Nicolas
Posted on June 29, 2016 at 14:46Hello, after adding the 6th service with aci_gatt_add_serv i get the errorcode 0x1f (out of memory) if i add the 7th service? This error is independent of the count of characteristics in the other services. How can i increase the possible count of services. I use stack mode 2. #bluenrg-ms
Posted on June 30, 2016 at 07:02Hello!I am using AM26LV31I driver for RS422. The power dissipation is written in datasheet as:Ultra-Low Power Dissipation� dc, 0.3 mW Max� 32 MHz All Channels (No Load), 385 mW TypCan anyone please tell me what is this 385mW power and the power-maximum dissipation ?Any help would be greatly appreciated. #power #am26lv31 #rs422 #uart
Posted on June 09, 2016 at 21:20Hello,I have downloaded the last version of STSW-BLUENRG-DK (2.0.0), unfortunely the executable GUI file is missing. Regards, Christophe.
Posted on June 29, 2016 at 11:51Hi Guys,I would to like develop a bluetotooth application using SPBTLE-RF BLE module. ReadingDT0049 Design tip documents I must to check IFR Register by BLUE NRG GUI, but i can't find this tool. Someone can help me? I have already downloaded BLUE NRG DK 2.0.1 and X- CUBE BLE software package. ThanksMatteo #ifr-blue_nrg_ifr_gui
Posted on June 29, 2016 at 14:00I have a question about possibility of implementation pocsag protocol on Spirit 1. I have eval and SPIRIT1 DK GUI, but there is possible to set maximum preamble to 32 bytes. Pocsag needs 72 bytes preamble. Did you implement pocsag protocol on spirit 1 or is it actually possible?
Posted on June 29, 2016 at 10:44Dear Users, I am trying to communicate between IDS001v4 and ids01a4 using SPIRIT1 DK (IDS001v4) and P2P_Demo (ids01a4). After configuring radio in DK I receive packets, but always occurs ''Packet lost. CRC error''. What could be the reason of such a behavior? Thank you! Pawel #spirit1-ids001v4-ids01a4
Posted on June 17, 2016 at 14:07Dear Community, I am trying to use PRINT macro available in BLE1 examples pack (SensorDemo). Is there a way to turn serial communication with the device, as turning DEBUG definition on doesn't allow any COM output? Thank you, Pawe? #bluenrg-serial-com
Posted on June 28, 2016 at 15:27Hello we are evaluating to use Contiki OS in Spirit1 + STM32 platform. I still have two doubts: 1.- is available OTA (Over The Air) upgrade for the microntroller? 2.- what's the size of the Contiki stack to program in the micro? Thanks in advance.
Posted on June 28, 2016 at 10:00Hello, again. In SPIRIT1 datasheet, in section of synthesizer band, especially for divider value, there are four values, i.e. divide-by-6, by-12, by-16 and by-32. But in File SPIRIT1-Library, which is part of SPIRIT1-DK Software, there is another value, divide-by-8, which give us a band 580-717 MHz. Is it possible SPIRIT1 to work in that Band? And, there are anither three combinatiopns of BS Field of SYNT0 Register - 000,110 and 111. Divide-by-? is on that combinations? Ah, by-the-way, I still wait for answer, for time to compute, AES Encryption. I measure it is about 30-40 us. Is it true? Sincerely: P. Pavlov, Electron consortium JSC, Sofia, Bulgaria
Posted on June 27, 2016 at 10:52Hi All,I am new in BlueNrg but not in developing C and I want to work withNUCLEOF411 and BlueNrg IDB041A1 board. Unfortunately I use Linux and Idon't want to buy IAR system. First step: I tried to download demo (en.x-cube-ble1.zip). I wonder, there is no Makefile in it:(I found .bin and .hex files for demos, I can flash it, and it works well with BlueNrg Android application. Because there is no Makefile, I tried to find some infos and I found Carmine Noviello's site. I can compile and flash the sensordemo based on his tutorial, but it cannot works well. Sometimes it cannot starts:''Program received signal SIGTRAP, Trace/breakpoint trap.0x080015e2 in call_host (arg=0x2000ffac, reason=1) at ../system/include/arm/semihosting.h:8080 asm volatile (''sometimes it can enter on master loop, but it isn't visible for android software. I tried to switch on/off NEW_SERVICES switch too.It is very interesting, the original sensordemo he
Posted on May 26, 2016 at 19:43I am using a STM32F0 mcu that run my application. How can i make a bootloader to my mcu appliccation throw the SPWF01SX.1. I was thinking of downloading throw AT+S.HTTPDFSUPDATE but it is not a secure connection. Did anyone done this? Thanks in advance #bootloader
Posted on January 29, 2016 at 17:41Hi everybody,this is to inform all of you that a new FW for SPWF01Sx, named 3.5, has just been released.It includes new features...:- AT+S.RMPEER- AT+S.HTTPREQ (thanks to Flow forum user)- AT+S.FSR- AT+S.HTTPDFSWRITE (thanks to burton.mark forum user)- etf_mode var- console1_delimiter var (thanks to coghlin.patrick forum user)- dhcp_lease_time var- dns_mode var- use_cgis var- use_ssis var- use_decoder var- wifi_region (thanks to elia.marco.002 forum user)...and bug fixing:- automatic deletion of RAM files with the same name- hidden AP (thanks to Joe forum user)- decoding function to firstset/output_demo (thanks to Flow forum user)- UART overrun (thanks to siebke.georg forum user)It's still not on the website, but you can contact your ST contact/distributor...Feel free to comment.Best regardsjerry
Posted on June 06, 2016 at 21:12HelloI began to work with this module. It is necessary to make a page, at the entrance to which is: 1) Displays the value of several gpio. 2) it was possible to set the several gpio. What code (command) should I place on a page-that-be had made a request to the module?
Posted on June 09, 2016 at 08:03Hi,I'am interfacing SPIRIT RF transceiver and using 50 mhz clock crystal.May i know what all changes have to do to work with 50 Mhz clock?May i know MCU states for 50 MHz clock?(in data sheet i have found only for 52 mhz)Thanks.
Posted on June 06, 2016 at 13:49Hello! The spectrum of the signal in figure 4 or figure 5 (AN4103. Using the SPIRIT1 transceiver under EN 300 220 at 169 MHz) does not correspond to the real measurements. Quick on and off of the transmitter generates a lot of harmonics. The result is a bad signal spectrum. I tried to use the ramp feature but got no result. Tell me how to configure the transmitter, that would not have these outbursts? #rf-spectrum #spirit1
Posted on May 31, 2016 at 00:55Hello guys, i'm new in programming stm32f0. I have stm32f091rc and i want to interface uSD using SPI peripheral. first i used stm32cubemx to select the SPI1 peripheral and configured the clock. then i exported the generated HAL libraries to uVision IDE. but i don't know how to continue.I read that first i need to write i/o driver APIs then link these APIs with FATfsbut i wasn't able to find any example similar to my project (using HAL libraries- uVision and STM32F0)I coded the SPI transmit and receive functions in blocking mode. but what are the other functions to initialize the sd card and check it's status? and how can i use them with SPI and FatFs.Thanks in advance #stm32f0 #spi #stm32 #uvision #usd
Posted on May 31, 2016 at 13:08Hello,I bought some X-NUCLEO-IDS01A4 for evaluation of the SPSGRF-868 module. I am not really pleased with the results. So far the best range I could get was 175 m in the same conditions in which I got 150 m with a competitor's Bluetooth 4.0 module, ie outside with a clear line of sight.I am using the P2P demo software, with reduced datarate and FEC activated. Please see below the configuration pasted from the file spirit1_appli.h :<code>/*************************Uncomment the the protocol to be used****************///#define USE_STack_PROTOCOL#define USE_BASIC_PROTOCOL#if defined(USE_STack_PROTOCOL)#define USE_STack_LLP /*Uncomment if LLP featured need to be used*/#endif/******************************************************************************/#if defined(X_NUCLEO_IDS01A4) #define USE_SPIRIT1_868MHz#elif defined(X_NUCLEO_IDS01A5) #define USE_SPIRIT1_915MHz#else#error SPIR
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.