Skip to main content
moataz
Visitor II
Jul 4, 2016 11:15 AM UTC
Question

Incorrect BOM Values of X-NUCLEO-IDB04A1 BlueNRG Board

Posted on July 04, 2016 at 13:15

Hello Regarding BOM values of:

http://www.st.com/content/ccc/resource/technical/document/bill_of_materials/d7/c0/bb/6b/fd/17/42/16/x-nucleo-idb04a1_bom.pdf/files/x-nucleo-idb04a1_bom.pdf/jcr:content/translations/en.x-nucleo-idb04a1_bom.pdf

L4, the required value is 1.8pF however the part number GRM1555C1H180JZ01 indicates 18pF, which is correct?

C25, the required value is 1.2pF however the part number GRM1555C1H120JZ01 indicates 12pF, which is correct?

Thanks in advance.
This topic has been closed for replies.