Skip to main content
pontus2
Associate II
Jun 27, 2016 11:52 AM UTC
Question

Connecting SPWF01S using WPS

Posted on June 27, 2016 at 13:52

Hello!

Is there a way to connect to an existing AP without hardcoding the SSID, login credentials etc? For example, using WPS. In the AT command spec there is a Table defining some errors where number 21 has the message ''Cannot use GPIO7. Reserved for WPS

 

feature''  but the meaning is set to ''!!!!Ignore!!!!''. Is this an upcoming feature? Or is there any other way to be able to connect to an arbitrary local AP?

Regards,

Pontus
    This topic has been closed for replies.

    1 reply

    Gerardo GALLUCCI
    ST Employee
    Jul 4, 2016 9:21 AM UTC
    Posted on July 04, 2016 at 11:21

    WPS is not part of SPWF01Sx features. You can use miniAP firstset webpage, and fill target AP credentials