Skip to main content
Visitor II
Jan 25, 2026 12:33 AM UTC
Question

Loop inside LL_ATON_RT_RunEpochBlock()

Hi!

I'm new with STM32CubeIDE and STM32N657X0-Q. I'm working with them because of my bachelor's thesis. My model size es 73KB but 432KB because of activations.

The input of my ML is data generated with CMSIS-DSP but I have issues in LL_ATON_RT_RunEpochBlock() line and, I can't see the output.

I've followed these guidelines:

And I have the following code:

LL_ATON_RT_Init_Network(&NN_Instance_Default); // Initialize passed network instance object
 do {
 /* Execute first/next step */
 ll_aton_rt_ret = LL_ATON_RT_RunEpochBlock(&NN_Instance_Default);
 /* Wait for next event */
 if (ll_aton_rt_ret == LL_ATON_RT_WFE) {
 	 timeout++;
 	 if (timeout > 1000000)
 	 {
 		 printf("STUCK IN WFE\n\r");
 		 break;
 	 }
 //LL_ATON_OSAL_WFE();
 }
 } while (ll_aton_rt_ret != LL_ATON_RT_DONE);

The strange part:

The timeout counter never increments because ll_aton_rt_ret == LL_ATON_RT_WFE is never true. It seems like the NPU isn't generating the expected interrupt or the runtime isn't receiving it.

My questions:

  1. Has anyone else experienced this specific issue where LL_ATON_RT_RunEpochBlock() doesn't return WFE?

  2. Could this be related to CACHEAXI initialization? I've seen mentions of this in other threads. But I don't know how to correct this issue, since I don't have enough experience.

  3. Are there specific steps I'm missing in the NPU initialization sequence?

Any guidance would be greatly appreciated. I feel like I'm close but stuck on this final hurdle!

Thanks in advance for your help.

Tags: stm32n6, nucleo-n657x0q, x-cube-ai, npu, ll_aton, inference, wfe, threadx

 

 

 

2 replies

Associate III
Jan 27, 2026 3:58 PM UTC

Hello, I have the exact same issue, have you found a solution yet?

Thanks

Associate III
Jan 28, 2026 4:14 PM UTC

Hello, have you enabled AXISRAM3, 4, 5 and 6? Enable RAMCFG in CubeMX and edit MX_RAMCFG_Init fuction in main.c:

 

/**
 * @brief RAMCFG Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_RAMCFG_Init(void)
{

 /* USER CODE BEGIN RAMCFG_Init 0 */

 /* USER CODE END RAMCFG_Init 0 */

 /* USER CODE BEGIN RAMCFG_Init 1 */
 /* Enable RAMCFG peripheral clock (must be enabled before accessing RAMCFG registers) */
 __HAL_RCC_RAMCFG_CLK_ENABLE();
 
 /* Enable NPU dedicated AXISRAM banks 3, 4, 5, 6 */
 __HAL_RCC_AXISRAM3_MEM_CLK_ENABLE();
 __HAL_RCC_AXISRAM4_MEM_CLK_ENABLE();
 __HAL_RCC_AXISRAM5_MEM_CLK_ENABLE();
 __HAL_RCC_AXISRAM6_MEM_CLK_ENABLE();
 
 /* Power on AXISRAM banks (they are in shutdown by default) */
 RAMCFG_HandleTypeDef hramcfg_temp = {0};
 hramcfg_temp.Instance = RAMCFG_SRAM3_AXI;
 HAL_RAMCFG_EnableAXISRAM(&hramcfg_temp);
 hramcfg_temp.Instance = RAMCFG_SRAM4_AXI;
 HAL_RAMCFG_EnableAXISRAM(&hramcfg_temp);
 hramcfg_temp.Instance = RAMCFG_SRAM5_AXI;
 HAL_RAMCFG_EnableAXISRAM(&hramcfg_temp);
 hramcfg_temp.Instance = RAMCFG_SRAM6_AXI;
 HAL_RAMCFG_EnableAXISRAM(&hramcfg_temp);
 /* USER CODE END RAMCFG_Init 1 */

 /** Initialize RAMCFG SRAM3
 */
 hramcfg_SRAM3.Instance = RAMCFG_SRAM3_AXI;
 if (HAL_RAMCFG_Init(&hramcfg_SRAM3) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initialize RAMCFG SRAM4
 */
 hramcfg_SRAM4.Instance = RAMCFG_SRAM4_AXI;
 if (HAL_RAMCFG_Init(&hramcfg_SRAM4) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initialize RAMCFG SRAM5
 */
 hramcfg_SRAM5.Instance = RAMCFG_SRAM5_AXI;
 if (HAL_RAMCFG_Init(&hramcfg_SRAM5) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initialize RAMCFG SRAM6
 */
 hramcfg_SRAM6.Instance = RAMCFG_SRAM6_AXI;
 if (HAL_RAMCFG_Init(&hramcfg_SRAM6) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN RAMCFG_Init 2 */

 /* USER CODE END RAMCFG_Init 2 */

}

this solved my issue.