Skip to main content
Associate II
Jan 20, 2026 6:00 PM UTC
Solved

How to write a FSBL Application for a custom STM32N6 board

Context : I want to write a FSBL load and run application on a custom minimal PCB based on STM32N6-DK design. The board uses SMPS power supply and not the default power supply of the STM32N6-DK. I follow this original tutorial  as a main example.
 
Problem faced: CubeProgrammer SigningTool version compatibility and header size
 
1) Write a custom external bootloader to write and read external flash memory
  • Modify the power supply parameter (System Core --> RCC --> SupplySource) in CubeMX to `PWR_SMPS_SUPPLY`
  • Generate ExtMemLoader template from CubeMX 
  • Build ExtMemLoader to generate .stldr file
    • make sure the post build script can be executed
    • manually copy the .stldr file generated in `/STM32CubeProgrammer.app/Contents/Resources/bin/ExternalLoader/` if necessary
 
 
2) Modify SigningTool header generation command in FSBL post-build
 
  • Build FSBL & Application following the original tutorial
  • Check heading size, it might be different from the 0x400 that is defined in CubeMX (caused by uninstalling then reinstalling CubeProgrammer thus SigningTool)
  • look for this message *[Header v2.3] Do not align the payload to the 0x400 offset, No padding bytes at the beginning of the payload*
  • Vector Table cannot be located at 0x240 for hardware alignment constraint, therefore it needs to be at 0x400 (following the header)
  • Add `--align` at the end of the SigningTool command to add padding bytes and get a 0x400 header (`STM32_SigningTool_CLI -bin FSBL.bin ... --align`)
  • Then rebuild and make sure header size is 0x400
 
 
3) Program flash and debug
 
  • Select the custom .stldr as External loaders in CubeProgrammer
  • Write trusted.bin files for both FSBL and Application following the original tutorial
  • To use the Debugger in CubeIDE you also need to add the custom .stldr file previously generated in Debug Configurations --> C/C++ Application --> Debugger --> External loaders). Follow the instructions from this tutorial 

 

I hope this short guide will help some of you. Feel free to reach out if you have any question.

Maxime MARCHETTO
Maxime MARCHETTOBest answer
ST Community Manager
Feb 26, 2026 3:03 PM UTC

Hello @cp5900 @,

Thanks for sharing this case and the solution you found. ​

To make this post more visible and easier to find by others who may face the same issue, I mark my reply as the solution. 

 


@cp5900 wrote:
Context : I want to write a FSBL load and run application on a custom minimal PCB based on STM32N6-DK design. The board uses SMPS power supply and not the default power supply of the STM32N6-DK. I follow this original tutorial  as a main example.
 
Problem faced: CubeProgrammer SigningTool version compatibility and header size
 
1) Write a custom external bootloader to write and read external flash memory
  • Modify the power supply parameter (System Core --> RCC --> SupplySource) in CubeMX to `PWR_SMPS_SUPPLY`
  • Generate ExtMemLoader template from CubeMX 
  • Build ExtMemLoader to generate .stldr file
    • make sure the post build script can be executed
    • manually copy the .stldr file generated in `/STM32CubeProgrammer.app/Contents/Resources/bin/ExternalLoader/` if necessary
 
 
2) Modify SigningTool header generation command in FSBL post-build
 
  • Build FSBL & Application following the original tutorial
  • Check heading size, it might be different from the 0x400 that is defined in CubeMX (caused by uninstalling then reinstalling CubeProgrammer thus SigningTool)
  • look for this message *[Header v2.3] Do not align the payload to the 0x400 offset, No padding bytes at the beginning of the payload*
  • Vector Table cannot be located at 0x240 for hardware alignment constraint, therefore it needs to be at 0x400 (following the header)
  • Add `--align` at the end of the SigningTool command to add padding bytes and get a 0x400 header (`STM32_SigningTool_CLI -bin FSBL.bin ... --align`)
  • Then rebuild and make sure header size is 0x400
 
 
3) Program flash and debug
 
  • Select the custom .stldr as External loaders in CubeProgrammer
  • Write trusted.bin files for both FSBL and Application following the original tutorial
  • To use the Debugger in CubeIDE you also need to add the custom .stldr file previously generated in Debug Configurations --> C/C++ Application --> Debugger --> External loaders). Follow the instructions from this tutorial 

 

I hope this short guide will help some of you. Feel free to reach out if you have any question.



Regards,
Maxime

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

3 replies

Julian E.
ST Technical Moderator
Feb 3, 2026 4:15 PM UTC

Hi @cp5900,

 

Thank you very much for sharing, I believe this will be useful for future readers!

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Maxime MARCHETTO
Maxime MARCHETTOBest answer
ST Community Manager
Feb 26, 2026 3:03 PM UTC

Hello @cp5900 @,

Thanks for sharing this case and the solution you found. ​

To make this post more visible and easier to find by others who may face the same issue, I mark my reply as the solution. 

 


@cp5900 wrote:
Context : I want to write a FSBL load and run application on a custom minimal PCB based on STM32N6-DK design. The board uses SMPS power supply and not the default power supply of the STM32N6-DK. I follow this original tutorial  as a main example.
 
Problem faced: CubeProgrammer SigningTool version compatibility and header size
 
1) Write a custom external bootloader to write and read external flash memory
  • Modify the power supply parameter (System Core --> RCC --> SupplySource) in CubeMX to `PWR_SMPS_SUPPLY`
  • Generate ExtMemLoader template from CubeMX 
  • Build ExtMemLoader to generate .stldr file
    • make sure the post build script can be executed
    • manually copy the .stldr file generated in `/STM32CubeProgrammer.app/Contents/Resources/bin/ExternalLoader/` if necessary
 
 
2) Modify SigningTool header generation command in FSBL post-build
 
  • Build FSBL & Application following the original tutorial
  • Check heading size, it might be different from the 0x400 that is defined in CubeMX (caused by uninstalling then reinstalling CubeProgrammer thus SigningTool)
  • look for this message *[Header v2.3] Do not align the payload to the 0x400 offset, No padding bytes at the beginning of the payload*
  • Vector Table cannot be located at 0x240 for hardware alignment constraint, therefore it needs to be at 0x400 (following the header)
  • Add `--align` at the end of the SigningTool command to add padding bytes and get a 0x400 header (`STM32_SigningTool_CLI -bin FSBL.bin ... --align`)
  • Then rebuild and make sure header size is 0x400
 
 
3) Program flash and debug
 
  • Select the custom .stldr as External loaders in CubeProgrammer
  • Write trusted.bin files for both FSBL and Application following the original tutorial
  • To use the Debugger in CubeIDE you also need to add the custom .stldr file previously generated in Debug Configurations --> C/C++ Application --> Debugger --> External loaders). Follow the instructions from this tutorial 

 

I hope this short guide will help some of you. Feel free to reach out if you have any question.



Regards,
Maxime

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
Aug 26, 2026 5:15 PM UTC

thankyou, its too important for me. this problem has already stump me a whole day!  i have never ,never ,never considered this key!!!!!