Get ready for the STM32 Summit 2026 | Online, November 3
Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.
Most recent activity
Posted on February 10, 2016 at 10:46HiWith regard to this device's circuit as shown in fig 2 of the datasheet, should the input be AC coupled or can it directly accept a bi-polar input signal?Ta.
Posted on February 04, 2016 at 13:53Hi,Is the tab or ''slug'' of E-TDA7391PD connected to anything? I'm guessing that it's connected to GND, but I cannot find any information regarding this.On the similar circuit TDA7391LV, it's stated in the datasheet that the ''tab'' of the ''Multiwatt 11'' version is connected to GND, but I don't see any information regarding the ''PowerSO-20'' versions.If it's not connected to GND. Is it okay to connect it to GND?Kind regards,Albin
Posted on January 21, 2016 at 11:46Factor must be consider for choosing the right 1> resolution 2> precision 3> accuracy 4> type of adc using these are factor consider for the choosing right embedded system
Posted on January 07, 2016 at 11:04Hi,I am using STA321MP to record the audio signal, I have observed the noise from its output signal when there is no speech. The period is ~20ms. Do you have any idea where it is from?
Posted on January 07, 2016 at 16:44hi, boys.I bought 100 TDA7297 and ran only 2. I wonder if there might be fakes in the market for this Amp Model , or if there is another version that works with other than the proposed schematic datasheet . Someone has something similar happened ?. The number of the batch of every hundred devices is : SINGAPORE W88030938 . Thanks for the help and comments. #tda7297
Posted on December 15, 2015 at 07:57Hi, Can i use single output only with stereo output provision? for eg: TDA7297 is 2+15W stereo IC, But i want single (mono) out only with 15W, Can i use single channel only? reaming channel should connect or make it floating /open? if open means, Its create any problem. Pls suggest me
Posted on December 15, 2015 at 07:37Hi, We have chosen TDA7266M 7W Mono amplifier for our new project with out Micro controller interface. As per datasheet recommenced test circuit (Figure 3a: Stand-alone Low-cost Application.) i have assembled & test the circuit with common VS & VCC 12V DC and VS5V & VCC12V. but no response of the output speaker (8Ohm 10W). If i missing any thing Please suggest me Thank You
Posted on December 03, 2015 at 10:51Hi, All! Could you please recommend audio amplifiers solution for mono recorder / player with following characteristics: electret micdinamic speaker 0.3W power voltage 3.0Vshutdown possibility is neccessarynot so expensivewill be used with STM32F3 12bit ADC & DAC for recording short voice tags to waypoints Currently I'm looking for TS472 mic preamp and class-D or AB BTL speaker amp. Might is be a better solution? BTW, is it possible to contol TS472 gain by MCU? Or add a limiter?
Posted on November 27, 2015 at 14:42TDA7575B in BOSE car amplifier - needs replacement. HOW?
Posted on November 08, 2015 at 19:24Anyone heard about a ST IC with the name 07502233?It sits in a Bosch Charger with a LM324AN beside it. Both are STMicroelectronics. But I can't find what type the 07502233 IC are! Any that know and can tell if it's possible to get it online?
Posted on November 03, 2015 at 17:13We have an extra op amp in the quad package that we'd like to use as a comparator to save cost. Any recommendations? I'm a little concerned about stability and oscillations.
Posted on October 19, 2015 at 18:30Hi, I'm looking for a class AB amplifier with integrated DAC and I2S bus and I found STm TDA7801. I'm a teacher and I would like to use this device at school for some projects. Unfortunately, I have no sufficient ability and time in order to design a board for this integrated circuit. So my question is if there is an evaluation board that I can exploit to use such amplifier. I made a lot of search on the web without finding it. Otherwise, how can I do in order to use it and avoiding to design the board by myself? Thank you Salvatore #tda7801 #dac #i2s #amplifier-ab
Posted on September 24, 2015 at 16:06Hi! STA309a documentation is little bit lacking on this topic, so some explanation is needed. Required configuration: Single stereo I2S input on SDI12 Two I2S outputs: stereo to main speakers and mono to subwoofer Questions: 1. What is the correct output I2S mapping: SDO12 to main speakers and SDO56 to subwoofer (right or left)? 2. Can you tell if the following configuration is correct? AMBMME and AMBMXE bits enabled (bass mix and crossover) CSS and RSS set to 10 (off) SUB enabled FSS and XO bits sets according to speaker configuration Thanks! #sta309a
Posted on July 17, 2015 at 23:24Hello,I'm setting up a system with a STA309A DSP and a STA510A amplifier.I'm expecting to connect two 8Ω loads with a maximum power of 50W each, but I can't find the graphics that show the estimated Power dissipation and the THD that I can expect at that level. The datasheet for other parts like the STA518A do have figures that allow me to calculate that. Is there an application note that describes how to calculate the required power supply for a specific power output?
Posted on September 28, 2015 at 20:32I am trying to use one I2S input and send out L/R stereo as standard class-D PWMs and output the subwoofer at line level. My confusion arises with properly setting up the cross-over and how to use the DDX Headphone output to create a line level signal. What configuration would you recommend to achieve this? Is there a way to switch between two different I2S inputs like a A/B selector in this configuration? #audio-processing #sta309a
Posted on October 02, 2015 at 08:32Dynamic Microphone preamp for differential output TS472
Posted on September 04, 2015 at 23:14Hi, I'm using STA369BWS as the amplifiers in my application. There are a pair of stereo speakers and a subwoofer speaker. The stereo speakers' resistance is 4 OHM, and the subwoofer one is 8 OHM. I'm using two STA369BWS to drive the stereo speakers in the stereo BTL mode, and the subwoofer in mono BTL mode. My power supply is 14~18V. The reference configuration in the datasheet for a stereo BTL mode is for a 8 OHM speaker, not 4 OHM. Can someone recommend the output configurations for my application? Thanks. #class-d-sta369bws-configurations
Posted on August 28, 2015 at 15:47Hello,I am developing new device with TDA7576B amplifier. TDA7576 input voltage -0.3 to 5V (from absolute maximum ratings). Is it rms value or input signal voltage must be positive only? I need computer line out signal to drive TDA7576B. Line out signal output voltage is 0.316 rms. Can I put line out signal to TDA7576B input directly?
Posted on August 27, 2015 at 09:31A amplifier system:ADC+STA339BW+MCU,MCU generate a 12MHz clock apply to ADC(connect to MCLK pin) and STA339BW(connect to XTI pin)。I don't know how many differences will be,will this effect THD+N,SNR? is there any document about this issue? thanks
Posted on July 11, 2015 at 09:29Dear Forum members, In one of my application, I need to drive photo LED of IL300 through TLO64. But it is not working. If I just replace TLO64 with TLO74, everything works proper. My initial guess was that TLO64 might not be supplying sufficient current. But looking at datasheet, I didn't find any major deviation in output current graph of both these IC's. Am I missing something?
Posted on July 10, 2015 at 09:08Hi!I'm new in this world and it's posible that my questions are not the most intelligent. I'm designing an array of loudspeakers and i have thought to use the TDA7264 amplifier, but i have some questions:· For the power supply, Should i consider the music power parameter?· If I'm going to use 8 TDA7264, Could I use only one standby/mute circuit for all devices (datasheet Figure 12)? Thanks!
Posted on June 23, 2015 at 00:48Hi, How can I configure the ST369 in a clipping mode. In the datasheet I found the configuration for: - Anti-clipping mode - Dynamic range compressing mode. Does there exists a configuration to switch-off both modes? Thanks in advance, Christiaan #sta369bw #clipping-mode
Posted on May 13, 2015 at 20:08Hi,Please suggest a method to design 6-channel audio mixer using STA309A. 6 Bluetooth devices will be interfaced to the SDI inputs of the mixer and the 6 mixed outputs will be given to the BT modules through SDO.Thanks and Regards,Manesh
Posted on May 14, 2015 at 23:54Is there an example configuration that gives the same results as the video in ''Directional Sound Capturing with ST MEMS microphones and Smart Voice processors'' ?I am curious how the microphone signal delay was applied, I don't see that available to me in APWorkbench.
Posted on May 11, 2015 at 02:41The TDA7391 (http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/CD00000162.pdf) has two pins that are named MUTE and SYNC. SYNC is supposed to be connected to ground through a resistor (named R2), and MUTE is supposed to be connected to a capacitor (named C3). The datasheet notes that: ''The values of C3 and R2 determine the time required to bias the amplifier.''The datasheet has an example circuit (Figure 3 in the datasheet) which shows R2 as 56 kOhm and C3 as 33 F. I think that last number must be a typo.Does anyone know what a good value for C3 is? Does anyone know how exactly the values of C3 and R2 determine the time required to bias the amplifier? Is it just the RC time?For what it's worth, the http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00051686.pdf (a similar device) has a R2 of 220 kOhm and a C3 of 2.2 uF in its example circuit.
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.