Skip to main content
panneerrajan_g
Associate
December 15, 2015
Question

Can i use 1CH. audio out with stereo provision IC ?

Posted on December 15, 2015 at 07:57

Hi,

Can i use single output only with stereo output provision?

for eg:

TDA7297 is 2+15W stereo IC,  But i want single (mono) out only with 15W,

Can i use single channel only?

reaming channel should connect or make it floating /open?

if open means, Its create any problem. Pls suggest me
This topic has been closed for replies.

2 replies

Nickname1623_O
Visitor II
December 15, 2015
Posted on December 15, 2015 at 08:23

hi Panneerr,

of course , you can just use one amplifier of stereo amplifier .

and you should connected non-used channel input coupling cap to ground  to avoid resonance .

by the way , due to non-used channel are in active status , so power dissipation will higher than mono amplifier IC .

Thanks ,

YT

panneerrajan_g
Associate
December 17, 2015
Posted on December 17, 2015 at 07:02

Hi Yun Tao,

Thank you,

Coupling capacitor require any specified value for unused input channel connect to ground.

can i connect 0.1uF 25V ceramic disc capacitor?

Pls. suggest