Excess Current Consumption Running B-L072Z-LRWAN1 From Battery??
Posted on December 11, 2017 at 20:21
I have removed all the solder bridges & links to minimise stray consumption.
When I measure the combined current through JP3 and JP1 (ie, MCU & RF), it is ~0.87mA between Tx pulses.

(SB19,14,17 are removed; JP2 is not fitted - so no current to USB_LRA)
But, when I power the board from the battery, and measure the battery current, I see
1.95mA

(SB18 is removed)
The ST LD39050 regulator (U7) is supposed to be ''low quiescent current'': the datasheet says it should only, typically, be taking 100uA at 500mA load - so we should be nowhere near that!
So where is this extra milliamp going??
EDIT
To clarify: the ~0.87mA to MCU & RF is measured while powered from the battery.
#current-consumption #b-l072z-lrwan1 #low-power #current
Note: this post was migrated and contained many threaded conversations, some content may be missing.