Skip to main content
Andrew Neil
Super User
May 10, 2022
Solved

Restore ST-Link Connection on B-L072Z-LRWAN1

  • May 10, 2022
  • 1 reply
  • 1976 views

In order to achieve minimum power drain on the B-L072Z-LRWAN1 discovery board, it is necessary to remove some solder bridges

See:

https://community.st.com/s/question/0D50X00009XkbSOSAZ/excess-current-consumption-running-bl072zlrwan1-from-battery

And:

https://community.st.com/s/question/0D50X00009q4M1zSAE/cant-power-bl072zlrwan1-with-battery

To be able to use the onboard ST-Link again, these connections need to be restored:

  • NRST: link CN4.3 to CN12.5;
  • SWD: fit two links on CN8;
  • VCOM: link CN5.1,2 to JP6.

0693W00000NpgutQAB.jpg 

Rather than have to mess about with 2 separate links for the SWD, a single-row 4-pin header can be adapted:

0693W00000Npgv3QAB.jpg

This topic has been closed for replies.
Best answer by Andrew Neil

It wasn't a question - just posting a tip.

1 reply

Andrew Neil
Andrew NeilAuthorBest answer
Super User
May 10, 2022

It wasn't a question - just posting a tip.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.