2015-03-24 10:38 AM
I have been working on setting up my MCU as a VCP CDC Device using STM32Cube for the past few days. I have studied the STM32Cube USB device library User Manual (UM1734) and have followed the steps outlined in part 7.5.6 which calls on my application to call the function USBD_CDC_Init().
void MX_USB_DEVICE_Init( void ) { /* Init Device Library,Add Supported Class and Start the library*/ USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS); USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC); USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS); USBD_Start(&hUsbDeviceFS); // USBD_CDC_Init called here hUsbDeviceFS.pClass->Init(&hUsbDeviceFS, DEVICE_FS); } I have changed the value of CDC_DATA_HS_MAX_PACKET_SIZE to 256 in usbd_cdc.h as detailed in this [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/USB%20CDC%20Bug%20in%20CubeMX%20firmware&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx¤tviews=3282]post to ensure that my device data packet size is 64 bytes. #define CDC_DATA_HS_MAX_PACKET_SIZE 256 /* Endpoint IN & OUT Packet size */ I have also ensured that my heap size is changed to the minimum recommended by ST support in another post on this forum, in my .ld file _Min_Heap_Size = 0x0400; /* required amount of heap */ _Min_Stack_Size = 0x0400; /* required amount of stack */ The problem is if I call the function USBD_CDC_Init() the MCU controller is listed as an UnKnown Device by Windows and stopped. If I comment out the call, my MCU is correctly recognised and configured as a VCP device in both Windows and Linux but all subsequent calls to USBD_CDC_SetTxBuffer will fail (HardFaultHandler is called) because the pClassData field of the USB Device handler is never initialized. I am caught between the devil and the deep blue sea, how do I proceeed? I am using a STM32f302k8 and STM32CubeMX version 4.6.0 with FW version 1.1.1 for STM32F3. #usb #usb #usb #stm32 #stm32 #stm32f4 #usb #discovery #stm32f32015-03-24 4:08 PM
static USBD_WHATEVER_HandleTypeDef hWhatever;
<
snip
>
pdev->pClassData = hWhatever;//USBD_malloc(sizeof (USBD_WHATEVER_HandleTypeDef));
2015-03-25 3:29 AM
Thank you for your reply Conor, I am actually using a static allocate, I've checked and it returns the desired memory:
/**
* @brief static single allocation
* @param size: size of allocated memory
* @retval None
*/
void
* USBD_static_malloc(uint32_t size)
{
static
uint32_t mem[
sizeof
(USBD_CDC_HandleTypeDef)];
return
mem;
}
2015-03-25 1:51 PM
I had similar problem
when I
started
to try
USB
CDCand
STM32
CubeMX. Don't call USBD_CDC_Init(), this function is called automatically during enumeration or virtual COMport opening.
I have problem if I start of sending of data before enumeration and port opening. I found solution on other forum, it isnecessary to have
any status information.I
did not find
anything like this in
HAL
library
. I added variable u8_cdc_initialized to CDC_Init_FS(void) and CDC_DeInit_FS(void).static int8_t CDC_Init_FS(void)
{
hUsbDevice_0 = &hUsbDeviceFS;
/* USER CODE BEGIN 3 */
/* Set Application Buffers */
USBD_CDC_SetTxBuffer(hUsbDevice_0, UserTxBufferFS, 0);
USBD_CDC_SetRxBuffer(hUsbDevice_0, UserRxBufferFS);
u8_cdc_initialized = 1;
return (USBD_OK);
/* USER CODE END 3 */
}
static int8_t CDC_DeInit_FS(void)
{
/* USER CODE BEGIN 4 */
u8_cdc_initialized = 0;
return (USBD_OK);
/* USER CODE END 4 */
}
All
function calls
of CDC_Transmit_FS()must
be conditional
:if (u8_cdc_initialized)
{
u8_buff[0] = 'c';
CDC_Transmit_FS(u8_buff, 1);
}
2015-03-26 3:13 AM
I thought that's what was supposed to happen ie. USBD_CDC_Init() being called automatically but if I don't call it explicitly, it never is which as I detailed above causes the device handlers pClassData field to never be initialized (see screenshot) and all calls to USBD_CDC_SetTxBuffer to fail.
I tried your method but again if I don't explicitly call USBD_CDC_Init(), CDC_Init_FS() will also never be called, leavingu8_cdc_initialized = 0. I am at a wits end, please help me.
________________
Attachments : PClassData_NULL.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzFJ&d=%2Fa%2F0X0000000bM9%2FF6.fOeR1tZAJsORVlF6SpLT2_5eoCQ_f7Bv_5i_gd8w&asPdf=false
2015-03-30 7:37 AM
Thank you Petr!!! You were right, my code was trying to send data before the port had been opened.
I realised during the weekend that I would never be able to see the initialization of u8_cdc_initialized whilst the MCU was connected to the debugger, which is why I had initially said your solution was not working for me. The solution I found was to disconnect and reconnect the MCU and read the output from the terminal, and I can see my data being sent from the MCU after a slight pause where the port is being opened. Do you have the link to the forum you read this on? It sounds more informative than ST's own documentation which actually told me to call USBD_CDC_Init() [Page 52 Part 7.5.6 of User manual UM1734] which cost me three days of debugging! Thank you so much for your help. Let me now try and create a protocol for my application.2015-04-15 11:44 AM
Please see project file attached for reference.
________________ Attachments : UsbDeviceCDC.7z : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzSa&d=%2Fa%2F0X0000000bM8%2FG_hFr7D.qepzLOZUBKzrXwOz9zLmk5lhAsq_3z6FtZo&asPdf=false2016-09-09 6:55 AM
I'm trying to set up a VCP on my stm32f4 discovery board and I'm also using CubeMX. I have implemented a status check variable like you suggested but I still get the same error even when I don't try to send anything, debug or regular execution. I read on device manager:
''Unknown USB Device (Device Descriptor Request Failed)Windows has stopped this device because it has reported problems. (Code 43)A request for the USB device descriptor failed.''2016-09-09 9:31 AM
Hi,
Are you using ST-Link with Windows 10? In this case, try with compatibility mode for windows 8 option.Regards2016-09-12 6:43 AM
Yes I'm using windows 10 and already changed compatibility mode and updated corresponding VCP drivers from ST but it didn't help. I also switched between IDEs (MDK4 and TrueStudio) but didn't change anything either. Help!!