cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX v4.19.0: Can't Find Nucleo-F767ZI

phroggie
Associate II
Posted on January 27, 2017 at 05:03

So I just installed v4.19.0 and now at the Nucleo-F767ZI is missing from the Boards List. (Just F746ZG and F722ZE are  there.) Prior to the install it was there and kinda worked but now it's not on the list.

What am I doing wrong?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Jeanne Joly
Senior III
Posted on January 30, 2017 at 11:08

Hello

Lemberg.Roger

and

Nicolas.HILAIRE

,

Just for your information, if you want to work with F767ZITx board before the next CubeMX release(CubeMx 4.20), the workaround is as follow :

Change in

A_ST_Nucleo144BoardsList.pdsc, this part of code :

<mountedDevice Dname='STM32F767ZITx ' Dvendor='STMicroelectronics:13' deviceIndex='0'/>

by this one :

<mountedDevice Dname='STM32F767ZITx' Dvendor='STMicroelectronics:13' deviceIndex='0'/>

(no space at the end of the Dname).

BR

Eric

View solution in original post

7 REPLIES 7
Khouloud GARSI
ST Employee
Posted on January 27, 2017 at 07:52

Hello

Lemberg.Roger

,

I will share internally your feedback for further review and we will keep you posted about the taken actions/explanation if needed.

Thank you for your contribution and we apologize for the

inconvenience this may cause.

Khouloud.

Nicolas HILAIRE
Associate II
Posted on January 27, 2017 at 11:44

I have the same issue.

I have that the board is described in the database but doesn't appear under the software

<board name='NUCLEO-F767ZI' orderForm='

https://community.st.com/external-link.jspa?url=https%3A%2F%2Fmy.st.com%2Fesample%2Fapp%3Fpage%3Dbasket%26amp%3Bpn%3DNUCLEO-F767ZI

' revision='Rev.B'

salesContact='

https://community.st.com/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fstonline%2Fcontactus%2Fcontacts%2Findex.php

' vendor='STMicroelectronics'

mxFile='boards/A71_Nucleo_NUCLEO-F767ZI_STM32F767ZI_Board.ioc'

ARMmbed=''

type='Nucleo144'>

<description>STMicroelectronics NUCLEO-F767ZI Board Support and Examples</description>

<image large='images/nucleo_144_large.jpg' small='images/nucleo_144_small.jpg'/>

<book category='overview' name='

https://community.st.com/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fevaluation-tools%2Fproduct-evaluation-tools%2Fmcu-eval-tools%2Fstm32-mcu-eval-tools%2Fstm32-mcu-nucleo%2Fnucleo-f767zi.html

' title='Nucleo STM32 F7 series development board'/>

<book category='manual' name='

https://community.st.com/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fuser_manual%2Fgroup0%2F26%2F49%2F90%2F2e%2F33%2F0d%2F4a%2Fda%2FDM00244518%2Ffiles%2FDM00244518.pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.DM00244518.pdf

' title='User Manual'/>

<mountedDevice Dname='STM32F767ZITx ' Dvendor='STMicroelectronics:13' deviceIndex='0'/>

<compatibleDevice DsubFamily='STM32F767' Dvendor='STMicroelectronics:13' deviceIndex='0'/>

<feature n='1' name='On-board ST-LINK/V2-1' type='ODbg'/>

<feature n='4' name='USB VBUS, ext. VIN, ext. 5V, ext +3.3V' type='PWR'/>

<feature n='1' name='10/100M Ethernet interface with external PHY (LAN8742A-CZ-TR)' type='ETH'/>

<feature n='1' name='USB FS (Full speed) with micro-AB Connector' type='USB'/>

<feature n='76' name='STMicroelectronics Morpho connector : (2 x 72)' type='DIO'/>

<feature n='32' name='STMicroelectronics Zio (Arduino connector)' type='DIO'/>

<feature n='2' u='1' name='Push-buttons: User and Reset' type='Button'/>

<feature n='3' u='1' name='LEDs: COM, Power, User LEDs' type='LED'/>

<debugInterface adapter='ST-Link' connector='Mini-USB'/>

</board>

But in the model there is a path to the empty model.

I took this file and save this model as my working copy.

My path is : C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\db\plugins\boardmanager\boards/A71_Nucleo_NUCLEO-F767ZI_STM32F767ZI_Board.ioc

I haven't finish my tests but it seems to be okay.

Hope it can help

Khouloud GARSI
ST Employee
Posted on January 27, 2017 at 14:06

Hello

Lemberg.Roger

/

lgm42

,

The issue is confirmed

using STM32CUBEMX 4. and will be

resolved and delivered in the next CubeMX release (CubeMX4.20).

Sorry for any inconvenience this may have caused.

Khouloud

Posted on January 27, 2017 at 16:42

Thank you so much, Nicolas.

However I'm missing something from your solution.

I found the code you outlined in the A_ST_Nucleo144BoardsList.pdsc file. The <board> element for the F767ZI board corresponds to the one for the F746ZG (for instance) and their mxFile attributes reference similar .ioc files in the boards folder (which it refers to with a relative path), both of which are present.

Was your solution to change that to an absolute path?

Peace 

Posted on January 28, 2017 at 15:14

No when I saw the model file (.ioc), I just open it and save it under my working copy.

I'm not creating project from scratch be from their ico file.

For my board there is two files : 

A71_Nucleo_NUCLEO-F767ZI_STM32F767ZI_Board.ioc

A71_Nucleo_NUCLEO-F767ZI_STM32F767ZI_Board_all config.ioc (or something like that)

Take the second because all IP have already been configured.

After some tests it works perfectly.

Jeanne Joly
Senior III
Posted on January 30, 2017 at 11:08

Hello

Lemberg.Roger

and

Nicolas.HILAIRE

,

Just for your information, if you want to work with F767ZITx board before the next CubeMX release(CubeMx 4.20), the workaround is as follow :

Change in

A_ST_Nucleo144BoardsList.pdsc, this part of code :

<mountedDevice Dname='STM32F767ZITx ' Dvendor='STMicroelectronics:13' deviceIndex='0'/>

by this one :

<mountedDevice Dname='STM32F767ZITx' Dvendor='STMicroelectronics:13' deviceIndex='0'/>

(no space at the end of the Dname).

BR

Eric

Posted on January 31, 2017 at 01:57

The workaround works like a charm.

Thanks Eric and to everyone else who helped out!!!!!!!