cancel
Showing results for 
Search instead for 
Did you mean: 

Migrating from the SPWF01Sx to the SPWF04Sx

steve239955_stm1_st
Associate II
Posted on June 28, 2017 at 17:20

Hello,

We're trying to migrate a board from the SPWF01SC to the SPWF04SC. Two of the additions to the SPWF04 are the LSE and HSE external clock pins. They're not displayed on the block diagram for the SPWF04 in its datasheet so does it use the STM32F429's internal RC oscillator by default or do we need to add oscillators to our board as per the X-NUCLEO-IDW04A1 evaluation board?

Thanks,

Steve

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Gerardo GALLUCCI
ST Employee
Posted on June 29, 2017 at 12:23

Hi Steve,

you can ignore HSE and LSE pins. Leave floating. Module uses STM32's internal oscillators.

You can migrate without HW efforts. Only pay attention to I/O levels (from 2v5 to 3v3)

Ciao

jerry

View solution in original post

2 REPLIES 2
Gerardo GALLUCCI
ST Employee
Posted on June 29, 2017 at 12:23

Hi Steve,

you can ignore HSE and LSE pins. Leave floating. Module uses STM32's internal oscillators.

You can migrate without HW efforts. Only pay attention to I/O levels (from 2v5 to 3v3)

Ciao

jerry

Posted on June 29, 2017 at 13:11

Hi Jerry,

Thanks for your quick response; a colleague had the evaluation board and I only noticed this morning that they're not populated on the IDW04 board!

Cheers,

Steve