cancel
Showing results for 
Search instead for 
Did you mean: 

www.st.com

Damien G.
ST Employee
Posted on May 23, 2018 at 09:12

ST25 SDK v1.2.0 available online

Hello,

http://www.st.com/content/st_com/en/products/embedded-software/st25-nfc-rfid-software/stsw-st25sdk001.html

of the Java ST25 SDK

http://www.st.com/content/st_com/en/products/embedded-software/st25-nfc-rfid-software/stsw-st25sdk001.html

.

New content include:

  • st25sdk.jar

    API changes:

    - TagHelper.identifyTypeVProduct() and TagHelper.identifyType4Product() can now throw the TAG_NOT_IN_THE_FIELD STException

    if the tag was moved out of the RF field in the middle of the discovery process.

    - ST25DVTag.readMailboxMessage and ST25DVTag.fastReadMailboxMessage return a status byte before the data when requested read size = 1.

    New Features:

    - Support for ST25TV02K tag with EAS and tamper detect features.

    - Other features such as digital signature and untraceable mode are available under NDA. Please contact ST.

    - Support for ST25DV-W1 and ST25DV-W2 dynamic tags with PWM output

    - New About class created to return the st25sdk library version + the list of extra features (available in NDA versions)

    - New STException MISSING_LIBRARY used when building an application with the SDK without the proper dependencies.

    Changes and improvements:

    - Added writeCCFile(byte[] buffer) to CCFileInterface.

    - NDEF WifiRecord can now handle all the possible authentication and encryption types

    Bug fixes:

    - Removed limitations of ST25DVTag.readMailboxMessage and ST25DVTag.fastReadMailboxMessage when asking for a single byte of data.

    Now no exception is sent + the status byte is returned before the data byte, to be coherent with the values returned for other sizes.

    - Added space between first name and last name values of the vCARD's [N]ame field
  • Reader libraries

    FEIG readers:

    - Updated transceive implementation to return response for ST25TV and ST25DV-W commands

    - Added method to set the response length before any command

    - Adjusted FEIG readers transmit/receive length parameters

    ST readers:

    - Fixed toggling PCB for Type 4 anti-collision sequence

    - Corrected JNI crash on reconnect

#st25sdk
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0