Skip to main content
Associate
Aug 27, 2025 5:37 AM UTC
Solved

Is STM8 recomended for beginners?

I have experience with PIC and AVR microcontrollers, but they lack the good debug features of the STM8 series. Furthermore, these microcontrollers aren't cheap. While looking for simple and inexpensive chips, I keep coming across the STM8 series.

Mastering a new microcontroller takes time. I'm confused about learning the STM8 because STMicroelectronics is recommending their STM32 series, which uses the ARM Cortex-M core. This recommendation makes me wonder if investing time in the STM8 is a good idea, or if it would be better to learn the more widely-supported and future-proof STM32 family.

 

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Aug 27, 2025 6:02 AM UTC

    Welcome @rabbi141, to the community!

    The STM8 and their tools are already very old, all date from the last millennium and are actually only useful for projects that are already running.

    In fact, the STM32 mentioned are the much more modern MCUs, where you can look at one of the STM32C0 for simple applications, for example.

    A warning in passing: questions regularly arise here in the community about so-called Blue Pill boards not working as desired. For years, only incompatible clones have been used for these products from Asian manufacturers.

    If you want to start with a ready-made and 100% functional and supported board, I recommend one of the NUCLEO boards, e.g. a nice and cosy NUCLEO-32, each of which also contains an ST-LINK debugger.

    Hope this helps?

    Good luck
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    30 replies

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Aug 27, 2025 6:02 AM UTC

    Welcome @rabbi141, to the community!

    The STM8 and their tools are already very old, all date from the last millennium and are actually only useful for projects that are already running.

    In fact, the STM32 mentioned are the much more modern MCUs, where you can look at one of the STM32C0 for simple applications, for example.

    A warning in passing: questions regularly arise here in the community about so-called Blue Pill boards not working as desired. For years, only incompatible clones have been used for these products from Asian manufacturers.

    If you want to start with a ready-made and 100% functional and supported board, I recommend one of the NUCLEO boards, e.g. a nice and cosy NUCLEO-32, each of which also contains an ST-LINK debugger.

    Hope this helps?

    Good luck
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Graduate
    Dec 7, 2025 11:55 AM UTC

    I don’t agree with you that you should switch to STM32 just because it’s modern. The fact is that I have a simple task: to use 1 pin to read an analogue signal, 2 pins to read digital signals, and 1 pin to write a digital signal. Therefore, I don’t see the point in overpaying $1 for STM32, which is 3 times larger than STM8 (if we compare the blue pill), and in which more than half of the pins will remain free. But to solve such a simple task, I didn’t even find an example of working with an ADC without interruptions in PlatformIO  and SPL examples. I spent 2 weeks of my precious time trying to program STM8 using AI, and it was a waste of time. Therefore, I’m returning to Arduino Mini Pro, where I have a lot of experience. And by the way, I will continue to look for cheap Chinese microcontrollers for simple tasks that will have good support and programming documentation. STM32 is a great solution for more complex tasks, but you need to have a solution for simpler tasks or delete the entire database and references to what you once had and could not bring to perfection.

    Graduate
    Jan 4, 2026 8:45 PM UTC

    Additionally, I've found more easier way to STM8 programming in sduino.

    Because I like the Linux OS.

    Explorer II
    Oct 31, 2025 10:53 AM UTC

    In my opinion. I would say that investing your time and effort for the STM8 is a great idea. here's why:

     

    The STM8 not use a specific core like his brother STM32. he use the classic CISC architecture making your journey of understanding it is worth it. I also use the STM8, specifically STM8L101K3T3. beside CISC architecture there are RISC architecture. both have their pros and cons. but it all the same. we all know the technology growth so fast past few years. to undertand all register of STM32N657X0 is absolutely amazing but to build fundamental concept is also essential is more preferable. it all build with transistor. i bit data is stored using some gate called latch. continue to combine them you get memory. "the computer has no standard". "if there's 100 company there will be 101 different architecture". all that is positive. keep up the good work @rabbi141 and STMicroelectronics!

    Andrew Neil
    Super User
    Oct 31, 2025 11:05 AM UTC

    @haimanTheSTM8 wrote:

    The STM8 not use a specific core like his brother STM32. 


    What do you mean by that?

    Of course it is a specific core - also a proprietary one.

     


    @haimanTheSTM8 wrote:

    "the computer has no standard". "if there's 100 company there will be 101 different architecture". 


    That, surely, is an advantage for STM32 - instead of yet another proprietary architecture (like STM8), it uses the industry-standard Cortex-M.

    Apart from the hardware, there's also the tools to consider.

    This recent example suggests that the tooling is not up to modern standards.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    Oct 31, 2025 11:20 AM UTC

    As we're waking up this old thread ...

     


    @rabbi141 wrote:

    I have experience with ... AVR microcontrollers, but they lack the good debug features of the STM8 series.


    Not sure that you mean by that?

    AVRs certainly have good on-chip debug ...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    whitehorsesoft
    Associate III
    Nov 25, 2025 7:43 PM UTC

    I'll throw in a comment on this old thread. My opinion: for anything other than hobby/training projects, STM8 will only have price / power profiles in its favor. It will be more difficult to spin up projects with, find documentation for, and collaborate with on a team.

    And, since you mentioned debug features, it's very hard to beat the step/breakpoint experience that comes with STM32 chips and STM32CubeIDE.

    But for a hobby/training project, I would recommend STM8 for the "bare metal" experience. Meaning, assembly programming and actually using the ISA. You can carry around most of the instructions in your head, and in my opinion the assembly is cleaner than corresponding C syntax. You won't be using complex procedures, there's simply no room for it. You're forced to be simple, but that's part of the beauty. If it sounds interesting, I'd especially recommend https://shop-pdp.net/ashtml/asmblr.htm, verified it works with STM8S003.

    Andrew Neil
    Super User
    Nov 26, 2025 9:50 AM UTC

    @whitehorsesoft wrote:

     It will be more difficult to spin up projects with, find documentation for, and collaborate with on a team.


    I think that's probably right.

    So, in that light, I don't follow the reasoning here:


    @whitehorsesoft wrote:

    But for a hobby/training project, I would recommend STM8 for the "bare metal" experience. .


    Surely, something like AVR would be more appropriate here - as it has far wider support ?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    whitehorsesoft
    Associate III
    Dec 9, 2025 1:04 PM UTC

    So, in that light, I don't follow the reasoning here:

    @whitehorsesoft wrote:

    But for a hobby/training project, I would recommend STM8 for the "bare metal" experience. .


    Surely, something like AVR would be more appropriate here - as it has far wider support ?


    That may be. Sorry, I was thinking in scope of ST products.

    Philipp Krause
    Senior II
    Dec 16, 2025 7:47 AM UTC

    Both the STM32 and the STM8 have good support in current FOSS tools. For the STM32, the FOSS toolchain is based around the GCC or clang compilers, for STM8 around the SDCC compiler.

    While the non-free Cosmic/IAR/Raisonance have been stagnating, SDCC keeps improving, including support for current and future C standards, and improved optimizations (to a lesser degree - after all the code generated by SDCC is already quite good).

    A comparison of compilers targeting the STM8 from 2024: http://www.colecovision.eu/stm8/compilers.shtml

     

    Andrew Neil
    Super User
    Dec 16, 2025 10:46 AM UTC

    Well, that's just compilers - what about other tools ... ?

     

    Remembering that the specific audience here is beginners.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Philipp Krause
    Senior II
    Dec 16, 2025 10:52 AM UTC

    Depends on what tools they are looking for, and what kind of beginner they are.

    E.g. a beginner to STM8 that has worked with IAR before likely would prefer the IAR suite for STM8. A beginner to STM8 that previously used GCC with Code::Blocks or Visual Studio would likely prefer to use SDCC with Code::Blocks or Visual Studio.

     

    P.S.: OP stated previous experience with PIC and AVR. PIC is likely SDCC (older 8-bit ones) or GCC (newer ARM-based ones) or XC8. AVR is most likely GCC or XC8. SDCC should be relatively easy to get started with for someone with GCC experience. Also, someone with IAR or GCC experience would likely feel limited by the gaps in C standard support in the Cosmic and Raisonance compilers.

     

    P.S.: Earlier I had made a mistake here, an listed Keil, which was wrong; my edit to fixy it apparently overlapped with a reply stating that I was wrong, so the reply below stating that I wam wrong is correct and fixed a mistake in an earlier version of the P.S. text above.

    Andrew Neil
    Super User
    Dec 17, 2025 12:54 PM UTC

    On the state of STM8 tool support: 

    https://community.st.com/t5/stm8-mcus/st-visual-develop-updates/td-p/763922

    "the outdated IDE creates unnecessary barriers for beginners, often discouraging them early in the learning process"

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Graduate II
    Dec 17, 2025 1:14 PM UTC
    Unfortunately, ST has not updated STVD for a long time. Which is scandalous. Works fine with windows 7, W10 64bit I failed to install. To solve these problems I have on virtualbox W7 STD and STVP, on top of that on linux Ubuntu. STVD with the Cosmic compiler works well, although it has its whims. STVP without problems, but not at the same time with STVD. I recently made a project for STM8L152R8. SPI, graphic LCD, ADC, extensive menu, almost 60kB batch.

    Discussion of installing STVD on Windows 10 split to separate thread.

    Andrew Neil
    Super User
    Dec 22, 2025 8:50 PM UTC

    @DarekR wrote:
    ST has not updated STVD for a long time. Which is scandalous

    But it aligns with what @Peter BENSCH said in the first reply.

    See also what @mƎALLEm said here and here.

     

    PS:

    See also:

    https://community.st.com/t5/stm8-mcus/stvd-mcu-selection-list-empty-dao360-re-register-not-work/m-p/868333/highlight/true#M10593

    "[STVD] is no longer being developed because all resources are focused on the more modern STM32"

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.