Skip to main content
Associate II
Dec 19, 2025 4:39 AM UTC
Solved

Help to Select MCU for Industrial automation

Dear ST team,

 

Please help to select controller for industrial automation. 

I have to design product for panel just to drive dc fan where the temperature high for cooling purpose.

STM8 controller STM8S003F3P6, STM8S103F3T6, one of the controllers is suitable?

Kindly provide contact details of your technical support team.

    mƎALLEm
    mƎALLEmBest answer
    ST Technical Moderator
    Dec 19, 2025 9:03 AM UTC

    STM32C0 family has lowest packages sizes.

    Example: STM32C011. Refer to the datasheet: 

    mALLEm_0-1766134906083.png

    and reference manual: RM0490

    C0 family is intended to replace 8-bit MCUs.

    Use STM32 MCU Finder tool to fine tune your selection.

     

     

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

    5 replies

    mƎALLEm
    ST Technical Moderator
    Dec 19, 2025 7:49 AM UTC

    Hello @Glodhi and welcome to the ST community,

    I suggest STM32C0 family instead of STM8 which is an old 8-bit MCU.

     

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
    GlodhiAuthor
    Associate II
    Dec 19, 2025 8:47 AM UTC

    but i require for small project thats why i am selecting the stm8s which have less gpio or cost effective.  4 gpio or 2 external interrupt or two pwm  need to use only? thats why i am not going on stm32 series.

     

    mƎALLEm
    mƎALLEmBest answer
    ST Technical Moderator
    Dec 19, 2025 9:03 AM UTC

    STM32C0 family has lowest packages sizes.

    Example: STM32C011. Refer to the datasheet: 

    mALLEm_0-1766134906083.png

    and reference manual: RM0490

    C0 family is intended to replace 8-bit MCUs.

    Use STM32 MCU Finder tool to fine tune your selection.

     

     

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.