Skip to main content
Rodo
Senior
Mar 19, 2025 2:57 AM UTC
Question

STM32H7A3 enabling SAI1 with I2S_CLKIN error?

Hi all,

I just upgraded cubeIDE from 1.17.0 to 1.18.0. 

I had set up a project in 1.17.0 without any issues. I was reading here some posts and I read that there is a dedicated I2S_CLKIN pin that I had missed. I was trying to figure out a clock source that would give me the 44.1kHz sampling and I figure 11.2896 MHz would do but is an odd frequency for the rest of the system. 

Anyhow... I enabled the I2S_CLKIN pin and set it for 11.2896 MHz. But when I save the code I keep getting an error that there is something wrong with SAI1 ... but I don't see what? I'm probably missing something basic but I can't see it so in my frustration I erased all projects and made I new one ... I still get the same error.  The zip file of the project is here but SAI1 is disabled. You need to set it to master or master with clock output and save it to see the error I get. There is no code from me just cubeMX (the version built-in cubeIDE 1.18.0). 

What am I missing? Thanks.

cubeIDE SAI1 error.png

 

cubeIDE SAI1 cfg.png

 

This topic has been closed for replies.

5 replies

KDJEM.1
ST Technical Moderator
Mar 19, 2025 10:15 AM UTC

Hello @Rodo;

 

Similar issue is reported here.

This issue has been raised internally to dev team for fix.

Internal ticket number: 204851 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

  

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Rodo
RodoAuthor
Senior
Mar 19, 2025 4:02 PM UTC

How do I find out when a solution is made available? Thanks

KDJEM.1
ST Technical Moderator
Mar 21, 2025 7:33 AM UTC

Hello @Rodo,

 

I'll let you know when the issue is solved in STM32CubeMX.

I apologize for any inconvenience.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KDJEM.1
ST Technical Moderator
Apr 14, 2025 3:34 PM UTC

Hello @Rodo,

 

Could you please try to use the latest STM32CubeMX 6.14.1 version and/or STM32CubeIDE1.18.1 version.

The SAI tab configuration issue is fixed as mentioned in STM32CubeMx 6.14.1 released.

KDJEM1_0-1744644830970.png

 

Please let me know if the issue is solved or not?

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Rodo
RodoAuthor
Senior
Apr 14, 2025 3:57 PM UTC

I removed cubeIDE v1.18.0 and installed v1.17.0 again. I don't think I'm gonna try v1.18.1 at this point. Thanks for the heads up though.