Associate II
May 3, 2019
Question
STM32F407VGTx / CDC / Error Driver
- May 3, 2019
- 29 replies
- 10836 views
Hello,
I test the CDC with my STM32F407VgTx in an up-to-date environment:
Windows 10 / STM32CubeMx v5.20 / SW4STM32 / System WorkBench for STM32/ST-LINK V2
The VCP v 1.50 driver for windows 10 has been installed normally and declared active.
The source of the CDC program used is:
\ STM32Cube_FW_F4_V1.24.0 \ STM32Cube_FW_F4_V1.24.0 \ Middleware \ ST \ STM32_USB_Device_Library \ Class \ CDC
When running the program, when init the USB, I get Windows Error 43.
Unknown USB Device (descriptor request failure).
Can you help me solve this problem?
In advance thank you
Robert