STM32CubeMX does NOT work in quiet mode
- 6 replies
- 1039 views
Follow-on from CubeMX code generation from command line.
I am posting again in hopes of getting meaningful answer.
I tried creating a simple script text file to automate code generation for my project. The script file has all of three lines:
config load DCC_tester.ioc
generate code .
exit
The feedback I got on why it did not work was my .ico file was corrupted. To prove this was not the case I used a very simple project file using one of your example projects from one of your released STM32H5 bundles.
The only modification I made was changing the name and making it a cmake project.
I am running on Windows 11 with CubeMX installed using all defaults.
I can click on the .ioc file from Windows Explorer and the MX IDE opens just fine. I can click the "GENERATE CODE" button and that also works just fine. All the files are generated as expected.
I try launching using the -q using ether a PowerShell script or a command line batch file and neither completes although it looks like its trying. Seems to stall leaving a MXTmpFiles folder. cmake and other files like startup and linker file are not generated.
I have attached the .ioc the script text file as well as PowerShell and batch file ... none work as expected.