Skip to main content
Associate
September 21, 2024
Question

[BUG] DAC software trigger at STM32L431 have not set DAC_SWTRIGR_SWTRIGx Bit.

  • September 21, 2024
  • 1 reply
  • 1395 views

My last page is: Re: Why DAC output nothing in software trigger? - STMicroelectronics Community

I have find CubeMX BUG.

I use STM32L431RCT6 and software version is STM32CubeL4 Firmware Package V1.18.0 / 07-June-2023

My STM32CubeMX config is:

Wshuo1_0-1726889243392.png

And my code in main() is:

 

 

HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_2, DAC_ALIGN_12B_R, 4095);
HAL_DAC_Start(&hdac1, DAC_CHANNEL_2);

 

 

But the PA5 have no voltage.

 

I find the "stm32l4xx_hal_dac.c" file HAL_DAC_Start() function is:

 

 

HAL_StatusTypeDef HAL_DAC_Start(DAC_HandleTypeDef *hdac, uint32_t Channel)
{
 /* Check the parameters */
 assert_param(IS_DAC_CHANNEL(Channel));

 /* Process locked */
 __HAL_LOCK(hdac);

 /* Change DAC state */
 hdac->State = HAL_DAC_STATE_BUSY;

 /* Enable the Peripheral */
 __HAL_DAC_ENABLE(hdac, Channel);

#if defined (STM32L4P5xx) || defined (STM32L4Q5xx) || defined (STM32L4R5xx) || defined (STM32L4R7xx) || defined (STM32L4R9xx) || defined (STM32L4S5xx) || defined (STM32L4S7xx) || defined(STM32L4S9xx)
 if (Channel == DAC_CHANNEL_1)
 {
 /* Check if software trigger enabled */
 if ((hdac->Instance->CR & (DAC_CR_TEN1 | DAC_CR_TSEL1)) == DAC_TRIGGER_SOFTWARE)
 {
 /* Enable the selected DAC software conversion */
 SET_BIT(hdac->Instance->SWTRIGR, DAC_SWTRIGR_SWTRIG1);
 }
 }
 else
 {
 /* Check if software trigger enabled */
 if ((hdac->Instance->CR & (DAC_CR_TEN2 | DAC_CR_TSEL2)) == (DAC_TRIGGER_SOFTWARE << (Channel & 0x10UL)))
 {
 /* Enable the selected DAC software conversion*/
 SET_BIT(hdac->Instance->SWTRIGR, DAC_SWTRIGR_SWTRIG2);
 }
 }

#endif /* STM32L4P5xx STM32L4Q5xx STM32L4R5xx STM32L4R7xx STM32L4R9xx STM32L4S5xx STM32L4S7xx STM32L4S9xx */

#if defined (STM32L431xx) || defined (STM32L432xx) || defined (STM32L433xx) || defined (STM32L442xx) || defined (STM32L443xx) || \
 defined (STM32L471xx) || defined (STM32L475xx) || defined (STM32L476xx) || defined (STM32L485xx) || defined (STM32L486xx) || defined (STM32L496xx) || defined (STM32L4A6xx)
 if(Channel == DAC_CHANNEL_1)
 {
 /* Check if software trigger enabled */
 if ((hdac->Instance->CR & (DAC_CR_TEN1 | DAC_CR_TSEL1)) == DAC_CR_TEN1)
 {
 /* Enable the selected DAC software conversion */
 SET_BIT(hdac->Instance->SWTRIGR, DAC_SWTRIGR_SWTRIG1);
 }
 }
 else
 {
 /* Check if software trigger enabled */
 if ((hdac->Instance->CR & (DAC_CR_TEN2 | DAC_CR_TSEL2)) == DAC_CR_TEN2)
 {
 /* Enable the selected DAC software conversion*/
 SET_BIT(hdac->Instance->SWTRIGR, DAC_SWTRIGR_SWTRIG2);
 }
 }
#endif /* STM32L431xx STM32L432xx STM32L433xx STM32L442xx STM32L443xx */
 /* STM32L471xx STM32L475xx STM32L476xx STM32L485xx STM32L486xx STM32L496xx STM32L4A6xx */


#if defined (STM32L451xx) || defined (STM32L452xx) || defined (STM32L462xx)
 /* Check if software trigger enabled */
 if((hdac->Instance->CR & (DAC_CR_TEN1 | DAC_CR_TSEL1)) == (DAC_CR_TEN1 | DAC_CR_TSEL1))
 {
 /* Enable the selected DAC software conversion */
 SET_BIT(hdac->Instance->SWTRIGR, DAC_SWTRIGR_SWTRIG1);
 }
#endif /* STM32L451xx STM32L452xx STM32L462xx */
 /* Change DAC state */
 hdac->State = HAL_DAC_STATE_READY;

 /* Process unlocked */
 __HAL_UNLOCK(hdac);

 /* Return function status */
 return HAL_OK;
}

 

 

 But in rm0394-stm32l41xxx42xxx43xxx44xxx45xxx46xxx-advanced-armbased-32bit-mcus-stmicroelectronics.pdf the TSELx config 0b111 with SWTRIG:

Wshuo1_1-1726889591823.png

 

SO the code in check if software trigger enabled have error:

 

#if defined (STM32L431xx) || defined (STM32L432xx) || defined (STM32L433xx) || defined (STM32L442xx) || defined (STM32L443xx) || \
 defined (STM32L471xx) || defined (STM32L475xx) || defined (STM32L476xx) || defined (STM32L485xx) || defined (STM32L486xx) || defined (STM32L496xx) || defined (STM32L4A6xx)
 if(Channel == DAC_CHANNEL_1)
 {
 /* Check if software trigger enabled */
 if ((hdac->Instance->CR & (DAC_CR_TEN1 | DAC_CR_TSEL1)) == DAC_CR_TEN1)
 {
 /* Enable the selected DAC software conversion */
 SET_BIT(hdac->Instance->SWTRIGR, DAC_SWTRIGR_SWTRIG1);
 }
 }
 else
 {
 /* Check if software trigger enabled */
 if ((hdac->Instance->CR & (DAC_CR_TEN2 | DAC_CR_TSEL2)) == DAC_CR_TEN2)
 {
 /* Enable the selected DAC software conversion*/
 SET_BIT(hdac->Instance->SWTRIGR, DAC_SWTRIGR_SWTRIG2);
 }
 }
#endif /* STM32L431xx STM32L432xx STM32L433xx STM32L442xx STM32L443xx */
 /* STM32L471xx STM32L475xx STM32L476xx STM32L485xx STM32L486xx STM32L496xx STM32L4A6xx */

 

 

Need change with:

 

#if defined (STM32L431xx) || defined (STM32L432xx) || defined (STM32L433xx) || defined (STM32L442xx) || defined (STM32L443xx) || \
 defined (STM32L471xx) || defined (STM32L475xx) || defined (STM32L476xx) || defined (STM32L485xx) || defined (STM32L486xx) || defined (STM32L496xx) || defined (STM32L4A6xx)
 if(Channel == DAC_CHANNEL_1)
 {
 /* Check if software trigger enabled */
 if ((hdac->Instance->CR & (DAC_CR_TEN1 | DAC_CR_TSEL1)) == (DAC_CR_TEN1 | DAC_CR_TSEL1)) {
 /* Enable the selected DAC software conversion */
 SET_BIT(hdac->Instance->SWTRIGR, DAC_SWTRIGR_SWTRIG1);
 }
 }
 else
 {
 /* Check if software trigger enabled */
 if ((hdac->Instance->CR & (DAC_CR_TEN2 | DAC_CR_TSEL2)) == (DAC_CR_TEN2 | DAC_CR_TSEL2)) {
 /* Enable the selected DAC software conversion*/
 SET_BIT(hdac->Instance->SWTRIGR, DAC_SWTRIGR_SWTRIG2);
 }
 }
#endif /* STM32L431xx STM32L432xx STM32L433xx STM32L442xx STM32L443xx */
 /* STM32L471xx STM32L475xx STM32L476xx STM32L485xx STM32L486xx STM32L496xx STM32L4A6xx */

 

So the PA5 have voltage.

 

I only test STM32L431RCT6.

 

 

This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
September 23, 2024

Hi @Wshuo.1 ,

Thank you and @waclawek.jan for bringing this issue to our attention.

I reported it internally to be fixed by our development team.

Internal ticket number: 191791 (This is an internal tracking number and is not accessible or usable by customers).

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.