cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE for Ubuntu 24.04

NNada.1
Associate II

Hello All,

 

    I am using Ubuntu 24.04 and STM32 Cube IDE 1.16 version. When I try to  burn code to a STM32F401RE Nucleo board. I am getting below error.

 

Could not determine GDB version using command: arm-none-eabi-gdb --version
arm-none-eabi-gdb: error while loading shared libraries: libncurses.so.5: cannot open shared object file: No such file or directory

 

and yes I have tried sudo get-install.

Does STM team has any suggestion ?

Thank you

2 REPLIES 2
Andrew Neil
Super User

https://community.st.com/t5/stm32cubeide-mcus/stm32cudeide-on-ubuntu-24-04-no-target/m-p/736399/highlight/true#M31898

 

https://community.st.com/t5/stm32cubeide-mcus/i-can-t-install-ide-cube-on-ubuntu-24/m-p/725849

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hello ,

   ST should write this at download page!! That Ubuntu 24.04  is not supported.

Is there any alternatives to use STM Controllers in 24.04 or changing the Os the only option?

Thank you,

Regards