Skip to main content
CColo.2
Associate II
December 28, 2025
Question

STM32CubeIDE 2.0.0 on macOS Tahoe 26.2 (Apple Silicon M4): text selection not visible

Ambiente

Sistema operativo Mac Tahoe 26.2 (25C56)

Apple Silicon M4

STM32CubeIDE 2.0.0 (x86_64, ejecutándose bajo Rosetta 2)

Asunto

STM32CubeIDE se inicia correctamente, pero la selección de texto no se representa visualmente en ninguna parte del IDE (editor, consola, vistas).

La selección del mouse y del teclado no muestra ningún resaltado.

Copiar/pegar funciona normalmente , lo que indica que la selección existe internamente pero no se muestra.

La selección de texto funciona correctamente en otras aplicaciones de macOS.

Pasos para reproducir

1. Inicie STM32CubeIDE en Rosetta:

arch -x86_64 /Aplicaciones/ST/STM32CubeIDE.app/Contenidos/MacOS/STM32CubeIDE

2.Abra cualquier archivo fuente.

3.Intenta seleccionar texto.

Solución de problemas realizados

Instalación de Rosetta 2 verificada.

Restablecer preferencias y espacio de trabajo.

Espacio de trabajo limpio probado.

 Deshabilitado el renderizado SWT Metal/gestos a través de opciones .ini.

El problema persiste.

21 replies

ST Technical Moderator
December 29, 2025

Hello CColo.2,

Thank you for reaching out. Would you mind providing your message in English, please?

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CColo.2
CColo.2Author
Associate II
December 29, 2025

Operating System: macOS Tahoe 26.2 (25C56)
Hardware: Apple Silicon M4
IDE: STM32CubeIDE 2.0.0 (x86_64, running under Rosetta 2)


Subject

STM32CubeIDE starts correctly, but text selection is not visually rendered anywhere in the IDE (editor, console, or views).


Description

Text selection using either mouse or keyboard is not visually highlighted anywhere in STM32CubeIDE.

Copy/paste operations work normally, which indicates that the text selection exists internally but is not rendered on screen.

Text selection works correctly in all other macOS applications.


Steps to Reproduce

  1. Launch STM32CubeIDE under Rosetta:

     
    arch -x86_64 /Applications/ST/STM32CubeIDE.app/Contents/MacOS/STM32CubeIDE
  2. Open any source file.

  3. Attempt to select text using mouse or keyboard.


Troubleshooting Performed

Verified Rosetta 2 installation

Reset IDE preferences and workspace

Tested with a clean workspace

Disabled SWT Metal rendering / gesture support via .ini options

The issue persists.

CColo.2
CColo.2Author
Associate II
December 29, 2025
Operating System: macOS Tahoe 26.2 (25C56)
Hardware: Apple Silicon M4
IDE: STM32CubeIDE 2.0.0 (x86_64, running under Rosetta 2)

Subject

STM32CubeIDE starts correctly, but text selection is not visually rendered anywhere in the IDE (editor, console, or views).

Description

Text selection using either mouse or keyboard is not visually highlighted anywhere in STM32CubeIDE.

Copy/paste operations work normally, which indicates that the text selection exists internally but is not rendered on screen.

Text selection works correctly in all other macOS applications.

Steps to Reproduce

Launch STM32CubeIDE under Rosetta:

arch -x86_64 /Applications/ST/STM32CubeIDE.app/Contents/MacOS/STM32CubeIDE
Open any source file.

Attempt to select text using mouse or keyboard.

Troubleshooting Performed

Verified Rosetta 2 installation

Reset IDE preferences and workspace

Tested with a clean workspace

Disabled SWT Metal rendering / gesture support via .ini options

The issue persists.


Best regard

Ing. Carlos Eduardo Colombo
carlosc@asesrl.com.ar
carlosc@asesrl.ar

ST Technical Moderator
December 30, 2025

Hello CColo.2,

This behavior is raised to development team for investigation via this ticket number: 224479.

I will keep you posted.

Regards.

 

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CColo.2
CColo.2Author
Associate II
January 5, 2026

ok, Thank you.

Visitor II
January 7, 2026

I have the exact same issue on MacOS Tahoe 26.2. @Aimen1 Is there an update or workaround for this? 

ST Technical Moderator
January 9, 2026

Hello FOFI,

macOS 26.2 was released in December 2025 after the release of the STM32CubeIDE 2.0.0. Therefore, STM32CubeIDE 2.0.0 is supported only on the earlier macOS 26 Tahoe version, as stated in RN114.

The issue will be fixed in a future release.

Aimen1_1-1767975574846.png

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ST Technical Moderator
January 12, 2026

Hello @FOFI 

Our development team remains committed to customers and collaborators satisfaction and is engaged in aligning the STM32CubeIDE with macOS Tahoe 26.2.

We will share further information as it becomes available.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
grisom13
Associate III
January 8, 2026

There are workarounds available already from users. So sad ST is not providing anything now. 

 

https://community.st.com/t5/stm32cubeide-mcus/warning-macos-update-to-26-1-breaks-eclipse-text-selection/td-p/854200

 

The fix for me is crashing the APP with an error, but other report its working 

Arete
Explorer
February 27, 2026

Still looking for an update, patch or workaround.

grisom13
Associate III
February 27, 2026

The fix exist. Need to manually patch Eclipse files. 

Graduate
April 16, 2026

I just ran into the same problem. MacOS was updated and now can't see selected text.

IDE 2.1.1

MacOS 26.4.1

Apple M4 Pro

Visitor II
April 23, 2026

I have the same problem. Makes the whole IDE unusable 

IDE 2.1.1
MacOS 26.4.1
Intel Core i7

grisom13
Associate III
April 23, 2026

the fix is available. check earlier posts