Skip to main content
Associate II
Jul 29, 2025 6:38 AM UTC
Solved

"Range [0,-1) out of bounds for length 48" trying to open Debug Configuration

Hello, I'm trying to set the debug configuration of my project, but I cannot open the debug file under C/C++ Application. Besides, running this project was not successful either.

Levyhy_0-1753770582011.png

I have tried switching workspace and uninstalling IDE, but neither worked.

Can anyone help me solve my problem? Thank you very much.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Aug 1, 2025 12:33 PM UTC

Hello @Levy-hy ,

We have reproduced this issue with CubeIDE 1.19 and I escalated it to our CubeIDE team for analysis (internal ticket number: 215198).

PS: Ticket number: 215198 is an internal tracking number and is not accessible or usable by customers.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

13 replies

mbarg.1
Senior III
Jul 29, 2025 7:55 AM UTC

Version of STM32CubeIde?

Version 1.18 are buggy - update to 1.19

Levy-hyAuthor
Associate II
Jul 29, 2025 8:15 AM UTC

Mine is 1.19, already the latest one

Andrew Neil
Super User
Jul 29, 2025 7:59 AM UTC

Did you try pressing the 'Details' button?

The message says, "Out of bounds for length 48".

The name of your Debug Configuration is very long* - maybe it's too long?

Maybe try just shortening the name?

 

PS: 

* The name certainly is over 48 characters!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Levy-hyAuthor
Associate II
Jul 29, 2025 8:24 AM UTC

Levyhy_0-1753777014899.png

Details are the same. I tired to rename the project to make its name shorter, but it didn't work either.

Then I opened another project, and found its run configuration back to normal. So I assume the problem lies in the project. But the project is the example AI demo project of STM32N6 and I'm stuck here:( 

 

ST Technical Moderator
Jul 29, 2025 8:37 AM UTC

@Levy-hy , Did you make any changes to the Demo project? 

Check Project configuration, such as memory allocation and linker scripts are correctly configured.

You can also, perform a clean build of the project to ensure no corrupted files are causing this issue.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Jul 29, 2025 8:23 AM UTC

Hello @mbarg.1 

Try follow the steps in this article : How to debug STM32N6 using STM32CubeIDE

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
Aug 1, 2025 12:33 PM UTC

Hello @Levy-hy ,

We have reproduced this issue with CubeIDE 1.19 and I escalated it to our CubeIDE team for analysis (internal ticket number: 215198).

PS: Ticket number: 215198 is an internal tracking number and is not accessible or usable by customers.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Associate II
Aug 8, 2025 5:55 AM UTC

Hello Imen.D,

I am also facing the same issue . Is there a resolution to the issue available?

Ghofrane GSOURI
ST Technical Moderator
Aug 19, 2025 11:39 AM UTC

Hello @Levy-hy 

As a workaround, try removing the following line from your .project file:

<nature>com.st.stm32cube.ide.mcu.MCUAppSProjectNature</nature>

 

GhofraneGSOURI_0-1755603295833.png

You will be able to debug your project successfully.

GhofraneGSOURI_1-1755603379550.png

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.