Skip to main content
RPG
Associate III
Jun 17, 2024 8:53 AM UTC
Solved

Problem installing X-CUBE-SPN1 extension in STM32CubeIDE

Hi

I get this error trying to install the X-CUBE-SPN1 extension for X-NUCLEO-IHM01A1 in STM32CubeIDE.

I have downloaded the latest version of the X-CUBE-SPN1 extension and version 1.13 and 1.15.1 of the IDE.

I get this error:

Screenshot 2024-06-17 at 10.45.55.png

Anyone has faced this problem?

Thanks in advance.

 

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jun 17, 2024 3:04 PM UTC

Not all X-CUBE packages are yet integrated in CubeMX or CubeIDE, but must be integrated manually. If one of the examples from the projects folder is sufficient for you, you can also unpack the X-CUBE in a path with a short name (e.g. C:\ST for Windows) and import the project directly from there.

The problem has already been discussed with a similar, non-integrated package.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

RPG
RPGAuthor
Associate III
Jun 17, 2024 9:05 AM UTC

I have tried installing other packages from local and apparently same issue occurs. Any idea of what could be the problem?

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jun 17, 2024 3:04 PM UTC

Not all X-CUBE packages are yet integrated in CubeMX or CubeIDE, but must be integrated manually. If one of the examples from the projects folder is sufficient for you, you can also unpack the X-CUBE in a path with a short name (e.g. C:\ST for Windows) and import the project directly from there.

The problem has already been discussed with a similar, non-integrated package.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RPG
RPGAuthor
Associate III
Jun 19, 2024 5:43 AM UTC

Thank you Peter. I will try installing it manually. There might be better documentation or installation instructions on this package.

Best regards,

Raul