Skip to main content
Associate III
Apr 16, 2026 9:16 AM UTC
Solved

debugger via UART without ST-LINK on NUCLEO-H755ZI-Q

hello ST Community!

I'm trying to connect via UART without USB ST-LINK to the NUCLEO-H755ZI-Q for debugging from the STM32CubeIDE environment, but I can't connect.

What settings do I need to make in the STM32CubeIDE environment to debug via UART?

I tried connecting via UART from the STM32CubeProgrammer environment to simply read flash memory, but it won't connect.

What settings do I need to make in the STM32CubeIDE environment to debug via UART without USB ST_LINK?

 

Thanks for supports

Andrew Neil
Andrew NeilBest answer
Super User
Apr 16, 2026 12:06 PM UTC

@Domy_ST wrote:

I would like to do full debugging via UART because in the future the Nucleo-H755ZI-Q microcontroller will be integrated into a board .


You realise that integrating ST Development boards into a final product is not allowed?

See the Terms of Use (via: https://www.st.com/en/evaluation-tools/nucleo-h755zi-q.html#documentation)

 


@Domy_ST wrote:

I'm not sure if I will have access to the SWD using the STDC14 - MIPI10 connector.


How to do this is described in the User Manual:

AndrewNeil_0-1776341136204.png

https://www.st.com/resource/en/user_manual/um2408-stm32h7-nucleo144-boards-mb1363-stmicroelectronics.pdf#page=17

also via: https://www.st.com/en/evaluation-tools/nucleo-h755zi-q.html#documentation

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

18 replies

mƎALLEm
ST Technical Moderator
Apr 16, 2026 9:22 AM UTC

Hello,


@Domy_ST wrote:

I tried connecting via UART from the STM32CubeProgrammer environment to simply read flash memory, but it won't connect.

 

What do you mean by connecting UART from CubeProgrammer? do you mean via ST bootloader?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Domy_STAuthor
Associate III
Apr 16, 2026 9:47 AM UTC

hello @mƎALLEm,

Yes, using the ST Bootloader via UART, you don't want to connect to the STm32CubeProgrammer, as described in this post:

https://community.st.com/t5/stm32cubeprogrammer-mcus/connection-via-uart-with-stm32cubeprogrammer/td-p/892681 

In addition to the ST Bootloader via UART, I also need to debug via UART without USB. ST-LINK with the STM32CubeIDE environment is this possible?

mƎALLEm
ST Technical Moderator
Apr 16, 2026 10:02 AM UTC

@Domy_ST wrote:

Yes, using the ST Bootloader via UART, you don't want to connect to the STm32CubeProgrammer, as described in this post:

https://community.st.com/t5/stm32cubeprogrammer-mcus/connection-via-uart-with-stm32cubeprogrammer/td-p/892681 



Did you use the same resource needed by the UART that are indicated in the AN2606 "Introduction to system memory boot mode on STM32 MCUs"?

USART3 needs PB11 and PB10 for the bootloader: 

mALLEm_1-1776333615409.png

While in the NUCLEO board is connected to PD8 and PD9 as indicated by the schematic:

mALLEm_0-1776333574494.png

 

So you need to wire and connect PB10 to PD8 and PB11 to PD9, so the STLINK-VCP will be connected to the USART3 and use the ST bootloader.

 


@Domy_ST wrote:

In addition to the ST Bootloader via UART, I also need to debug via UART without USB. ST-LINK with the STM32CubeIDE environment is this possible?


Not clear what do you mean by debug with UART in CubeIDE!

Do you need to display messages over printf in CubeIDE or you need totally to debug the application with UART?? Because that's not possible as it doesn't make sense.

To display messages over UART using printf you need to make a retarget of UART to printf.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Apr 16, 2026 9:59 AM UTC

What do you mean by, "debugging" here?

Are you simply looking to give printf-style outputs, or do you want the full control that SWD/JTAG provides?

 

SWD/JTAG gives a direct connection to the chip's internal debug hardware - you can't do that via UART.

The closest would be to implement some sort of Debug Monitor; eg,

Step-through debugging with no debugger on Cortex-M

 

But, if you can provide a UART connection - why not provide a SWD connection? It only needs* 2 wires (plus ground)...

 

* Although 4 is better - including NRST and VDD

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Domy_STAuthor
Associate III
Apr 16, 2026 11:39 AM UTC

@Andrew Neil Yes, I know how to use the printf monitor debug via UART. My intention was to fully debug via UART. If you tell me that's not possible, I'll just use the printf monitor debug and take a look at the link you provided.

Thanks