Skip to main content
Amel NASRI
ST Technical Moderator
March 2, 2023

How to recognize a genuine ST-LINK/V2 versus a cloned one

To answer the questions like "Is my ST-Link/V2 genuine? Where to find a genuine ST-Link/V2? Why my device isn't recognized?" and other related ones, please refer to the following:

Where to find a genuine ST-Link/V2

ST-Link official in-circuit debuggers and programmers are available from standard STMicroelectronics distributors. Both STLINK-V3MINIE and STLINK-V3SET are usually available in volume, while the availability leadtime of ST-LINK/V2 may temporarily increase.

How to recognize a genuine ST-Link/V2

667.jpg668.jpg
669.jpg670.jpg

Should a ST-Link/V2 clone properly work with any ST tool or FW?

ST resources are dedicated to support genuine ST-Link products. We are not committed to ensure that clones are properly working with the firmware that we are delivering.

How to re-use the ST-Link section from a STM32 Nucleo board

For reference, the pricing of STLINK-V3MINIE probe and of selected Nucleo boards is around 10$, i.e half the price of ST-LINK/V2.
The embedded ST-Link from a Nucleo-64 board may seamlessly be used to program and debug an external STM32 application. The related settings are described in the User Manual of the Nucleo-64 board UM1724 in the paragraph covering the embedded ST-Link/V2-1.
 

5 replies

Andrew Neil
Super User
July 31, 2024

Note that anything looking like this is a fake/clone - even if it does have an "ST" logo on it:

AndrewNeil_0-1722419957735.png 

   AndrewNeil_1-1722420112805.png

 

 

 

There are many of these fakes/clones which all look identical, but they do not have consistent pinouts - the pinouts can be different, even when bought from the same place!

AndrewNeil_2-1722420232052.pngAndrewNeil_3-1722420257252.png


The above collected from a couple of previous posts:

https://community.st.com/t5/stm32-mcus-products/blue-pill-stm32f1-board-gets-programmed-through-arduino-ide-but/m-p/668483/highlight/true#M242662

https://community.st.com/t5/stm32-mcus-products/debug-problem-with-clone-st-linkv2/m-p/661306/highlight/true#M240845 

 

PS:

Example of a lookalike fake ST-Link:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/is-this-a-genuine-st-link/m-p/867869/highlight/true#M29139

 

#FakeSTLink #CloneSTLink

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
BarryWhit
Lead
August 18, 2024

The clones also don't break out (without manual modding) the SWO pin needed for the "Serial Wire Viewer" (SWV) functionality in CubeIDE, which is very very useful while developing.

"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."
Andreas Bolsch
Lead III
August 18, 2024

And RST is SWIM reset, not SWD reset signal. Moreover there are clones around which have totally weird pull-up/pull-downs on SWDIO and/or SWCLK. Causes communication to target to cease sporadically:

https://www.mikrocontroller.net/topic/515218

Probably the manufacturer just took a reel of resistors without knowing anything about the functionality of the circuit.  

avinash_elec
Associate III
June 20, 2025

How do they get the firmware of ST link? Is it freely available? 

Andrew Neil
Super User
June 20, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.