Skip to main content
Associate II
Dec 15, 2025 12:30 PM UTC
Solved

Debugging TouchGFX example project on STM32H757I-EVAL fails to program

I have a new STM32H757I-EVAL board. The examples that can programmed on it ran perfectly.

I want to compile and debug the TouchGFX example myself but I only managed to kill the app that is running on it.

I've created the TouchGFX example from within STMCube32IDE by selecting the evaluation board, and then the example. It builds without errors.

In Debug Configuration, on Debug tab under External Loaders, I've added MT25TL01G_STM32H747I-DISCO.stldr with Enabled set to true and Initialised set to false.

When I select debug, it starts to program but fails after a while. Below is the output from Console.

What is wrong, and how can I fix it?

 

STMicroelectronics ST-LINK GDB server. Version 7.10.0

Copyright (c) 2025, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Info : default port : 7184

Info : Remote address: 127.0.0.1

Info : stlinkserver already running, exit

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

-------------------------------------------------------------------

STM32CubeProgrammer v2.19.0

-------------------------------------------------------------------

 

 

 

Log output file: /tmp/STM32CubeProgrammer_a1UHge.log

ST-Link Server is running on port : 7184

ST-LINK SN : 003D003D3234510637333934

ST-LINK FW : V3J16M7

Info : default port : 7184

Info : Remote address: 127.0.0.1

Info : stlinkserver already running, exit

Info : default port : 7184

Info : Remote address: 127.0.0.1

Info : stlinkserver already running, exit

Board : STM32H757I-EVAL

Voltage : 3.27V

SWD freq : 8000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x450

Revision ID : Rev V

Device name : STM32H7xx

Flash size : 2 MBytes

Device type : MCU

Device CPU : Cortex-M7/M4

BL Version : 0x91

 

Opening and parsing file: ST-LINK_GDB_server_OwfSTT.srec

 

 

Memory Programming ...

File : ST-LINK_GDB_server_OwfSTT.srec

Size : 30.07 MB

Address : 0x08000000

 

 

 

Erasing memory corresponding to sector 0:

Erasing internal memory sector 0

 

Erasing memory corresponding to sector 0:

Erasing internal memory sectors [10 13]

 

Erasing memory corresponding to sector 0:

Erasing external memory sectors [544 780]

Error: failed to erase memory

 

 

Error: failed to erase memory

Encountered Error when opening /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_2.2.100.202412061334/tools/bin/STM32_Programmer_CLI

Error in STM32CubeProgrammer

Shutting down...

Exit.

 

 

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 16, 2025 11:07 AM UTC

Hello @Pieter25 and welcome to the ST community,

Because you are using STM32H757I-EVAL board (Eval board) and you set the incorrect flash loader MT25TL01G_STM32H747I-DISCO.stldr (used for Disco board).

You need to use MT25TL01G_STM32H747-EVAL.stldr (I think it's compatible with STM32H757I-EVAL board with the same hardware configuration) :

mALLEm_0-1765883043744.png

Hope that helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 16, 2025 11:07 AM UTC

Hello @Pieter25 and welcome to the ST community,

Because you are using STM32H757I-EVAL board (Eval board) and you set the incorrect flash loader MT25TL01G_STM32H747I-DISCO.stldr (used for Disco board).

You need to use MT25TL01G_STM32H747-EVAL.stldr (I think it's compatible with STM32H757I-EVAL board with the same hardware configuration) :

mALLEm_0-1765883043744.png

Hope that helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
Dec 16, 2025 1:26 PM UTC

A follow-up question here.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.