Skip to main content
yilmazkircicek
Associate III
April 13, 2025
Solved

Cannot open ico file from link provided by ST


@TDK wrote:

They're not made using STM32CubeMX.


There should be an internal reason of this decision but it does not seem reasonable for a customer viewpoint. An expert ST staff could easily done this for all of us. Anyway, at least we have an example.

Thanks for your time...

New question moved from this original thread.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
April 14, 2025

Hello @yilmazkircicek ,

I've normally opened H74_Discovery_STM32H745I-DISCO_STM32H745XIH_Board_AllConfig.ioc as shown in this screenshot:

mALLEm_0-1744631430759.png

How did you download that file? please download the all package from github:

mALLEm_1-1744631559363.png

Unzip the package and open the ioc file with the latest version of CubeMx (the latest version is 6.14)

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

8 replies

Pavel A.
April 13, 2025

Some new MCU families do include .ioc files.  The internal reason is that many STM32 product families and their examples have were released long ago, before the CubeMX stabilized. Also, updates and development of CubeMX would require resources for regression testing of these examples. The "expert staff" has probably other important things to do ))

The .ioc files for many ST boards are available here. Though these .ioc's are not coupled with specific functional example code. Al least, this is something to start from.

 

yilmazkircicek
Associate III
April 14, 2025

Thanks for the link, I have tried "H74_Discovery_STM32H745I-DISCO_STM32H745XIH_Board_AllConfig.ioc" and here is the result; a perfect forward and backward compatibility :) 

yilmazkircicek_0-1744620553719.png

 

 

Pavel A.
April 14, 2025

What is your CubeMX version? I have 6.11.1 here, it opens this ioc file without issues.

 

.

Pavel A.
April 14, 2025

@KDJEM.1 @mƎALLEm   ? Why CubeMX 6.14 fails to open .ioc files from github that open successfully with v. 6.11.1 ?@