Skip to main content
Associate
Sep 7, 2023 2:06 PM UTC
Solved

STM32F446ZE not booting

Hello,

some of our boards do not boot after powering them. We realised that most of the time this happens, the 1.2V at VCAP1 and VCAP2 == 0V. At our boards the BYPASS_REG pin is floating. So there are two questions for us now:

1. Could the floating BYPASS_REG  pin cause our Problems?

2. does the BYPASS_REG pin have an internal pulldown resistor?

We also realised, that if we add a 10µF capacitor to the NRST pin, the board will boot everytime. (Normaly there is a 100nF capacitor)

Thank you in advance :)

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Sep 8, 2023 7:05 AM UTC

Correct. It would be mentioned in the data sheet if there was an internal pull-down at the pin BYPASS_REG. This is corroborated by the statement in section 3.17.1: On packages embedding the BYPASS_REG pin, the regulator is enabled by holding BYPASS_REG low. ...so you have to actively pull it to GND and not let it float (for low).

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

Peter BENSCH
ST Technical Moderator
Sep 7, 2023 2:28 PM UTC

You are obviously using one of the packages WLCSP or UFBGA and therefore have the pin BYPASS_REG. However, this pin must have a defined level and must not float. I assume that you want to use the internal voltage regulator, so you should connect BYPASS_REG to GND via a pull-down.

In this case, it is also mandatory to connect a 2.2µF capacitor to GND on each of the pins VCAP1 and VCAP2 (see data sheet). You should reduce to 100nF at NRST again.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
CO_itAuthor
Associate
Sep 7, 2023 3:58 PM UTC

Thank you for the feedback. We already realised that we should had connected this pin.

Can I correctly understand from your answer that there is no internal pulldown resistor installed on the pin?

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Sep 8, 2023 7:05 AM UTC

Correct. It would be mentioned in the data sheet if there was an internal pull-down at the pin BYPASS_REG. This is corroborated by the statement in section 3.17.1: On packages embedding the BYPASS_REG pin, the regulator is enabled by holding BYPASS_REG low. ...so you have to actively pull it to GND and not let it float (for low).

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Issamos
Super User
Sep 7, 2023 2:28 PM UTC

Hello @CO_it 

This faq and this AN2606 may help you.

Best regards.

II

CO_itAuthor
Associate
Sep 8, 2023 8:20 AM UTC

Tnak you