Skip to main content
Associate
April 3, 2024
Question

STM32 MCU Choosing and programming

  • April 3, 2024
  • 4 replies
  • 2758 views

Hello everyone!

After some more studying on STM32 ecosystem and how the programming of those boards work I've come to a blunder:

I am designing a project with an STM32 Microcontroller that I need to program (of course), and I don't know what method should I use. Initially I thought it would be perfect to go with the USB, but then I realised that the development board that I used to program via plug'n'play USB (where the idea of USB programming came), has an ST-Link debugger included that allowed me to do so.

This means that I either have to include a debugger in my schematic and PCB design (more space, more components, bigger board etc), or buy a separate one and get the JTAG/SWD pins out with a connector. I also understand that with BOOT0 hooked to power, via a switch, the MCU is programmable with USB, but I don't understand what other tools do I need to make the USB programming possible.....

 

1. What is the best way to have a smooth programming experience with my board (it might need several trial and error with the code until its working and complete - I am also a noobie regarding the STM32 programming)?

 

Regarding the MCU model, initially I chose STM32F103, but some guy told me it's quite primitive and has no DFU which makes it harder to program/debug via USB. In the past I worked with STM32L010RB dev board, maybe I should switch to that one??? My application is about measuring some currents and transferring the values to my PC - the values are transferred via I2C to the MCU, and we are talking about 46 measurements values that are in the form of Voltage and corresponding current. It is USB-powered.

 

2.What MCU should I choose??

 

3. Can someone enlighten me on this path of working with and STM32 on a more advanced manner than "dev board light the LED blink blink"??

This topic has been closed for replies.

4 replies

Andrew Neil
Super User
April 3, 2024

Yes, the Standard way is to provide an SWD connection.

At a minimum, it's just 3 pins - SWDIO, SWCLK, and GND - but it's best to also include Reset and VDD.

https://documentation-service.arm.com/static/5fce6c49e167456a35b36af1

 

Recent thread on debug connections:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/st-link-with-jst-adapter/m-p/653685

note that you don't necessarily have to provide an actual connector - could be just "test points" on the PCB.

Another common practice is to provide the footprint for a connector, but not fit it in production.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AlexB99Author
Associate
April 3, 2024

Thank you very much for the insights.

Pavel A.
April 3, 2024

@AlexB99 This depends very much on your product requirements. Ability to use the debugger is a great support & recovery option. Note that the SWD connector has several good variants, from a miniature header with pins to holes & needles.  But this ability is also a security breach. A secure debugger interface is available only in recent STM32 MCUs. Most of older STM32s such as your F1 do not have secure debugging. If you choose to enable read-out protection (RDP), the debug interface will be useless.

>  I am also a noobie regarding the STM32 programming

Then please see here.

 

MM..1
Super User
April 3, 2024

Any Nucleo 1. cut upper debuger and on your board only CN counterpart required.

MM1_0-1712160110595.pngBOOT0 isnt used with SWD, but  what other tools do I need to make the USB programming possible = CubeProgrammer sw

2.you ask MCU as minimum you need choice one with USB when USB com is your plan without debuger.

3. CubeIDE ...