Skip to main content
Associate
Nov 6, 2024 11:31 AM UTC
Solved

RTC is not working properly. (Vbat related problem)

We are making a board using stm32f767nih6. There seems to be a problem with RTC and Vbat while testing the board.

First, we are using LSE with a 32.768Khz external crystal oscillator. However, there is a symptom that it slows down by about 10 seconds during approximately 40 minutes.

Second, we have set up Vbat to supply 3.3V using a coin battery. However, when the power is turned off and turned on after a certain period of time, the RTC restarts around the point where the power was turned off.

For example, when the power is turned off at 10:00 and turned on at 10:30, the time displayed on the device is 10:00.

 

Seyoung_0-1730892683758.png

 

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Nov 6, 2024 3:02 PM UTC

I have just checked the parameters of your crystal again: the CFS-20632768DZFB specifies Rs=35kohms, C0=1.2pF and CL=12.5pF (variant F).

The STM32F767 has four drive modes for the LSE: low, medium low, medium high and high. The default value is 0 (see RM0410, section 5.3.20), which results in LSEDRV[1:0]=00 = Low Drive.

I then calculated the values of the crystal according to AN2867 and obtained the following for the gain margin, which must always be above 5:

  • Low: 2.155
  • Medium Low: 3.367
  • Medium High: 7.631
  • High: 12.12

If you set the LSE drive level from Low to at least Medium High in your initialisation routine, LSE should at least work properly (assuming a suitable layout). It is important to enable write access to the backup domain beforehand. Until this is possible again in CubeMX, you can insert this after SystemClock_Config(); in the block /* USER CODE BEGIN SysInit */:

HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_MEDIUMHIGH);
HAL_PWR_DisableBkUpAccess();

Once again: the observed deviation of 10 seconds within 40 minutes will probably be reduced at best, but it may also have other reasons, e.g. the layout.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

Andrew Neil
Super User
Nov 6, 2024 11:41 AM UTC

@Seyoung wrote:

we are using LSE with a 32.768Khz external crystal oscillator.

AndrewNeil_0-1730893207538.png

That's just a crystal - not a crystal oscillator:

https://community.st.com/t5/stm32-mcus-products/stm32f4-osc-problem/m-p/664136/highlight/true#M241592

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
PGump.1
Senior II
Nov 6, 2024 12:01 PM UTC

Hi,

I think that you don't have the LSE enabled.

Kind regards
Pedro

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.
Peter BENSCH
ST Technical Moderator
Nov 6, 2024 12:20 PM UTC

@Seyoung The behaviour sounds very unusual. At first I assumed that you were inadvertently using the free-running LSI instead of the LSE as the clock source for the RTC. However, 10s deviation within 40min, which corresponds to 4167ppm, is far too much even for LSI. Perhaps you should add the programming of the RTC and LSE here.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SeyoungAuthor
Associate
Nov 6, 2024 12:25 PM UTC

1 (1).jpg

3.jpg

2 (1).jpg

PGump.1
Senior II
Nov 6, 2024 12:49 PM UTC

Hi,

I'm going to suggest the crystal capacitance loading is far too high, making it run slow, and when it switches to VBAT it stalls...

Kind regards
Pedro

 

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Nov 6, 2024 3:02 PM UTC

I have just checked the parameters of your crystal again: the CFS-20632768DZFB specifies Rs=35kohms, C0=1.2pF and CL=12.5pF (variant F).

The STM32F767 has four drive modes for the LSE: low, medium low, medium high and high. The default value is 0 (see RM0410, section 5.3.20), which results in LSEDRV[1:0]=00 = Low Drive.

I then calculated the values of the crystal according to AN2867 and obtained the following for the gain margin, which must always be above 5:

  • Low: 2.155
  • Medium Low: 3.367
  • Medium High: 7.631
  • High: 12.12

If you set the LSE drive level from Low to at least Medium High in your initialisation routine, LSE should at least work properly (assuming a suitable layout). It is important to enable write access to the backup domain beforehand. Until this is possible again in CubeMX, you can insert this after SystemClock_Config(); in the block /* USER CODE BEGIN SysInit */:

HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_MEDIUMHIGH);
HAL_PWR_DisableBkUpAccess();

Once again: the observed deviation of 10 seconds within 40 minutes will probably be reduced at best, but it may also have other reasons, e.g. the layout.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.