cancel
Showing results for 
Search instead for 
Did you mean: 

Make use of the 64k CCM

jorgen2
Associate
Posted on January 11, 2012 at 11:08

I've spent (too many) hours trying to figure out how to use the CCM for something useful.

And with useful I mean easy access from my code written in C. I use GNU GCC, etc

(the Yagarto toolchain).

At first I thought that putting some variable, array into a specified section, let's call it .ccm, (and of course the appropriate lines in the linker script) would be the solution.

For example:

uint8_t test[1024] __attribute__ ((section(''.cmm'')));

Well, it works... Kind of... :\

I compiles and links nicely. Checking the memory map/dump of the generated ELF-file I see that the array is located @0x1000 0000

However, producing a binary image produces a LARGE 100+MB file. Doing a hex-file makes it smaller but will not load into ST-Link Utility (file too large to fit, it says)

Now... That's probably due to the gap between 0x1000 FFFF and 0x2000 0000

The part in the linker script is something like (under the SECTIONS part)

.ccm :

{

  .= ALING(4);

  *(.ccm)

  .= ALIGN(4);

} >CCMRAM

And CCM is defined under MEMORY as

  CCRAM    (rwx)      : ORIGIN = 0x10000000, LENGTH = 64K

Also tried to use NOLOAD to make it NOBITS instead of PROGBITS but it still takes

up space in the binary or hex-file. Removing the section with objcopy and --remove-section .ccm does nothing to help either.

Isn't there anyway of makeing your own section behave like the .bss section and not

taking space in the image?

I hope I make sense with my problem/question.

Best regards // J�rgen

#stm32-stm32f4-ccm-linker-section #gcc-linker-ccm
This discussion is locked. Please start a new topic to ask your question.
44 REPLIES 44
carmine
Associate II
Posted on February 04, 2016 at 19:39

He is saying a completely different story. He says that the assign instruction doesn't change the content of CCM[0] location. Initialization doesn't play a role here. It's obviously that he also needs init routines for .data and .bss somewhere, but if the memory location doesn't change when he does an assign, then the linker is placing that variable elsewhere in SRAM.

Radosław
Senior III
Posted on February 04, 2016 at 19:43

So what? Linker is do  anything what he want?  NOT POSSIBLE.

This variable is propably removed by linker so value in CCRAM will not changed.

jdcowpland
Associate II
Posted on February 05, 2016 at 10:33

I don't have semihosting on, but following your thoughts, I did a read after assigning the value, and it read back the value I had written. So it looks like is actually working, and that it's the memory browser/debugger that can't read CCM or something. Thanks for the idea!

carmine
Associate II
Posted on February 05, 2016 at 11:07

Just to be sure that it's placed in CCM, you can also declare a pointer fixed to 0x10000000 location and check if the content matches.

Radosław
Senior III
Posted on February 05, 2016 at 12:21

Wow. Better solution is to creater pointer to this variable and check it is fits to CCRAM region.