Skip to main content
jorgen2
Associate
January 11, 2012
Question

Make use of the 64k CCM

  • January 11, 2012
  • 44 replies
  • 8839 views
Posted on January 11, 2012 at 11:08

I've spent (too many) hours trying to figure out how to use the CCM for something useful.

And with useful I mean easy access from my code written in C. I use GNU GCC, etc

(the Yagarto toolchain).

At first I thought that putting some variable, array into a specified section, let's call it .ccm, (and of course the appropriate lines in the linker script) would be the solution.

For example:

uint8_t test[1024] __attribute__ ((section(''.cmm'')));

Well, it works... Kind of... :\

I compiles and links nicely. Checking the memory map/dump of the generated ELF-file I see that the array is located @0x1000 0000

However, producing a binary image produces a LARGE 100+MB file. Doing a hex-file makes it smaller but will not load into ST-Link Utility (file too large to fit, it says)

Now... That's probably due to the gap between 0x1000 FFFF and 0x2000 0000

The part in the linker script is something like (under the SECTIONS part)

.ccm :

{

  .= ALING(4);

  *(.ccm)

  .= ALIGN(4);

} >CCMRAM

And CCM is defined under MEMORY as

  CCRAM    (rwx)      : ORIGIN = 0x10000000, LENGTH = 64K

Also tried to use NOLOAD to make it NOBITS instead of PROGBITS but it still takes

up space in the binary or hex-file. Removing the section with objcopy and --remove-section .ccm does nothing to help either.

Isn't there anyway of makeing your own section behave like the .bss section and not

taking space in the image?

I hope I make sense with my problem/question.

Best regards // J�rgen

#stm32-stm32f4-ccm-linker-section #gcc-linker-ccm
This topic has been closed for replies.

44 replies

Tesla DeLorean
Guru
September 29, 2014
Posted on September 29, 2014 at 04:01

I'm going to cross-link with this Keil related post for the F427 (2MB Flash, 256KB RAM - 192/64)

https://community.st.com/0D50X00009XkgpJSAR

 

Edit: Fixed DEAD LINK, original post from Sep 28 2014

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
jdcowpland
Associate III
February 4, 2016
Posted on February 04, 2016 at 16:09

Hey folks,

I'm trying to write data to the CCM RAM on my STM32F4, and as far as I can tell, I've implemented the suggestions here, but as far as I can tell it's not working. I've added the following to my linker script:

.ccm (NOLOAD) :
{
. = ALIGN(4);
*(.ccm)
*(.ccm.*)
. = ALIGN(4);
} > ram1

where ram1 is defined:

MEMORY
{
rom (rx) : ORIGIN = 0x08020000, LENGTH = 0x000dFFFF
ram (rwx) : ORIGIN = 0x20000000, LENGTH = 0x00020000
ram1 (rwx) : ORIGIN = 0x10000000, LENGTH = 0x00100000
}

In my function I then have

uint8_t CCM[1024] __attribute__((section(''.ccm'')));
CCM[0]= 0xFF;

But I see no change at location 0x10000000 in my debug memory browser. Anyone point out what I'm doing wrong?
carmine
Associate III
February 4, 2016
Posted on February 04, 2016 at 17:02

If CCM array is defined in a function, then you need to define it as static if you want to place in CCM. Otherwise, you have to ''move'' the whole stack in CCM.

jdcowpland
Associate III
February 4, 2016
Posted on February 04, 2016 at 17:04

Sorry, CCM array is actually declared as a global at the top of the c file.

Radosław
Associate II
February 4, 2016
Posted on February 04, 2016 at 17:28

 remove post

carmine
Associate III
February 4, 2016
Posted on February 04, 2016 at 17:37

Too few informations. Where do you call the ''

CCM[0]= 0xFF;

'' instruction? What about compiler optimization levels? (Try to use -ON as optimization level).

jdcowpland
Associate III
February 4, 2016
Posted on February 04, 2016 at 17:42

Sorry will try to provide more info. Optimization is turned off. I am using CooCox CoIDE. I am have a large amount of code, but at the moment am just testing trying to write to CCM, so I just have a function which is called in the main function which then attempts to write that byte to CMM.

carmine
Associate III
February 4, 2016
Posted on February 04, 2016 at 17:59

The only issue I can see (which, however, I think is not related to the your) is the LENGTH of CCM memory which is wrong (remove one zero, or write LENGTH=64K).

If you have semihosting of you can print something to an UART interface, try to printout the address of CCM array. It could be an issue related with the debugger or the memory viewer. Define also two symbols in liker script:

.ccm (NOLOAD) :
{
. = ALIGN(4);
 _sccm = .;
*(.ccm)
*(.ccm.*)
. = ALIGN(4);
 _eccm = .;
} > ram1

and see what is contained in _sccm and _eccm.
Radosław
Associate II
February 4, 2016
Posted on February 04, 2016 at 18:10

Don't say wrong information. Optimization level is no important. Garbage colector will remove this variable if it isn't used or will be optimized.

Define this variable as volatile and use it.

This linker section that you create is half of solution, becose you must remember that variable will be not initialized even if you will initialize them in code. In second hand C standard says that non initiazed variable should be '0'.

carmine
Associate III
February 4, 2016
Posted on February 04, 2016 at 19:39

He is saying a completely different story. He says that the assign instruction doesn't change the content of CCM[0] location. Initialization doesn't play a role here. It's obviously that he also needs init routines for .data and .bss somewhere, but if the memory location doesn't change when he does an assign, then the linker is placing that variable elsewhere in SRAM.