Question
Implementing the HSE on the STM32G030K6Tx
- 8 replies
- 765 views
Hi all,
I am designing a PCB using the STM32G030K6Tx and for my application I only require the HSE external crystal, which I believe I connect to GPIO pins PC14 and PC15. When I go the the .ioc file in the STM32CubeIDE (System Core -> RCC) I see there is only an option to enable the LSE and no option to enable the HSE. How do I go able enabling the HSE? I have attached an image of the relevant section of the .ioc file.