Skip to main content
spd-kalyan
Associate
Jul 16, 2025 6:54 AM UTC
Solved

Unable to read data on SPI MISO line with STM32G07 when communicating with ADS124S06.

Hii Team, 

I'm using STM32G070RBT6 MCU to communicate with ADS124S06. 
I've configured the SPI on the MCU for Mode1 and GPIOs CS, RST, START pins as output (NO pull up/ pull down) and DRDY as input (NO pull up/ pull down). 
GPIO Configuration:

spdkalyan_0-1752646887601.png

SPI Configuartion:

spdkalyan_1-1752646996937.png

spdkalyan_2-1752647055903.png

Clock Configuration: 
 

spdkalyan_3-1752647146330.png

Code : 

spdkalyan_6-1752647510127.pngspdkalyan_4-1752647346103.pngspdkalyan_5-1752647388169.png


the ADS124S06_Init function: 

 
bool ADS124S06_Init(ADS124S06_Handle *dev) {

DEBUG_PRINT("Entered init Function");

// RESET pin sequence

HAL_GPIO_WritePin(dev->reset_port, dev->reset_pin, GPIO_PIN_RESET);

HAL_Delay(1);

HAL_GPIO_WritePin(dev->reset_port, dev->reset_pin, GPIO_PIN_SET);

HAL_Delay(5);

ADS124S06_WriteRegister(dev, 0x02, 0x54); // I/p MUX: AIN5-AIN4 0x54

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x03, 0x00); // GAIN: PGA=1, 20SPS

ADS124S06_WriteRegister(dev, 0x04, 0x14); // DataRAte : 20SPS, osc-4.096MHz

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x05, 0x0A); // REF : internal 2.5V On always.

ADS124S06_WriteRegister(dev, 0x06, 0x00); // IDACMAG

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x07, 0xFF); // IDACMUX

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x08, 0x00); // VBIAS

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x09, 0x10); // SYS

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x0A, 0x00);

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x0B, 0x00);

ADS124S06_WriteRegister(dev, 0x0C, 0x00);

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x0D, 0x00);

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x0E, 0x00);

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x0F, 0x40);

ADS124S06_WriteRegister(dev, 0x10, 0x00);

HAL_Delay(1);

ADS124S06_WriteRegister(dev, 0x11, 0x00);

HAL_Delay(1);

return true;

}


bool ADS124S06_WriteRegister(ADS124S06_Handle *dev, uint8_t reg, uint8_t data) {

uint8_t cmd[3] = { ADS_CMD_WREG | (reg & 0x1F), 0x00, data };



cs_low(dev);

bool ok = HAL_SPI_Transmit(dev->hspi, cmd, 3, ADS_TIMEOUT) == HAL_OK;

cs_high(dev);

return ok;

}


in the ADS124S06_ReadRegister function I'm just doing
{
uint8_t txData[20];
uint8_t rxData[20];

txData[0] = 0x20 ; //RREG

txData[1] = 0x11;

txData[2] = 0x00;

txData[3] = 0x00;

txData[4] = 0x00;

txData[5] = 0x00;

txData[6] = 0x00;

txData[7] = 0x00;

txData[8] = 0x00;

txData[9] = 0x00;

txData[10] = 0x00;

txData[11] = 0x00;

txData[12] = 0x00;

txData[13] = 0x00;

txData[14] = 0x00;

txData[15] = 0x00;

txData[16] = 0x00;

txData[17] = 0x00;

txData[18] = 0x00;

txData[19] = 0x00;


cs_low(dev);
HAL_SPI_TransmitReceive(dev->hspi, txData, rxData, sizeof(rxData), 100);

cs_high(dev);

for (uint8_t i =0; i<20;i++)

{

DEBUG_PRINT("rxdata[%d] = 0x%02X",i, rxData[i]);

}


///////////////////////

static void cs_low(ADS124S06_Handle *dev) {

HAL_GPIO_WritePin(dev->cs_port, dev->cs_pin, GPIO_PIN_RESET);

}



static void cs_high(ADS124S06_Handle *dev) {

HAL_GPIO_WritePin(dev->cs_port, dev->cs_pin, GPIO_PIN_SET);

}



this is what I'm doing. I've configured all the SPI settings as per the datasheet of ADS124S06 and able to receive the data on MISO line,
I've verified it using logic analyser.

spdkalyan_10-1752648008683.png

written data zoom out view

spdkalyan_9-1752647972706.png

 

read data RREG

spdkalyan_7-1752647869756.png

zoom out view
spdkalyan_8-1752647899498.png


by seeing the logic analyser output, I can say that the data is available on MISO line but through firmware unable to receive/store it into buffer.
in debug mode keeping the rxData[20] in global and addded it into LiveExpressions, I'm facing an issue that rxData is not filling.

spdkalyan_11-1752648374624.png


in this only SPI1 is enabled and also uart for debugging.

spdkalyan_12-1752648439469.png


Please help me out from this issue. I hope I've given all the necessary information to debug this issue in detail, I can also provide any further information needed regarding the same.

Thank you, Kindly Please help me. 


Edited to apply source code formatting - please see How to insert source code for future reference.

This topic has been closed for replies.
spd-kalyan
spd-kalyanBest answer
Associate
Jul 18, 2025 10:39 AM UTC

Hii @Saket_Om, @Andrew Neil 

Thank you for your detailed and insightful responses regarding the SPI states.

I’m pleased to inform you that the issue has been resolved, and I can now be able to successfully receive data on rxData. The problem was traced to improper soldering at the controller end, which has been corrected now.

I sincerely apologize for my oversight. I hope that your expertise will continue to guide me in my future tests. Thank you again for your time and support.

15 replies

Andrew Neil
Super User
Jul 16, 2025 8:01 AM UTC

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results - in particular, How to insert source code.

I'll edit the post for you, but all the indentation has already been lost.

What board are you referring to?

Please show a schematic of how the ADS124S06 is connected; some goof, clear photos of your setup would also help.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Jul 16, 2025 8:08 AM UTC

Here:

HAL_SPI_TransmitReceive(dev->hspi, txData, rxData, sizeof(rxData), 100);

The length needs to be the total length of the transaction - both transmit and receive.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
spd-kalyan
Associate
Jul 16, 2025 10:27 AM UTC

Thanks for the response. 
I'm referring to STM32G070RBT6.
Let's keep it short. I'm gonna read only single register value. So, according to ADS124S06 datasheet, to read register value, we should use RREG command (0x20 | regAddress, 0x00) 

//Reads Single Register

uint8_t ADS124S06_ReadRegisters(ADS124S06_Handle *dev)
{
 uint8_t txData[3];
 // Prepare RREG command
 txData[0] = 0x22 ; // (0x20 | 0x02) = 0x22
 txData[1] = 0x00; // no.of register - 1 = (1-1) = 0x00
 txData[2] = 0xFF; // dummy data to receive value
 // Pull CS low to start communication
 cs_low(dev);
 HAL_SPI_TransmitReceive(dev->hspi, txData, rxData, 3, 100);
 cs_high(dev);
 return rxData[2];
}

When I run this code, I got the output in logic analyser as given Screenshot 

spdkalyan_2-1752660552989.png
same SPI lines are connected to logic analyser lines, and the screenshot shows us the data on MISO line. 
I'm transmitting 2 bytes and receiving 1 Byte. So, the total size I've given was 3. 

spdkalyan_6-1752661789198.png

rxData[3] is not being updated. 



Sorry, I'm unable to provide the setup pictures. 
schematic lines from the ADC to STM32G070RBT6.

spdkalyan_3-1752661314863.png
pullups are added for these three lines.

spdkalyan_4-1752661363939.png

spdkalyan_5-1752661667786.png


Thank you. 

 

 

 

Andrew Neil
Super User
Jul 16, 2025 10:30 AM UTC

@spd-kalyan wrote:

I'm transmitting 2 bytes and receiving 1 Byte. So, the total size I've given was 3. 


And that's working?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
spd-kalyan
Associate
Jul 16, 2025 10:41 AM UTC

Hardware is working fine as we're seeing the output in logic analyser, but the firmware side is the problem. 

I want the data to be stored in rxData buffer, but it is not happening. only 0x00 are in rxData buffer.

uint8_t ADS124S06_ReadRegisters(ADS124S06_Handle *dev)
{
 uint8_t txData[3];
 // Prepare RREG command
 txData[0] = 0x22 ;
 txData[1] = 0x00;
 txData[2] = 0xFF;
 // Pull CS low to start communication
 cs_low(dev);
 HAL_SPI_TransmitReceive(dev->hspi, txData, rxData, 3, 100);
 cs_high(dev);
 return rxData[2];
}

//expected output.
rxData[0] = 0x00;
rxData[1] = 0x00;
rxData[2] = 0x54;

//actual output. 
rxData[0] = 0x00;
rxData[1] = 0x00;
rxData[2] = 0x00;

logic Analyser output. 

spdkalyan_0-1752662629980.png

zoom-out view

spdkalyan_1-1752662669608.png

 

 

spd-kalyan
Associate
Jul 17, 2025 6:18 AM UTC

Hii @Andrew Neil, Good morning,

I also tried with Transmit and receive individual calls, and also on interrupt mode. Data on MISO line is visible but not in rxData buffer. 

uint8_t ADS124S06_ReadRegisters(ADS124S06_Handle *dev)
{
 uint8_t txData[2];
 // Prepare RREG command
 txData[0] = 0x22 ;
 txData[1] = 0x00;
// txData[2] = 0xFF;
 // Pull CS low to start communication
 cs_low(dev);
// HAL_SPI_TransmitReceive(dev->hspi, txData, rxData, 3, 100);
// HAL_SPI_TransmitReceive_IT(dev->hspi, txData, rxData, 3);
 HAL_SPI_Transmit(dev->hspi, txData, 2, 100);
 HAL_SPI_Receive(dev->hspi, rxData, 1, 100);
 cs_high(dev);
 return rxData[0];
}

Kindly, let me know anything specific to be changed. 

logic analyser output. 

spdkalyan_2-1752732886522.png


STMCubeIDE Debug mode Live expressions

spdkalyan_3-1752732959459.png

Also tried transmitting the rxData on UART and checked in serial monitor, still the value is 0x00.

What should I do? I'm with no clue and helpless. Please help me out. Thank you.

 

. 

Andrew Neil
Super User
Jul 17, 2025 8:57 AM UTC

Are you sure the signal is actually reaching the STM32 pin?

Probe directly on the pin of the STM32 package.

Can you read both high & low with the pin configured just as a GPIO input?

Have you tested this on a standard devboard?

Maybe try bit-banging ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
spd-kalyan
Associate
Jul 17, 2025 9:56 AM UTC

Hii @Andrew Neil, 

I wanted to share some observations from my recent tests with the STM32 MISO pin and the ADS124S08EVM. During my testing to verify if the MISO pin on the STM32 was functioning correctly, I shorted the MISO and MOSI pins to create a loopback while the ADC was also connected. Surprisingly, instead of receiving the data sent on the MOSI line, I received the expected data from the ADC. This was unexpected, and I'm curious about the reason behind this behavior.

Additionally, I noticed a difference in the MISO line behavior between the STM32 and the ADS124S08EVM. When using the ADS124S08EVM as a reference, the MISO line is initially high and goes low when data is received (high on pulses). However, with the STM32, the MISO line remains low and only goes high during pulses. Could this difference in the MISO line's idle state (high vs. low) be related to the issue? I've attached images for your reference.

STM32 Connected with ADS124S06 in parallel with logic analyser.

spdkalyan_0-1752746145603.png
ADS124S08EVM SPI line connected with logic anaylser.

spdkalyan_1-1752746216643.png

 

 

ST Technical Moderator
Jul 17, 2025 2:51 PM UTC

Hello @spd-kalyan 

Could you try with the below configuration:

HAL_SPI_TransmitReceive(dev->hspi, (uint8_t *)txData, (uint8_t *)rxData, 3, 100);
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
spd-kalyan
Associate
Jul 18, 2025 4:51 AM UTC

Hii @Saket_Om, Thanks for your time. 

I tried with the data type you've given too, but the rx_buf is not being updated. 
In my observations this issue is based on configuration of SPI. I'm expecting MISO line to be high in idle. 

spd-kalyan
spd-kalyanAuthorBest answer
Associate
Jul 18, 2025 10:39 AM UTC

Hii @Saket_Om, @Andrew Neil 

Thank you for your detailed and insightful responses regarding the SPI states.

I’m pleased to inform you that the issue has been resolved, and I can now be able to successfully receive data on rxData. The problem was traced to improper soldering at the controller end, which has been corrected now.

I sincerely apologize for my oversight. I hope that your expertise will continue to guide me in my future tests. Thank you again for your time and support.

Andrew Neil
Super User
Jul 18, 2025 11:20 AM UTC

@spd-kalyan wrote:

Thank you for your detailed and insightful responses regarding the SPI states..


You're welcome!

 


@spd-kalyan wrote:

The problem was traced to improper soldering at the controller end, which has been corrected now.


That was the reason behind this.

 

#ProbeAtThePin

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.