Skip to main content
Senior
August 11, 2025
Question

Stm32U031 -- Problems waking from STOP2 with EXTI

  • August 11, 2025
  • 11 replies
  • 1461 views

Howdy;

I have a li'l stm32u031, with a pushbutton attached to PA0. This MCU is clocked with no external oscillators. 

I've configured the button/pin to work with Timer2/Channel1 in Input Capture mode when the MCU is in run mode, to detect and measure button presses. This works swell. 

I'd like to be able to put this device into STOP2 mode, and be able to re-awaken it with the button. My understanding is that I'd do this by de-initing it as an alt function pin, and re-initing it for EXTI. 

At the moment, I'm doing this:

 // Stop all timer channels
 HAL_TIM_IC_Stop_IT(&htim2, TIM_CHANNEL_1);
 HAL_TIM_OC_Stop_IT(&htim2, TIM_CHANNEL_2);
 HAL_TIM_OC_Stop_IT(&htim2, TIM_CHANNEL_3);

 // Stop the timer itself
 HAL_TIM_Base_Stop(&htim2);

 // Mask any stray interrupts and clear latched flags
 __HAL_TIM_DISABLE_IT(&htim2, TIM_IT_UPDATE | TIM_IT_CC1 | TIM_IT_CC2 | TIM_IT_CC3 | TIM_IT_CC4);
 __HAL_TIM_CLEAR_FLAG(&htim2, TIM_FLAG_UPDATE | TIM_FLAG_CC1 | TIM_FLAG_CC2 | TIM_FLAG_CC3 | TIM_FLAG_CC4 |
 TIM_FLAG_CC1OF | TIM_FLAG_CC2OF | TIM_FLAG_CC3OF | TIM_FLAG_CC4OF);

 // Switch NVIC off + clear any pending interrupts
 // to avoid surprise ISR on resume
 NVIC_DisableIRQ(TIM2_IRQn);
 NVIC_ClearPendingIRQ(TIM2_IRQn);

 // Disconnect the peripheral clock for a few extra µA
 __HAL_RCC_TIM2_CLK_DISABLE();

 // Now we are going to configure our
 // button to create an interrupt when pressed
 // using EXTI instead of our timer.

 // We are going to de-init our pin
 // which disconnect it from Timer2.
 HAL_GPIO_DeInit(MAIN_BUTTON_GPIO_Port, MAIN_BUTTON_Pin);

 // Then re-configure it thusly:
 GPIO_InitTypeDef gpio_config = {0};
 gpio_config.Pin = MAIN_BUTTON_Pin;
 gpio_config.Mode = GPIO_MODE_IT_RISING;
 gpio_config.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(MAIN_BUTTON_GPIO_Port, &gpio_config);

 // Clear any stale pending before sleeping
 __HAL_GPIO_EXTI_CLEAR_IT(MAIN_BUTTON_Pin);

 NVIC_ClearPendingIRQ(EXTI0_1_IRQn);
 HAL_NVIC_SetPriority(EXTI0_1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI0_1_IRQn);


 // now, sleepytime:
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
 RCC->CFGR |= RCC_CFGR_STOPWUCK;
 HAL_SuspendTick();
 HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);

This only partially works - I can put it to sleep, then wake it up a time or two using this button. But eventually it seems to get 'stuck' in STOP2, and the button presses no longer work. This behavior is repeatable, but the 'number of wakeups" I seem to be able to perform changes each time I restart the device - sometimes it won't wake up at all, sometimes I get 2-3 wakeups before it stops working. 

I've tried all manner of mucking around using the higher-level HAL stuff, as well as individual LL syntax, but I can't quite seem to fix this problem, nor do I understand why it's happening. This line:

 RCC->CFGR |= RCC_CFGR_STOPWUCK;

I found in this thread, where someone else seemed to be having a similar problem (maybe), but it doesn't seem to affect the experience I'm having. 

I'm curious if anyone might have some advice.

thanks!

 

This topic has been closed for replies.

11 replies

ST Technical Moderator
August 12, 2025
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
sb_stAuthor
Senior
August 12, 2025

Thanks @Saket_Om!

It seems that what's causing me trouble is trying to rebuild the system clock after coming out of Stop2. 

Initially, I was doing this:

SystemClock_Config();

immediately after coming out of stop2. Your example shows something slightly different, which I've modified to fit my own clock panel settings:

static void resume_clocks() {

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 uint32_t pFLatency = 0;

 /* Enable Power Control clock */
 __HAL_RCC_PWR_CLK_ENABLE();

 /* Get the Oscillators configuration according to the internal RCC registers */
 HAL_RCC_GetOscConfig(&RCC_OscInitStruct);

 /* After wake-up from STOP reconfigure the system clock: Enable HSI. 
 Note in my setup, I do not use PLL */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_11;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Get the Clocks configuration according to the internal RCC registers */
 HAL_RCC_GetClockConfig(&RCC_ClkInitStruct, &pFLatency);

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV16;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }

 HAL_InitTick(TICK_INT_PRIORITY);
 HAL_ResumeTick();
}

In either case, I experience this "works a few times, then stops working" behavior, where I can successfully put the device into stop2, but can no longer awaken it. 

However, I notice that if I completely skip this clock configuration step, and just simply go straight to:

 HAL_InitTick(TICK_INT_PRIORITY);
 HAL_ResumeTick();

this "sometimes it works, sometimes it doesn't" behavior goes away completely...the device can be put to sleep and successfully awakened repeatedly with no issues. 

This seems quite strange to me - most resources I can find say that it's absolutely mandatory to do this clock-rebuilding step, and I can't quite understand why skipping it completely seems to make my system stable. 

FWIW, the way I am testing this is by simply turning on an LED after coming out of sleep immediately after the above.

 

ST Technical Moderator
August 13, 2025

Hello @sb_st 

To assist you more efficiently, could you please share your project with us?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
sb_stAuthor
Senior
August 14, 2025

To try to add info after further testing:

I can enter SLEEP mode using my current logic, and come out of it fine.

HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI);

but entering any of Stop0, Stop1 or Stop2 modes seems to 'trap' the device, and I'm unable to consistently wake it:

HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);

 

ST Technical Moderator
August 15, 2025

Hello @sb_st 

I tried to implement your scenario based on the example STM32CubeU0/Projects/NUCLEO-U083RC/Examples/PWR/PWR_STOP2 at main · STMicroelectronics/STM32CubeU0 · GitHub

It works fine on my end. Please find the main file attached.

I used the same system clock config as in the example and I set the GPIO pull configuration to gpio_config.Pull = GPIO_PULLUP for GPIO EXTI in main_button_standby().

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
sb_stAuthor
Senior
August 15, 2025

I found what seems like a smoking gun. 

My system uses RNG, which - by default - is clocked by MSI. I notice that when I disable RNG, this odd behavior goes away completely. When I configure the RNG to be clocked by PLLQ instead of MSI, this also seems to get rid of the problematic behavior. 

I'm attaching files exemplifying these three scenarios here. 

Screenshot 2025-08-15 at 6.09.37 AM.png

Screenshot 2025-08-12 at 11.36.52 AM.png

I am still trying to understand what I might be missing in the MSI case that causes this sporadic hanging, and whether there's a way to solve this (mostly because I am interested in learning - it makes me feel a little itchy to just switch to PLLQ without clearly understanding why that works and the MSI case does not). 

ST Technical Moderator
August 20, 2025

Hello @sb_st 

Did you change the GPIO pull configuration of EXTI button to GPIO_PULLUP?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
sb_stAuthor
Senior
August 29, 2025

To be honest, I don't remember - I tried a ton of stuff to make this work, and eventually landed on the issue I highlighted here, which identified my issue as being related to using the RNG peripheral. I think the GPIO switching from timer to EXTI was not actually the root of my problems. 

My work around, also mentioned in that post - clocking RNG from PLLQ rather than MSI - got my system behavior in a more stable manner. Why this is I'm