Skip to main content
Associate III
Jun 9, 2025 10:25 AM UTC
Solved

Read/Write file into eMMC using Fatfs on STM32H750B-dk

Hello,
I am working on a project using the STM32H750B-DK board with an eMMC storage device, interfaced via the SDMMC1 peripheral and the FatFs library for file operations. However, I am unable to read or write files to the eMMC.

I have implemented the drivers and example code from `~\STM32Cube_FW_H7_V1.12.1\Projects\STM32H745I-DISCO\Applications\FatFs\FatFs_Shared_Device` and `~\STM32Cube_FW_H7_V1.12.1\Drivers\BSP\STM32H750B-DK`, but we are still unable to create files or perform read/write operations on the eMMC (4GB).

I am sharing my project zip file. Any guidance on adjustments or in configuration can be a big help.
Thank You.

This topic has been closed for replies.
Prajyot1Best answer
Associate III
Jun 11, 2025 12:11 PM UTC

UPDATE:
i was able to create files or perform read/write operations on the eMMC (4GB) using `~\STM32Cube_FW_H7_V1.12.1\Projects\STM32H745I-DISCO\Applications\FatFs\FatFs_Shared_Device` and `~\STM32Cube_FW_H7_V1.12.1\Drivers\BSP\STM32H750B-DK`. the low level i/o implementation was wrong.

7 replies

Andrew Neil
Super User
Jun 9, 2025 10:57 AM UTC

What tests/investigations/debugging have you done to find where/why it's failing ?

Does it build cleanly - ie, with no errors and no warnings?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Prajyot1Author
Associate III
Jun 9, 2025 11:25 AM UTC

@Andrew Neil 
Yes , we have build the project without errors.

i have customize diskio.c for eMMC
Action: Modified diskio.c to interface with the STM32H750B-DK’s SDMMC peripheral using the HAL MMC driver.
In diskio.c , implemented the required functions (disk_initialize, disk_status, disk_read, disk_write, disk_ioctl) to call HAL functions from stm32h7xx_hal_mmc.c.

while  debugging:

fres = f_mkfs("", FM_ANY, 0, workBuffer, sizeof(workBuffer));
 if (fres != FR_OK) {
 printf("f_mkfs failed: %d\n", fres);
 }

 i got fres = FR_DISK_ERR.


Andrew Neil
Super User
Jun 9, 2025 11:55 AM UTC

@Prajyot1 wrote:

 i got fres = FR_DISK_ERR.


So have you looked-up what that error code means?

Have you stepped into f_mks() to see where & why it fails?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Jun 12, 2025 8:02 AM UTC

@Prajyot1 Thanks for marking the solution.

Your new question has been split to a new thread: STM32H750B-dk: access eMMC through USB OTG.

Please keep to one question per thread.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.