Skip to main content
MKash.3
Visitor II
Mar 2, 2026 4:13 AM UTC
Solved

Can't find FATFS Middleware option for STM32U5 SPI SD Card Integration in CubeMx

Dear ST Community,

I hope you are doing well.

I am currently working with the STM32U5 development board and would like to integrate an SD card module using SPI communication.

However, while configuring my project in STM32CubeMX / CubeIDE, I was unable to find the FATFS middleware option under the middleware section. My goal is to use FATFS with an SD card operating in SPI mode.

Could you please guide me on how to enable or integrate FATFS for SPI-based SD card communication on the STM32U5 series? If manual integration is required, I would appreciate any official documentation, example projects, or recommended procedures.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 6, 2026 11:25 AM UTC

Hello,

From this post it seems U5 supports only FileX but not FATFS in CubeMx.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

3 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 6, 2026 11:25 AM UTC

Hello,

From this post it seems U5 supports only FileX but not FATFS in CubeMx.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Mar 6, 2026 11:34 AM UTC

@mƎALLEm wrote:

U5 supports only FileX but not FATFS.


You mean, ST only provides FileX in a ready-to-go format for the U5.

 

@MKash.3  There is nothing in the U5 itself to prevent it running FatFs - just like any other microcontroller.

FatFs is not limited to any particular microcontroller or architecture:

https://elm-chan.org/fsw/ff/

 

See also: 

https://community.st.com/t5/stm32cubemx-mcus/fatfs-middleware-for-stm32u5-mcus/m-p/884252/highlight/true#M35350

 

PS:

Some more embedded file system options here.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
Mar 6, 2026 12:04 PM UTC

The OP is asking for STM32U5/FatFS configuration in CubeMx.

It's obvious FatFS could run on STM32U5 but there is no ready to use FatFS example on that series. The user needs to port FatFS to STM32U5 himself.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.