Skip to main content
Associate II
January 21, 2026
Solved

Why are there two holes under the MCU on NUCLEO-G474RE ?

  • January 21, 2026
  • 9 replies
  • 739 views

I noticed two holes at Bottom of the MCU area on the STM32G4 Nucleo board. What is their purpose?stm32 g4.jpeg

Best answer by Kavi

yes, now i can understand the purpose.

thank you :)

stmcusocket.jpg

9 replies

Andrew Neil
Super User
January 21, 2026

I see it also on Nucleo-L476RG (haven't checked further).

 

I don't know, but I think it might be to facilitate a QFP socket?

ISTR seeing some early Nucleos with sockets - probably used only internally by ST?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
KaviAuthor
Associate II
January 21, 2026

I’m developing a custom board for my application, so I need clarification on the purpose of these holes before deciding whether to include them in my PCB.

Andrew Neil
Super User
January 21, 2026

There is no need to have them on a target board.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
waclawek.jan
Super User
January 21, 2026

As @Andrew Neil said, it's for a ZIF socket. It's even listed in the BOM 

HW110Yamaichi socket for LQFP64, with positioning pins.LQFP64YAMAICHIIC149-064-169-B5Not Fitted0

It's not populated on the boards which are sold to the public, but ST uses them for development internally.

JW

Andrew Neil
Super User
January 21, 2026

Well spotted!

 

@Kavi I suspect that's also what the four solder pads at the corners of the QFP footprint are for:

AndrewNeil_0-1768999931927.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
January 21, 2026

@Andrew Neil wrote:

@Kavi I suspect that's also what the four solder pads at the corners of the QFP footprint are for:

AndrewNeil_0-1768999931927.png

 


I confirm.. these solder pads are used to solder the socket.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
February 24, 2026
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.