Skip to main content
Associate II
October 23, 2023
Question

the windows computer recognized the st-link v2 as universal serial bus instead virtual port

Hi.

After firmware upgrade for st-link v2, windows computer recognized the st-link as universal serial bus instead of virtual com port. whenever i try to program to MCU, there is error like a "No target device found".

How can I solve it?

Below image is the device manager to be recognized as Universal serial bus. there is no PORT.

 

ST-Link V2.PNG

 

Thank advance.

BR

 

This topic has been closed for replies.

21 replies

Peter BENSCH
ST Technical Moderator
October 23, 2023

Welcome @kevin1971, to the community!

Which software and settings did you use for the firmware upgrade?
Can you please also upload a photo of your ST-LINK/V2 here?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
kevin1971Author
Associate II
October 23, 2023

Hi.

Below is the image which I have used.

st-link.PNG

utility.PNG

AScha.3
Super User
October 23, 2023

try with stm32CubeProgrammer . (st-link utility is outdated.)

If you feel a post has answered your question, please click on " Best Answer ".
kevin1971Author
Associate II
October 23, 2023

Hi.

I tried to program in the cubeISE using above st-link v2, the error message is "no target device found".

In this regard, if i use the stm32CubeProgrammer, will it work to program?

 

Thank you.

BR

 

Peter BENSCH
ST Technical Moderator
October 23, 2023

You have used the ST-LINK utility, which is long out of date and on NRND (Not Recommended for New Designs). The firmware is also outdated and should be updated with STM32CubeProg.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
kevin1971Author
Associate II
October 23, 2023

Hi

 

Below is the upgrade using CubeProgrammer after install it.

upgrade.PNG

 

However,

If i tried to program with connect, below is error message which i got.

 

connect.PNG

 

Thank advance

BR

 

AScha.3
Super User
October 23, 2023

so st-link working now. ok.

but target shows 0 V only - now power on target ! (or you didnt connect VDD ( 3,3V )to st-link .

connect 3,3 V to target !

If you feel a post has answered your question, please click on " Best Answer ".
Tesla DeLorean
Guru
October 23, 2023

Show how this is connected to your target. Needs VCC, GND, SWDIO, SWCLK minimum.

This type of ST-LINK/V2 does NOT provide a COM Port / VCP

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
kevin1971Author
Associate II
October 23, 2023

Powre is up with 3.07V. however, no stm32 target found as below image.

power.PNG

My SWIO, SWCLK, VDD, RST as below schematic. 

VDD : 1

SWIO : 7

SWCLK : 9

RESET : 15

GND : 4

ST.PNG

 

 

 

 

 

Thanks in advance.

Regards

 

Tesla DeLorean
Guru
October 23, 2023

Ok, but the diode suggests that you expect the ST-LINK to power the 3.3V whereas the expectations for the buffers is that your target powers them. Check the voltage you see on pin 1/2 of the 20-pin header

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
kevin1971Author
Associate II
October 23, 2023

Hi Tesla,

You mean that the target board should provide the power 3.3V to the st-link VDD pin 1/2 of the 20-pin header.

or,Is 3.07V little bit low voltage for flashing?

 

Thanks

Regards,

kevin1971Author
Associate II
October 24, 2023

Hi 

After measuring the voltage of 1/2 of 20-pin header with tester,  the value of voltage is 3.13V.

Thank you.

Regards,

kevin1971Author
Associate II
October 25, 2023

Hi,

MCU is STM32L072CZ.

Boot0 is to wired with GND. Now Voltage is 3.25V for VDD : 3.25V, SWDIO, SWCLK, nRST, RST.

Even if I tried to connect with My MCU Board which housed STM32L072CZ, it didn't connect with them.

Please help me.

 

thank you in advance.

Kevin