Skip to main content
Associate
April 21, 2026
Question

NUCLEO-U5A5ZJ-Q and nRF7002 interface using vanillas Zephyr

Hello STM team,

 

We are working to interface the  NUCLEO-U5A5ZJ-Q and nRF7002-DK using QSPI. We are using vanillas zephyr. We are able to built the code for SPI. But can not be able to built for QSPI. It will be very helpful if you provide a proper support to interface this.

19 replies

Andrew Neil
Super User
April 21, 2026

Welcome to the forum.

Please give some more details of your setup - see:

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
April 21, 2026

IDE: vanilla zephyr

STM32: NucleoU5A5ZJ-Q

nRF-wifi: nRF7002-DK kit

Interface protocol: QSPI

Code: Shell test code (From list of example code in IDE)

 

I am able to built the shell code for STM32 successfully. That is working on SPI protocol.

I want to use QSPI protocol. For that I have added the overlay file to configure the QSPI pins of the NucleoU5A5ZJ (Overlay file is attached already). In overlay file the nRF7002 accepts the SPI, QSPI or Coaxe instance. And NucleoU5A5ZJ is having OctoSPI.

/*
 * Copyright (c) 2023 STMicroelectronics
 *
 * SPDX-License-Identifier: Apache-2.0
 */
/ {
	chosen {
		zephyr,wifi = &wlan0;
	};
};

&octospi1 {
	pinctrl-0 = <&octospim_p1_clk_pa3 &octospim_p1_ncs_pa2 &octospim_p1_dqs_pa1
				 &octospim_p1_io0_pb1 &octospim_p1_io1_pb0 
				 &octospim_p1_io2_pa7 &octospim_p1_io3_pa6 
				 &octospim_p1_io4_pc1 &octospim_p1_io5_pc2
				 &octospim_p1_io6_pc3 &octospim_p1_io7_pc0>;

	pinctrl-names = "default";

	dmas = <&gpdma1 0 7 0x10440>,
		 <&gpdma1 1 6 0x10480>;
	dma-names = "tx","rx";

	nrf70: &octospi1 {
		compatible = "nordic,nrf7002-spi";
		status = "okay";
		reg = <0>;
 
		/* Control GPIOs - using available pins that don't conflict */
		iovdd-ctrl-gpios = <&gpiob 7 (GPIO_ACTIVE_HIGH | GPIO_PULL_DOWN)>; /* D0 */
		bucken-gpios = <&gpiob 6 (GPIO_ACTIVE_HIGH | GPIO_PULL_DOWN)>; /* D1 */
		host-irq-gpios = <&gpiog 12 GPIO_ACTIVE_HIGH>; /* D7 */
		/* List of interfaces */
		wlan0: wlan0 {
			compatible = "nordic,wlan";
		};
		/* Wi-Fi TX power limits */
		wifi-max-tx-pwr-2g-dsss = <21>;
		wifi-max-tx-pwr-2g-mcs0 = <16>;
		wifi-max-tx-pwr-2g-mcs7 = <16>;
		wifi-max-tx-pwr-5g-low-mcs0 = <13>;
		wifi-max-tx-pwr-5g-low-mcs7 = <13>;
		wifi-max-tx-pwr-5g-mid-mcs0 = <13>;
		wifi-max-tx-pwr-5g-mid-mcs7 = <13>;
		wifi-max-tx-pwr-5g-high-mcs0 = <12>;
		wifi-max-tx-pwr-5g-high-mcs7 = <12>;
	};

	status = "okay";
};

// &spi1 {
// 	status = "okay";
// 	pinctrl-0 = <&spi1_sck_pa1 &spi1_miso_pa11 &spi1_mosi_pa12>;
// 	pinctrl-names = "default";
// 	cs-gpios = <&gpiod 14 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
// 	/* High speed SPI configuration for STM32H7 */
// 	clock-frequency = <DT_FREQ_M(50)>; /* 50MHz SPI clock */
 
// 	nrf70: nrf7002-spi@0 {
// 		compatible = "nordic,nrf7002-spi";
// 		status = "okay";
// 		reg = <0>;
// 		spi-max-frequency = <DT_FREQ_M(8)>; /* Increased from 8MHz to 16MHz */
 
// 		/* Control GPIOs - using available pins that don't conflict */
// 		iovdd-ctrl-gpios = <&gpiob 7 (GPIO_ACTIVE_HIGH | GPIO_PULL_DOWN)>; /* D0 */
// 		bucken-gpios = <&gpiob 6 (GPIO_ACTIVE_HIGH | GPIO_PULL_DOWN)>; /* D1 */
// 		host-irq-gpios = <&gpiog 12 GPIO_ACTIVE_HIGH>; /* D7 */
// 		/* List of interfaces */
// 		wlan0: wlan0 {
// 			compatible = "nordic,wlan";
// 		};
// 		/* Wi-Fi TX power limits */
// 		wifi-max-tx-pwr-2g-dsss = <21>;
// 		wifi-max-tx-pwr-2g-mcs0 = <16>;
// 		wifi-max-tx-pwr-2g-mcs7 = <16>;
// 		wifi-max-tx-pwr-5g-low-mcs0 = <13>;
// 		wifi-max-tx-pwr-5g-low-mcs7 = <13>;
// 		wifi-max-tx-pwr-5g-mid-mcs0 = <13>;
// 		wifi-max-tx-pwr-5g-mid-mcs7 = <13>;
// 		wifi-max-tx-pwr-5g-high-mcs0 = <12>;
// 		wifi-max-tx-pwr-5g-high-mcs7 = <12>;
// 	};
// };

Problem statement: Need to know how can we connect the OctoSPI with the nRF7002 in the overlay file. We tried to use OctoSPI instance with nRF7002, but it throughs error when built.

nRF accept SPI, QSPI or Coaxe instance only.

While NucleoU5A5ZJ supports SPI and OctoSPI.

Andrew Neil
Super User
April 21, 2026

Please show the schematic of how you have the nRF7002 connected to the Nucleo.

 

Is the nRF7002 on an eval board, or similar?

EDIT: It's an nRF7002-DK - see follow-up questions below.

 


@ElectrifyServices wrote:

I am able to built the shell code for STM32 successfully. That is working on SPI protocol.


So you have the nRF7002 working OK in SPI mode?

 


@ElectrifyServices wrote:

We tried to use OctoSPI instance with nRF7002, but it throughs error when built.


Please show the error(s) that you get.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
April 21, 2026

@Andrew Neil wrote:

Is the nRF7002 on an eval board, or similar?


Sorry, you did say it's an nRF7002-DK.

So this: https://www.nordicsemi.com/Products/Development-hardware/nRF7002-DK

 

That kit includes an nRF5340 SoC as host processor for the nRF7002 - so are you sure you've fully disconnected that to allow your STM32 to be the host?

Have you confirmed your hardware setup with Nordic?

https://devzone.nordicsemi.com/

 

PS:

Have you got OctoSPI working with the nRF5340 ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Pavel A.
April 22, 2026

Documentation brief for the nRF7002-DK says that the DK has its own host MCU.

There's no indication that the nRF7002 chip of the DK can be connected to external host.

 

 

Associate
April 22, 2026

Hello Pavel,

Yes, the nRF7002-DK has the nRF5340 as the on board host MCU.

I have not run the code on the hardware setup yet. I need to check the nRF7002-DK documents for that.

I have ordered the nRF7002-EK already. Once I receive that board I can test on it. This is just to get start with existing hardware available with me.

Associate
April 23, 2026

I have a update in this project.

I received the nRF7002-EK board. I make the all necessary connection between NucleoU5A5ZJ-Q and nRF7002-EK. 

I test the shell code working on SPI interface and that get worked.

So now, I am able to operate the nRF7002 using STM32 board using SPI protocol. I am able to scan the available wifi and also get connected to one of it. This is working fine.

So now coming to a same page, My hardware setup is tested and working fine for SPI interface.

Now, I just need to figure out how to port the shell example code to work on QSPI.

image.pngimage.png 

nRF7002-EK: https://www.nordicsemi.com/Products/Development-hardware/nRF7002-EK
NucleoU5A5ZJ-Q: https://www.st.com/en/evaluation-tools/nucleo-u5a5zj-q.html

 

Andrew Neil
Super User
April 23, 2026

Is there a Nordic/Zephyr example which demonstrates using the nRF7002 over QSPI ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
April 23, 2026

no there is no example code that demonstrate using the nRF7002 over QSPI.

 

Andrew Neil
Super User
April 23, 2026

@ElectrifyServices wrote:

no there is no example code that demonstrate using the nRF7002 over QSPI.


Might be worth asking Nordic to provide it, then - or, at least, to give guidance.

 

Do you really need QSPI - is SPI not sufficient ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
April 23, 2026

I have already ask with Nordic team. But they are taking time to reply back. And also not helping me to solve the problem. I don't know if they support the other host MCU to get work with nRF7002 via QSPI ?image.png

 

Yes, I require to work on QSPI instead of SPI protocol. As QSPI is more faster compared to SPI. Our application requires speed.

Associate
August 7, 2026

Could you please tell me if this problem has been resolved? I'm also looking for a similar solution. 

thanks~

Andrew Neil
Super User
August 7, 2026
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.