Skip to main content
Associate
December 17, 2024
Question

Issues with VNQ9080AJTR Quad-Channel high-side driver Output and Input Behavior.

Hello STM Community,

I'm currently working with the VNQ9080AJTR Quad Channel High-Side Driver, and I'm encountering a couple of issues that I hope someone here can help me resolve

1.Output Voltage Regulation: With a constant VCC supply of 12V, the output of the IC is randomly regulated to 7-8V instead of maintaining a stable 12V output. This issue seems to occur intermittently, and I can't pinpoint a specific trigger for when it happens. Has anyone experienced similar behavior? What could be causing the output voltage to drop unexpectedly?

2.Input Pin Voltage: I have connected the input pin (which is supposed to take signals from the microcontroller) to control the driver, but at times, I'm reading 7-8V at this input pin instead of the expected logic-level voltage.

For both issues, I’ve verified my connections and ensured proper grounding. The behavior is random, making troubleshooting difficult.

Datasheet : https://www.st.com/resource/en/datasheet/vnq9080aj.pdf

This topic has been closed for replies.

4 replies

MBONA.1
ST Employee
December 17, 2024
Dear Divyansh12,
 
 there is something strange on this behavior.
 
To support you we need to have a schematic and more information.
 
Waiting for your feedback.
 
BR
 
 
 
Associate
December 21, 2024

Hello,

Please find the schematic attached below for the IPD.Screenshot 2024-12-21 132141.png

Associate
October 3, 2025

Hi, I've got same and similar issues with VNQ9080. I get about 3V on outputs, in other case three outputs work well, the fourth is all time on 7V, with input to ground. I hope somebody from ST will help us. 

Peter BENSCH
ST Technical Moderator
October 13, 2025

@stojank You can find the answer to your question here.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.