Skip to main content
Associate III
Sep 25, 2024 8:28 PM UTC
Solved

Unable to connect to STM32H523

Hi,

I am trying to connect to a STM32H523RET MCU via SWD using a J-link Debugger (CubeProgrammer v2.17.0).
Reading the Product ID fails, so I get asked to select the MCU manually.

WhoIsJohnGalt_2-1727295663441.png

Unfortunately the list does not contain any STM32H52x MCU

WhoIsJohnGalt_3-1727295706101.png

 

But when I am trying to connect via Jlink - Commander I can find der MCU in the list and also connect to it:

WhoIsJohnGalt_0-1727295541006.png

WhoIsJohnGalt_1-1727295559401.png

Does anybody have an idea, why I can't find the MCU in the list when using the CubeProgrammer?

Thanks for any hints.

Regards

John

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Oct 2, 2024 2:34 PM UTC

Hi @WhoIsJohnGalt ,

After check, this issue is related to the access port when connecting with J-Link and will be fixed in the upcoming release of STM32CubeProgrammer.

For now, you can manually change the access port from 0 to 1, which should resolve the issue with the current version.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

8 replies

ST Technical Moderator
Sep 25, 2024 9:15 PM UTC

Hello @WhoIsJohnGalt ,

Try connecting with other MCU to check if the problem is reproduced with the tools used.

Try to “Connect Under Reset” mode.

Does your J-Link connect to any other STM32 targets?

Check these links that may help you:

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Associate III
Sep 26, 2024 8:25 AM UTC

Thanks for your quick response.

The first link I already checked and the connection with the jlink-commander does work fine (see first post screenshots). So therefore I assume the SWD lines are connected correctly.
(Unrelated side note: connecting via USB-DFU in CubeProgrammer also works fine)

 

CubeProgrammer:
Trying to connect with "Connect Under Reset" mode + "Software Reset" leads also to a failed PRODID read (as shown in first post".

 

I will check the value off the pull down capacitor on the NRST line of the MCU...

 

Regards,

John

 

 

 

Associate III
Sep 26, 2024 11:05 AM UTC

Pull down capacitor is 100 nF, as recommended...

Associate III
Sep 27, 2024 2:07 PM UTC

@Imen.D I have also tested to connect via J-Flash, which works fine.

WhoIsJohnGalt_0-1727445794869.png

Could it be that this is a CubeProgrammer issue?
(Connecting to a STM32U545 device works also with the CubeProgrammer)

Regards,

John

 

ST Technical Moderator
Sep 30, 2024 8:58 AM UTC

Hi @WhoIsJohnGalt ,

I escalated this issue internally to the appropriate team via ticket (ID 192398) in order to analyze this and take the necessary action.

PS: internal ticket ID 192398 is only for reference, not available outside of ST.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
Oct 2, 2024 2:34 PM UTC

Hi @WhoIsJohnGalt ,

After check, this issue is related to the access port when connecting with J-Link and will be fixed in the upcoming release of STM32CubeProgrammer.

For now, you can manually change the access port from 0 to 1, which should resolve the issue with the current version.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Nov 27, 2024 3:40 PM UTC

Hello @WhoIsJohnGalt ,

I would inform you that this issue is fixed in the latest release of STM32CubeProgrammer (v2.18) available here on st.com.

Thank you for your patience and your kind understanding.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks