STM32CubeProgrammer Failure on STM32L4 with Error: Operation exceeds memory limits
- 5 replies
- 1772 views
Hi,
I am trying to flash MCU firmware on my STM32L4A6VGTx MCU in bootloader mode over UART using cube programmer v2.17.0. I tried through UI and command line but in both the cases it if failing with error- Operation exceeds memory limits.
Please refer output below and screen shot as well as logs attached.
=======================================================================
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=COM5 br=115200 -e all -w C:\Users\GUR11373\Downloads\LMU-LTE-416-86x-Rev11746.bin 0x08000000
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
Serial Port COM5 is successfully opened.
Port configuration: parity = even, baudrate = 115200, data-bit = 8,
stop-bit = 1.0, flow-control = off
Activating device: OK
Board : --
Chip ID: 0x461
BootLoader protocol version: 3.1
Device name : STM32L496xx/STM32L4A6xx
Flash size : 1 MBytes (default)
Device type : MCU
Revision ID : --
Device CPU : Cortex-M4
Mass erase ...
Mass erase command correctly executed.
Note: if there's any flash protection, it will not be erased.
Memory Programming ...
Opening and parsing file: LMU-LTE-416-86x-Rev11746.bin
File : LMU-LTE-416-86x-Rev11746.bin
Size : 551.46 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Error: Operation exceeds memory limits
Error: failed to erase memory
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>
=======================================================================
I got to know there are some changes in address ranges in MCU database config files like the one provided on link- https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32cubeprogrammer-failure/td-p/636609. However, this does not apply to out STM32L4A6 board.
Please provide a similar fix for my board referring to STM32_Prog_DB_0x461.xml.
Looking forward for the early resolution of same.
Thanks
Ramakant