Skip to main content
Associate II
September 9, 2025
Solved

STLink V2 SWD operation without connecting VDD_TARGET PIN

Dear ST Community.

I am designing devices with STM32WL microcontrollers with highly limited board space. I routed out traces for all SWD signals (VDD, GND, NRST, SWDIO, SWCLK)

I have my Prototype Board, original ST-Link V2 with V2J45S7 Firmware and STM32CubeProgrammer version v2.20.0. During testing I realized that the connection to Prototype is stable only when I connect all 5 signals. For some reason I thought that "VDD_Target" pin on ST-Link side can be left floating.

I have found a previous post:
https://community.st.com/t5/stm32-mcus-boards-and-hardware/how-to-connect-the-stlink-v2-to-my-board/m-p/94389
but unfortunately in my case I have to have "VDD_Target" signal connected on both ends. When disconnected STMCubeProgrammer responds with error shown below:

MJaworski_0-1757416779861.png

Do I need to have all SWD signals being connected in order to program my Prototype or is there any hidden option in ST-Link/STMCubeProgrammer that I can turn on, so in final design I can omit routing VDD pin for SWD connector?

Kind regards
Marek Jaworski.

This topic has been closed for replies.
MJaworskiBest answer
Associate II
September 16, 2025

Okay people, let's wrap the thread up.

Thank you very much mfgkw and other users for help with this one, now jumping to conclusion:

1. STLink-V2 requires "VDD_TARGET" Pin connected in order to establish a connection with the Prototype BUT, it doesn't have to be connected to the Prototype itself, any other source of valid voltage on this pin allows to establish a connection between ST-Link and Prototype

2. When using ST-Link from Nucleo Boards, there is no need for connecting "VDD_TARGET" to Prototype. From what I saw an Nucleo schematics (Document MB1136, p. 4):

MJaworski_0-1758017623801.png

there is a pullup resistor on the VDD_TARGET pin, so without connecting it to the Prototype, pullup provides a valid voltage to PA0(AIN_1) Pin

3. There is unverified claim that this pin doesn't have to be connected when using Keil software.

If there is nothing more to add, we can close this thread and let it get indexed by google for future generations.

20 replies

MJaworskiAuthor
Associate II
September 12, 2025

Thank you very much for your experiment mfgkw, it proves that STLink can be deceived by external power supply.

I do have a question though: does your setup work when you have Supply B disconnected from STLink's VDD? If so, I then believe that there is some error in my Prototype, I will look on signal lines with oscilloscope to detect possible faulty behaviour.

Associate II
September 12, 2025

> I do have a question though: does your setup work when you have Supply B disconnected from STLink's VDD?

no, then I have no connection.

 

 

MJaworskiAuthor
Associate II
September 12, 2025

Alright, correct me if I'm wrong but then it means that STLink-V2 requires "VDD_Target" to be connected in order to work properly. That's a bummer.

Associate II
September 12, 2025

VDD has to be provided to the ST-Link, but not necessarily from your board.

Andrew Neil
Super User
September 15, 2025

@mfgkw wrote:

VDD has to be provided to the ST-Link


... or must it?

@Suresh_M in this thread claims to have it working in Keil without a Target VDD connection ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MJaworskiAuthorBest answer
Associate II
September 16, 2025

Okay people, let's wrap the thread up.

Thank you very much mfgkw and other users for help with this one, now jumping to conclusion:

1. STLink-V2 requires "VDD_TARGET" Pin connected in order to establish a connection with the Prototype BUT, it doesn't have to be connected to the Prototype itself, any other source of valid voltage on this pin allows to establish a connection between ST-Link and Prototype

2. When using ST-Link from Nucleo Boards, there is no need for connecting "VDD_TARGET" to Prototype. From what I saw an Nucleo schematics (Document MB1136, p. 4):

MJaworski_0-1758017623801.png

there is a pullup resistor on the VDD_TARGET pin, so without connecting it to the Prototype, pullup provides a valid voltage to PA0(AIN_1) Pin

3. There is unverified claim that this pin doesn't have to be connected when using Keil software.

If there is nothing more to add, we can close this thread and let it get indexed by google for future generations.

Andrew Neil
Super User
September 16, 2025

@MJaworski wrote:

If there is nothing more to add, we can close this thread and let it get indexed by google for future generations.


The way to do that is to Mark the solution (you can always change the marked post later, if further info comes to light)

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.